This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5060: 容性负载开机测试问题

Part Number: LM5060


电路图跟评估板一致,阻性负载开机时,通过调节MOSFET的GATE对GND的电容,使7A负载时可以正常开机。

但在容性负载下(电子负载CC模式下),负载电流0.2A时,开机起不来,MOSFET开机一直振荡,估计是保护了。

想问下:

1. 在容性负载情况下,哪些参数可以调试使电路正常开机?

2. 评估板有调试过容性负载(电子负载恒流模式CC)开机的情况吗?

  • Hi

       容性负载应该会造成过载。

       没有做过容性的测试,因为这个芯片一般都是用于阻性负载。

  • RESTART AFTER OVER-CURRENT FAULT EVENT

    When a VDS fault condition has occurred and the TIMER pinvoltage has reached 2V, the LM5060 latches off the externalMOSFET. In order to initiate a restart, either the EN pin, theVINpin, or the UVLO pin must be toggled low and then high.

    过流保护后重新启动,需要EN、VIN或UVLO管脚先触发低,然后再触发高。

    其中VIN、UVLO都有一个阈值,比较好理解,EN有高和低两个阈值,触发低和触发高是否分别对应低和高的阈值?

    能否对上面故障后的恢复条件具体说明下?

  • Hi

        将保护过程的波形传上来看一下?

        一般结合波形和datasheet说明来看,比较容易理解。