Other Parts Discussed in Thread: BQ76940
使用bq76940+78350+76200方案做电池管理,14S
要求电池放电电流在50A,可是当我设置过流保护15A时候,
用20A放电,电池组正常保护,用30A放电,MOS在保护瞬间一下就烧坏了,当时电池电压是53V。
之前保护值设置60A,使用30A放电到欠压保护没有问题。
电路图如下:
MOS管型号:HYG028N10NS1B6 5对
相关参数:
请问电路如何改善才能满足要求,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.