Other Parts Discussed in Thread: GPCCHEM
得到GPRC数据后导入文件,直接就在低温-20°测试,依然出现了跳变从28%-0%,这个是什么原因,是否导入文件后要先学习常温曲线,然后低温下是不是也要学习曲线,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,从您提供的数据看,这个结果是正常的,请参考下面帖子的内容。
您好,The terminate voltage is where the gauge aims to report 0%, if it thinks that the Ra table is higher than it really is or that the load being applied is higher than it is it will report 0% earlier than the terminate voltage since it thinks there are higher IR losses that are expected. The load select setting can be used to determine the current used to simulate. I see you have already done the learning cycle so the Ra table should be updated, so changing load rate to something like the Present Average Discharge or Average Current may be better for the application.
您好,这个问题已经在E2E英文论坛发帖,请继续关注。