This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: BQSTUDIO上LED电量指示灯寄存器怎么设置才能达到以下要求?

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ76920EVM, BQSTUDIO

您好,

我使用BQ76920EVM,配置LED电量指示灯寄存器时,预计实现以下3种状态:

1.给电池充电时,LED闪烁,充满电后停止闪烁,LED灯常亮;

2.接上负载时,电池进入放电状态,LED根据电量状态100%电量时5个LED灯亮,80%电量4个LED灯亮,60%电量3个LED灯亮,40%电量2个LED灯亮,20%电量1个LED灯亮

3,电池不接负载也未进行充电时,LED灯不亮。

请问在BQSTUDIO软件上需要如何设置寄存器才可以实现以上3种状态?

谢谢!