Other Parts Discussed in Thread: BQSTUDIO, , BQ4050
因为设备有自耗电加电芯自耗电加电池保护板自耗电,电压从开始7V,27%的电量2个月存储期间,电压因为自耗电降到6.4V拿出来使用仍然是27%电量,但是一开始放电,电量就从27%变为0%了,请问这个是什么原因导致的,为什么电压掉了,电量没有更新,在睡眠期间的自耗电耗掉的电量会更新电量百分比吗?还是哪里设置有问题,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,正常芯片在sleep mode会定时唤醒检测电压,温度,电流等参数。您可以看一下相关参数的设置。
如果参数设置没有问题,建议您用最新的固件试一下还有没有这个问题。
电池装在主机上的自耗电是2.5ma左右,但是我们用负载模拟9ma放电,接上BQSTUDIO显示没有放电电流,然后电压下降,没有更新容量。请问要怎么处理
您好,正在询问更了解这款芯片的TI工程师,稍后回复。
您好,这个问题已经在E2E英文论坛发帖,暂时没有收到回复,请继续关注该帖。
您好,请检测SRP-SRN电压. 电流必须流过检测电阻,芯片才能检测到放电。
您好,正在询问更了解这款芯片的TI工程师,稍后回复。
您好,The HW must be designed so that any current from the cell flows through the sense resistor. There is no other way around this.
有没有其他方式可以解决这个问题,或者芯片里面的设置,有没有其他芯片能解决
你好,或者芯片里面能不能设置自耗电的数值,去更新电量
您好,可以设置自耗电的参数, 您可以试一下。
没有找到 在哪里可以设置BQ28Z610
您好,This gauge doesn't use self-discharge parameters. It will automatically adjust with OCV measurements for self-discharge, which is supposed to be significantly less than a typical current.
有没有其他芯片的方案能解决这个问题自耗电2.5ma太小,硬件检测不到,使电量更新的问题?
您好,BQ27542-G1和BQ4050是带self-discharge参数的芯片。
有没有什么办法能检测的到2.5ma的自耗电的硬件方式,可以推荐的
您好, 非常抱歉, 没有找到相关资料。