This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: Full available capacity和Qmax的区别

Part Number: BQ40Z50-R2


(1) .我在论坛看见说,Full available capacity指的是当电池处于极小电流(C/20)放电条件下可以释放出来的电量。感觉Qmax也是指在小电流放电条件下能释放出来的电量。两者有什么区别?

(2) . 根据阻抗跟踪算法,FCC=Qstart+PassedCharge+RM      

                               RM=(DOD final-DOD present)*Qmax

因为有电流和温度补偿,所以DOD final不是0%的OCV对应的DOD.

但如果是FAC的话,因为不计算电流和温度补偿,所以用的DOD final就是0%的OCV对应的DOD。

FCC和FAC计算公式的前2部分一样,只是RM中DOD final不一样,

可以这么理解吗?

  • 您好

    1, Qmax: Maximum battery chemical capacity, FAC是 the fully charged state to the terminate voltage, in mAh or mWh。一般QMAX要比FAC大。

    2, 是的,FAC未补偿,FCC有补偿

    FAC是This read-only command pair returns the uncompensated (less than C/20 load) capacity of the battery when fully charged. 

    FCC 是compensated (less than C/20 load) capacity of the battery when fully charged.