This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG1020EVM-006: What is your light source model and test method?

Part Number: LMG1020EVM-006
Other Parts Discussed in Thread: TIDA-01573

Hello TI engineers. So far, I have tested The LMG1020EVM-006 with R5-R8 . But I had to test a real laser diode to see the drive capability of the EVM.

I saw the results of your test in the manual ( TIDA-01573) and I would like to know your light source model and test method.

1. Which model of Laser Diode did your use in this experiment?

2.What is the test protocol?  (I already know that you are using Sorebo equipment, but are you directly aligning the Laser  light source with the detector and that's it?)

Looking forward to your reply!

THANK YOU!

  • Hi

        能够中文说明一下你的问题? 不是太明确你的意思。

       另外这个第三方公司提供的参考电路方案,所有的资料都在网站:  www.ti.com.cn/.../TIDA-01573

  • TI的工程师您好:

      我已经用R5-R8测试了LMG1020EVM-006。但我必须测试一个真正的激光二极管,看看EVM的驱动能力。

           我看到了您手册(TIDA-01573)中的测试结果,我想要知道测试时具体的激光二极管型号和测试方法。

    1.您在这个实验中所用的光源型号是什么?

     

    2.这个实验的测试方案是怎样的?
    我已经知道你们使用的是Thorlabs的设备,但是是直接将激光光源与探测器对准就可以么?

    我希望有一个测试的光路图或者 设备连接图 可以作为参考。

    关于EVM的电路方案和设计资料我已经看过了,但并没有提到测试时具体的 激光二极管型号 和 测试光路等信息。所以还需要麻烦您帮我找一下有没有相关资料。尤其是 手册里提到 两个905nm,75W的激光二极管,这个二极管的具体型号是什么?或者厂家的链接能不能提供一下?

    感谢!

  • Hi

         我这边也没有详细的资料,这些设计都是第三方公司的,提供的信息都在上述网站上(我们没有其他信息)。

         不过你可以在美国E2E上问一下: https://e2e.ti.com/