Part Number: BQ27200
量产写值过程出现写值参数错误0X78(SEDV1)写错了会有什么影响
老机种量产时,写值错误了,这个值写高了会有什么影响?
因已经做成了成品才发现,现在容量一直不更新
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ27200
量产写值过程出现写值参数错误0X78(SEDV1)写错了会有什么影响
老机种量产时,写值错误了,这个值写高了会有什么影响?
因已经做成了成品才发现,现在容量一直不更新
您好,请参考下面文档的1.3 Scaled End-of-Discharge Voltage First
将按比例缩放的放电终止电压优先 (SEDV1) 电压设置为电池所在的阈值 预计在典型负载条件下剩余 6.25% 的容量。
建议将参数改正以后,确认容量是否更新。
您好,评估板用户手册说明PROG pin需要21V。
The EEPROM screen allows the user to read and write the 10 EEPROM registers of bq27200. There are checkboxes (Enable LMD Aging, Customer ID #) that when its status are changed it will cause an automatic write to the EEPROM to ensure that the selections apply accordingly. Always when writing to the EEPROM ensure that the 21V pulse to PROG pin is available.
hi Star
感谢回复,想请教如下问题:
1,如果不更新EEPROM(0x78这个参数不更新),是否可以正常使用,和更新后的有何区别
2,在不更新EEPROM(0x78)的情况下是否可以通过老化learning 等方式更新容量