如图,在BQ4050的CEDV Smoothing Config中,EOC Smooth Current这一项参数的具体作用是什么?我看它的单位是%,那么若将它设为1%,意思是Max Smoothing Current的1%?
此外,Max Smoothing Current是平滑算法计算出的值吗?并不真实存在?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如图,在BQ4050的CEDV Smoothing Config中,EOC Smooth Current这一项参数的具体作用是什么?我看它的单位是%,那么若将它设为1%,意思是Max Smoothing Current的1%?
此外,Max Smoothing Current是平滑算法计算出的值吗?并不真实存在?
您好 ,
It is a percentage of the design capacity used to determine at what taper current threshold to state smoothing.
(EOC Smooth Current * Design Capacity) / 10
Division by 10 is to get the proper units, since it is stored as an integer and we need it to be in 0.1% units.
您好,
By default it is set to 0.2%, you can set it to 1% which would be the max listed in the TRM. So the smoothing would occur when 0.001*1200 = 12mA of charge current is flowing.
If you need a higher threshold you can manually write the register with the Advanced Communication Tab if the BQZ will not allow it.
Fri May 05 15:04:22 CST 2023 Device Version Info = 9e34_0_01 BQZ Device Name = bq4050 BQZ Firmware Version = V0_01_BLD22 Design Capacity = 1200 Design Voltage = 11100 Specification Info = 0x0031 Manufacturer Date = 1980-1-1 Serial Number = 0x0001 Manufacturer Name = Texas Instruments Device Name = bq4050 Device Chemistry = LION Sample,DateTime,ElapsedTime,ManufAccess,RemCapAlarm,RemTimeAlarm,BattMode,@Rate(@),@TimeFull,@TimeEmpty,@RateOK,Temperature,Voltage,Current,AvgCurr,MaxErr,RSOC,ASOC,SOH,RemCap,FullChgCap,RunTimeEmty,RunTimeEmty,AvgTimeFull,ChgCurr,ChgVolt,BattStat,CycleCnt,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,CellVolt3,CellVolt4,vBAT,vPACK,CellCurr1,CellCurr2,CellCurr3,CellCurr4,CellPower1,CellPower2,CellPower3,CellPower4,Power,AvgPow,IntTemp,TS1Temp,TS2Temp,TS3Temp,TS4Temp,CellTemp,FETTemp,CEDV_RC,DSGCap,CEDVThr,CEDVFltV,ChgDeficit,LogRowTime(ms),LogStatus 1,2023-05-05 15:04:26,4.006,0x0187,300,10,0x6000,0,65535,65535,1,32.4,12367,1579,1582,100,80,73,92,875,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4131,4117,4118,0,12404,12447,1578,1576,1576,0,652,649,649,0,1952,1954,32.6,32.4,-53.5,-53.5,-53.5,32.4,-273.2,876,1075,9447,11413,0,758,SUCCESS 2,2023-05-05 15:04:31,8.014,0x0187,300,10,0x6000,0,65535,65535,1,32.5,12368,1568,1579,100,80,74,92,877,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4131,4118,4119,0,12404,12441,1569,1565,1567,0,648,644,645,0,1939,1952,32.8,32.5,-53.5,-53.5,-53.5,32.5,-273.2,878,1075,9447,11413,0,780,SUCCESS 3,2023-05-05 15:04:35,12.016,0x0187,300,10,0x6000,0,65535,65535,1,32.5,12370,1559,1575,100,80,74,92,879,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4132,4118,4120,0,12398,12451,1559,1558,1558,0,644,642,642,0,1927,1947,32.7,32.4,-53.5,-53.5,-53.5,32.4,-273.2,880,1075,9447,11413,0,764,SUCCESS 4,2023-05-05 15:04:39,16.021,0x0187,300,10,0x6000,0,65535,65535,1,32.4,12371,1550,1570,100,80,74,92,881,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4132,4119,4120,0,12407,12450,1550,1548,1549,0,640,638,638,0,1916,1941,32.7,32.4,-53.5,-53.5,-53.5,32.4,-273.2,882,1075,9447,11413,0,774,SUCCESS 5,2023-05-05 15:04:43,20.028,0x0187,300,10,0x6000,0,65535,65535,1,32.5,12372,1542,1564,100,80,74,92,882,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4133,4119,4121,0,12407,12444,1541,1540,1542,0,637,634,635,0,1907,1934,32.9,32.6,-53.5,-53.5,-53.5,32.6,-273.2,883,1075,9447,11413,0,750,SUCCESS 6,2023-05-05 15:04:47,24.029,0x0187,300,10,0x6000,0,65535,65535,1,32.5,12374,1533,1557,100,80,74,92,884,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4133,4120,4121,0,12407,12453,1531,1530,1531,0,633,630,631,0,1896,1926,32.7,32.5,-53.5,-53.5,-53.5,32.5,-273.2,885,1075,9447,11413,0,765,SUCCESS 7,2023-05-05 15:04:51,28.037,0x0187,300,10,0x6000,0,65535,65535,1,32.6,12374,1522,1550,100,81,74,92,886,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4133,4120,4122,0,12410,12446,1523,1521,1523,0,629,627,628,0,1883,1917,32.9,32.6,-53.5,-53.5,-53.5,32.6,-273.2,887,1075,9447,11413,0,759,SUCCESS 8,2023-05-05 15:04:55,32.047,0x0187,300,10,0x6000,0,65535,65535,1,32.6,12376,1517,1542,100,81,74,92,887,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4134,4121,4122,0,12404,12456,1516,1515,1514,0,627,624,624,0,1876,1908,32.8,32.5,-53.5,-53.5,-53.5,32.5,-273.2,888,1075,9447,11413,0,762,SUCCESS 9,2023-05-05 15:04:59,36.055,0x0187,300,10,0x6000,0,65535,65535,1,32.5,12378,1509,1535,100,81,75,92,889,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4135,4121,4123,0,12414,12457,1509,1506,1506,0,624,621,621,0,1867,1899,32.7,32.5,-53.5,-53.5,-53.5,32.5,-273.2,890,1075,9447,11413,0,756,SUCCESS 10,2023-05-05 15:05:03,40.060,0x0187,300,10,0x6000,0,65535,65535,1,32.6,12379,1501,1529,100,81,75,92,891,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4135,4121,4124,0,12415,12449,1501,1500,1501,0,621,618,619,0,1857,1890,32.9,32.6,-53.5,-53.5,-53.5,32.6,-273.2,892,1075,9447,11413,0,766,SUCCESS 11,2023-05-05 15:05:07,44.072,0x0187,300,10,0x6000,0,65535,65535,1,32.6,12380,1493,1522,100,81,75,92,892,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4135,4122,4124,0,12408,12450,1493,1491,1492,0,617,615,615,0,1847,1881,32.7,32.6,-53.5,-53.5,-53.5,32.6,-273.2,893,1075,9447,11413,0,769,SUCCESS 12,2023-05-05 15:05:11,48.075,0x0187,300,10,0x6000,0,65535,65535,1,32.7,12381,1485,1514,100,81,75,92,894,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4135,4122,4125,0,12409,12460,1484,1483,1483,0,614,611,612,0,1837,1871,32.9,32.7,-53.5,-53.5,-53.5,32.7,-273.2,895,1075,9447,11413,0,751,SUCCESS 13,2023-05-05 15:05:15,52.087,0x0187,300,10,0x6000,0,65535,65535,1,32.9,12382,1476,1506,100,81,75,92,895,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4135,4122,4125,0,12419,12452,1475,1475,1475,0,610,608,608,0,1826,1861,32.7,32.9,-53.5,-53.5,-53.5,32.9,-273.2,897,1075,9447,11413,0,755,SUCCESS 14,2023-05-05 15:05:19,56.101,0x0187,300,10,0x6000,0,65535,65535,1,32.9,12384,1468,1498,100,82,75,92,897,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4136,4123,4125,0,12412,12458,1467,1469,1467,0,607,606,605,0,1818,1852,33.0,32.9,-53.5,-53.5,-53.5,32.9,-273.2,898,1075,9447,11413,0,754,SUCCESS 15,2023-05-05 15:05:23,60.114,0x0187,300,10,0x6000,0,65535,65535,1,33.0,12385,1459,1490,100,82,75,92,899,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4136,4123,4126,0,12420,12453,1457,1458,1457,0,603,601,601,0,1806,1842,33.2,32.9,-53.5,-53.5,-53.5,32.9,-273.2,900,1075,9447,11413,0,757,SUCCESS 16,2023-05-05 15:05:27,64.122,0x0187,300,10,0x6000,0,65535,65535,1,33.0,12386,1451,1481,100,82,75,92,900,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4137,4123,4127,0,12415,12456,1448,1451,1451,0,599,598,599,0,1795,1832,32.9,32.9,-53.5,-53.5,-53.5,32.9,-273.2,901,1075,9447,11413,0,752,SUCCESS 17,2023-05-05 15:05:31,68.136,0x0187,300,10,0x6000,0,65535,65535,1,32.8,12388,1442,1473,100,82,76,92,902,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4137,4124,4127,0,12417,12464,1439,1442,1441,0,595,595,595,0,1786,1822,33.0,32.8,-53.5,-53.5,-53.5,32.8,-273.2,903,1075,9447,11413,0,748,SUCCESS 18,2023-05-05 15:05:35,72.151,0x0187,300,10,0x6000,0,65535,65535,1,32.7,12389,1434,1465,100,82,76,92,903,1105,65535,65535,17,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4137,4125,4128,0,12425,12457,1432,1432,1433,0,592,591,592,0,1774,1811,32.9,32.7,-53.5,-53.5,-53.5,32.7,-273.2,905,1075,9447,11413,0,770,SUCCESS 19,2023-05-05 15:05:39,76.152,0x0187,300,10,0x6000,0,65535,65535,1,32.7,12391,1425,1456,100,82,76,92,905,1105,65535,65535,16,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4138,4125,4128,0,12417,12460,1423,1423,1423,0,589,587,587,0,1764,1801,33.0,32.7,-53.5,-53.5,-53.5,32.7,-273.2,906,1075,9447,11413,0,750,SUCCESS 20,2023-05-05 15:05:43,80.161,0x0187,300,10,0x6000,0,65535,65535,1,32.8,12391,1416,1448,100,83,76,92,907,1105,65535,65535,16,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4138,4125,4129,0,12420,12467,1416,1415,1415,0,586,584,584,0,1753,1790,33.0,32.8,-53.5,-53.5,-53.5,32.8,-273.2,908,1075,9447,11413,0,760,SUCCESS 21,2023-05-05 15:05:47,84.167,0x0187,300,10,0x6000,0,65535,65535,1,32.9,12393,1407,1439,100,83,76,92,908,1105,65535,65535,16,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4138,4126,4129,0,12428,12469,1406,1405,1406,0,582,580,581,0,1742,1780,33.0,32.9,-53.5,-53.5,-53.5,32.9,-273.2,909,1075,9447,11413,0,752,SUCCESS 22,2023-05-05 15:05:51,88.170,0x0187,300,10,0x6000,0,65535,65535,1,32.9,12394,1398,1430,100,83,76,92,910,1105,65535,65535,16,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4139,4126,4130,0,12427,12469,1397,1397,1396,0,578,576,577,0,1732,1769,33.2,32.9,-53.5,-53.5,-53.5,32.9,-273.2,911,1075,9447,11413,0,766,SUCCESS 23,2023-05-05 15:05:55,92.169,0x0187,300,10,0x6000,0,65535,65535,1,32.8,12395,1389,1421,100,83,76,92,911,1105,65535,65535,16,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4139,4126,4130,0,12433,12470,1387,1387,1386,0,574,572,572,0,1721,1759,33.0,32.8,-53.5,-53.5,-53.5,32.8,-273.2,912,1075,9447,11413,0,767,SUCCESS 24,2023-05-05 15:05:59,96.181,0x0187,300,10,0x6000,0,65535,65535,1,32.8,12397,1379,1412,100,83,77,92,913,1105,65535,65535,16,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4140,4127,4131,0,12433,12465,1378,1376,1377,0,570,568,569,0,1708,1747,33.1,32.8,-53.5,-53.5,-53.5,32.8,-273.2,914,1075,9447,11413,0,756,SUCCESS 25,2023-05-05 15:06:03,100.186,0x0187,300,10,0x6000,0,65535,65535,1,32.8,12398,1370,1403,100,83,77,92,914,1105,65535,65535,16,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4140,4127,4132,0,12426,12475,1369,1368,1368,0,567,565,565,0,1697,1736,32.9,32.8,-53.5,-53.5,-53.5,32.8,-273.2,915,1075,9447,11413,0,782,SUCCESS 26,2023-05-05 15:06:07,104.200,0x0187,300,10,0x6000,0,65535,65535,1,33.0,12400,1360,1394,100,83,77,92,916,1105,65535,65535,16,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4140,4128,4132,0,12437,12475,1356,1358,1357,0,561,561,561,0,1684,1725,33.0,33.0,-53.5,-53.5,-53.5,33.0,-273.2,917,1075,9447,11413,0,754,SUCCESS 27,2023-05-05 15:06:11,108.212,0x0187,300,10,0x6000,0,65535,65535,1,33.1,12401,1347,1384,100,83,77,92,917,1105,65535,65535,16,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4141,4128,4133,0,12437,12468,1345,1346,1348,0,557,556,557,0,1670,1712,33.1,33.1,-53.5,-53.5,-53.5,33.1,-273.2,918,1075,9447,11413,0,755,SUCCESS 28,2023-05-05 15:06:15,112.228,0x0187,300,10,0x6000,0,65535,65535,1,33.3,12402,1338,1374,100,84,77,92,919,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4141,4128,4133,0,12430,12478,1336,1336,1336,0,553,552,552,0,1658,1700,33.2,33.3,-53.5,-53.5,-53.5,33.3,-273.2,920,1075,9447,11413,0,1513,SUCCESS 29,2023-05-05 15:06:19,116.237,0x0187,300,10,0x6000,0,65535,65535,1,33.4,12404,1329,1364,100,84,77,92,920,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4142,4129,4134,0,12441,12470,1325,1324,1325,0,549,547,548,0,1644,1688,32.9,33.4,-53.5,-53.5,-53.5,33.4,-273.2,922,1075,9447,11413,0,1580,SUCCESS 30,2023-05-05 15:06:23,120.241,0x0187,300,10,0x6000,0,65535,65535,1,33.4,12405,1318,1354,100,84,77,92,922,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4142,4129,4135,0,12434,12477,1313,1313,1314,0,544,542,543,0,1631,1676,33.1,33.4,-53.5,-53.5,-53.5,33.4,-273.2,923,1075,9447,11413,0,1520,SUCCESS 31,2023-05-05 15:06:27,124.253,0x0187,300,10,0x6000,0,65535,65535,1,33.4,12407,1308,1344,100,84,77,92,923,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4142,4129,4135,0,12445,12479,1304,1303,1304,0,540,538,539,0,1619,1664,32.9,33.4,-53.5,-53.5,-53.5,33.4,-273.2,925,1075,9447,11413,0,1509,SUCCESS 32,2023-05-05 15:06:31,128.253,0x0187,300,10,0x6000,0,65535,65535,1,33.3,12408,1297,1334,100,84,78,92,925,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4143,4130,4136,0,12443,12472,1294,1293,1293,0,536,534,535,0,1606,1651,33.1,33.3,-53.5,-53.5,-53.5,33.3,-273.2,926,1075,9447,11413,0,1612,SUCCESS 33,2023-05-05 15:06:35,132.268,0x0187,300,10,0x6000,0,65535,65535,1,33.3,12411,1287,1324,100,84,78,92,926,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4144,4130,4137,0,12437,12485,1284,1285,1285,0,532,531,532,0,1595,1639,33.2,33.3,-53.5,-53.5,-53.5,33.3,-273.2,927,1075,9447,11413,0,1563,SUCCESS 34,2023-05-05 15:06:39,136.270,0x0187,300,10,0x6000,0,65535,65535,1,33.3,12412,1275,1313,100,84,78,92,928,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4145,4131,4137,0,12449,12483,1273,1273,1274,0,528,526,527,0,1581,1626,33.0,33.3,-53.5,-53.5,-53.5,33.3,-273.2,929,1075,9447,11413,0,1546,SUCCESS 35,2023-05-05 15:06:43,140.277,0x0187,300,10,0x6000,0,65535,65535,1,33.3,12413,1265,1303,100,85,78,92,929,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4145,4132,4138,0,12449,12476,1263,1263,1265,0,524,522,523,0,1569,1614,33.2,33.3,-53.5,-53.5,-53.5,33.3,-273.2,930,1075,9447,11413,0,1538,SUCCESS 36,2023-05-05 15:06:47,144.286,0x0187,300,10,0x6000,0,65535,65535,1,33.3,12415,1254,1293,100,85,78,92,930,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4146,4132,4138,0,12443,12487,1252,1252,1253,0,519,517,518,0,1556,1601,33.1,33.3,-53.5,-53.5,-53.5,33.3,-273.2,932,1075,9447,11413,0,1602,SUCCESS 37,2023-05-05 15:06:51,148.289,0x0187,300,10,0x6000,0,65535,65535,1,33.3,12417,1244,1282,100,85,78,92,932,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4146,4132,4139,0,12453,12488,1239,1239,1242,0,514,512,514,0,1541,1588,33.3,33.3,-53.5,-53.5,-53.5,33.3,-273.2,933,1075,9447,11413,0,1571,SUCCESS 38,2023-05-05 15:06:55,152.293,0x0187,300,10,0x6000,0,65535,65535,1,33.4,12418,1233,1272,100,85,78,92,933,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4147,4133,4140,0,12450,12491,1228,1228,1232,0,509,508,510,0,1526,1575,33.2,33.4,-53.5,-53.5,-53.5,33.4,-273.2,934,1075,9447,11413,0,1620,SUCCESS 39,2023-05-05 15:06:59,156.307,0x0187,300,10,0x6000,0,65535,65535,1,33.5,12420,1220,1261,100,85,78,92,935,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4147,4133,4140,0,12448,12491,1215,1214,1215,0,504,502,503,0,1510,1561,32.9,33.5,-53.5,-53.5,-53.5,33.5,-273.2,936,1075,9447,11413,0,1584,SUCCESS 40,2023-05-05 15:07:03,160.318,0x0187,300,10,0x6000,0,65535,65535,1,33.5,12421,1207,1249,100,85,78,92,936,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4148,4133,4141,0,12458,12484,1204,1205,1204,0,499,498,499,0,1496,1547,33.2,33.5,-53.5,-53.5,-53.5,33.5,-273.2,937,1075,9447,11413,0,1626,SUCCESS 41,2023-05-05 15:07:07,164.328,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12424,1196,1237,100,85,79,92,937,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4148,4134,4142,0,12451,12485,1194,1192,1192,0,495,493,494,0,1483,1533,33.1,33.5,-53.5,-53.5,-53.5,33.5,-273.2,938,1075,9447,11413,0,1656,SUCCESS 42,2023-05-05 15:07:11,168.338,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12425,1185,1226,100,85,79,92,939,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4149,4135,4142,0,12452,12494,1180,1181,1181,0,490,488,489,0,1469,1519,33.2,33.6,-53.5,-53.5,-53.5,33.6,-273.2,940,1075,9447,11413,0,1532,SUCCESS 43,2023-05-05 15:07:15,172.349,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12426,1171,1214,100,86,79,92,940,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4150,4135,4142,0,12461,12488,1167,1165,1168,0,484,482,484,0,1453,1504,33.1,33.6,-53.5,-53.5,-53.5,33.6,-273.2,941,1075,9447,11413,0,1568,SUCCESS 44,2023-05-05 15:07:19,176.363,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12428,1159,1202,100,86,79,92,941,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4150,4135,4143,0,12458,12488,1157,1154,1156,0,480,477,479,0,1438,1490,33.1,33.6,-53.5,-53.5,-53.5,33.6,-273.2,942,1075,9447,11413,0,1548,SUCCESS 45,2023-05-05 15:07:23,180.375,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12430,1151,1191,100,86,79,92,942,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4151,4136,4144,0,12456,12500,1146,1144,1146,0,476,473,475,0,1425,1476,33.1,33.5,-53.5,-53.5,-53.5,33.6,-273.2,944,1075,9447,11413,0,1618,SUCCESS 46,2023-05-05 15:07:27,184.384,0x0187,300,10,0x6000,0,65535,65535,1,33.5,12432,1139,1179,100,86,79,92,944,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4152,4136,4145,0,12462,12493,1135,1133,1136,0,471,469,471,0,1412,1462,32.9,33.5,-53.5,-53.5,-53.5,33.5,-273.2,945,1075,9447,11413,0,1626,SUCCESS 47,2023-05-05 15:07:31,188.386,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12433,1126,1168,100,86,79,92,945,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4152,4137,4145,0,12462,12502,1122,1123,1123,0,466,465,465,0,1398,1448,33.2,33.6,-53.5,-53.5,-53.5,33.6,-273.2,946,1075,9447,11413,0,1466,SUCCESS 48,2023-05-05 15:07:35,192.392,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12435,1116,1156,100,86,79,92,946,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4153,4137,4146,0,12472,12503,1111,1114,1111,0,461,461,461,0,1384,1433,33.1,33.6,-53.5,-53.5,-53.5,33.6,-273.2,947,1075,9447,11413,0,1545,SUCCESS 49,2023-05-05 15:07:39,196.398,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12437,1103,1144,100,86,79,92,947,1105,65535,65535,14,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4154,4138,4146,0,12473,12496,1100,1099,1096,0,457,455,454,0,1367,1419,33.2,33.6,-53.5,-53.5,-53.5,33.6,-273.2,948,1075,9447,11413,0,1521,SUCCESS 50,2023-05-05 15:07:43,200.408,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12439,1091,1132,100,86,80,92,949,1105,65535,65535,14,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4154,4138,4147,0,12467,12506,1088,1088,1086,0,452,450,450,0,1353,1404,33.2,33.6,-53.5,-53.5,-53.5,33.6,-273.2,950,1075,9447,11413,0,1526,SUCCESS 51,2023-05-05 15:07:47,204.419,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12440,1079,1121,100,86,80,92,950,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4155,4139,4148,0,12478,12507,1078,1076,1074,0,448,445,445,0,1339,1390,33.1,33.6,-53.5,-53.5,-53.5,33.6,-273.2,951,1075,9447,11413,0,1558,SUCCESS 52,2023-05-05 15:07:51,208.427,0x0187,300,10,0x6000,0,65535,65535,1,33.5,12442,1067,1109,100,87,80,92,951,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4155,4139,4149,0,12478,12500,1067,1065,1063,0,443,441,441,0,1324,1375,33.3,33.4,-53.5,-53.5,-53.5,33.4,-273.2,952,1075,9447,11413,0,1524,SUCCESS 53,2023-05-05 15:07:55,212.435,0x0187,300,10,0x6000,0,65535,65535,1,33.4,12444,1055,1097,100,87,80,92,952,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4156,4140,4149,0,12472,12510,1053,1054,1052,0,438,436,436,0,1310,1361,33.2,33.4,-53.5,-53.5,-53.5,33.4,-273.2,953,1075,9447,11413,0,1559,SUCCESS 54,2023-05-05 15:07:59,216.435,0x0187,300,10,0x6000,0,65535,65535,1,33.5,12446,1043,1085,100,87,80,92,953,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4157,4140,4150,0,12482,12506,1042,1041,1040,0,433,431,432,0,1296,1346,33.3,33.5,-53.5,-53.5,-53.5,33.5,-273.2,954,1075,9447,11413,0,1572,SUCCESS 55,2023-05-05 15:08:03,220.441,0x0187,300,10,0x6000,0,65535,65535,1,33.5,12447,1032,1073,100,87,80,92,955,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4157,4140,4150,0,12476,12515,1032,1030,1030,0,429,426,427,0,1281,1332,33.2,33.5,-53.5,-53.5,-53.5,33.5,-273.2,955,1075,9447,11413,0,1594,SUCCESS 56,2023-05-05 15:08:07,224.449,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12449,1022,1062,100,87,80,92,956,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4158,4141,4151,0,12486,12514,1019,1018,1018,0,424,422,423,0,1267,1318,33.1,33.6,-53.5,-53.5,-53.5,33.6,-273.2,957,1075,9447,11413,0,1593,SUCCESS 57,2023-05-05 15:08:11,228.463,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12451,1011,1053,100,87,80,92,957,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4158,4142,4151,0,12485,12508,1006,1010,1006,0,418,418,418,0,1255,1307,33.2,33.7,-53.5,-53.5,-53.5,33.7,-273.2,958,1075,9447,11413,0,1533,SUCCESS 58,2023-05-05 15:08:15,232.470,0x0187,300,10,0x6000,0,65535,65535,1,33.7,12452,1000,1042,100,87,80,92,958,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4159,4142,4152,0,12481,12507,997,998,996,0,415,413,414,0,1242,1293,33.1,33.7,-53.5,-53.5,-53.5,33.7,-273.2,959,1075,9447,11413,0,1556,SUCCESS 59,2023-05-05 15:08:19,236.472,0x0187,300,10,0x6000,0,65535,65535,1,33.7,12453,989,1030,100,87,80,92,959,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4159,4142,4153,0,12481,12517,986,988,986,0,410,409,409,0,1229,1279,33.2,33.7,-53.5,-53.5,-53.5,33.7,-273.2,960,1075,9447,11413,0,1539,SUCCESS 60,2023-05-05 15:08:23,240.487,0x0187,300,10,0x6000,0,65535,65535,1,33.7,12455,979,1019,100,87,80,92,960,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4160,4143,4153,0,12491,12513,975,975,974,0,406,404,405,0,1216,1266,33.1,33.7,-53.5,-53.5,-53.5,33.7,-273.2,961,1075,9447,11413,0,1527,SUCCESS 61,2023-05-05 15:08:27,244.488,0x0187,300,10,0x6000,0,65535,65535,1,33.7,12457,969,1009,100,87,81,92,961,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4160,4144,4153,0,12484,12512,964,964,964,0,401,399,400,0,1203,1253,33.2,33.6,-53.5,-53.5,-53.5,33.6,-273.2,962,1075,9447,11413,0,1545,SUCCESS 62,2023-05-05 15:08:31,248.495,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12458,958,998,100,88,81,92,962,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4161,4144,4154,0,12488,12516,955,954,953,0,397,395,396,0,1191,1239,33.4,33.6,-53.5,-53.5,-53.5,33.6,-273.2,963,1075,9447,11413,0,1505,SUCCESS 63,2023-05-05 15:08:35,252.506,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12460,949,987,100,88,81,92,963,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4162,4145,4154,0,12488,12516,945,947,945,0,393,393,393,0,1179,1226,33.2,33.6,-53.5,-53.5,-53.5,33.6,-273.2,964,1075,9447,11413,0,1599,SUCCESS 64,2023-05-05 15:08:39,256.516,0x0187,300,10,0x6000,0,65535,65535,1,33.6,12462,939,977,100,88,81,92,964,1105,65535,65535,15,0,0,0x0080,63,0x0187,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4162,4145,4155,0,12489,12523,937,936,934,0,390,388,388,0,1168,1214,33.2,33.5,-53.5,-53.5,-53.5,33.5,-273.2,965,1075,9447,11413,0,1617,SUCCESS 65,2023-05-05 15:08:43,260.519,0x01C7,300,10,0x6000,0,65535,65535,1,33.5,12463,929,967,100,88,81,92,965,1105,65535,65535,15,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4163,4146,4155,0,12498,12517,927,926,925,0,386,384,384,0,1155,1201,33.1,33.5,-53.5,-53.5,-53.5,33.5,-273.2,966,1075,9447,11413,0,1513,SUCCESS 66,2023-05-05 15:08:47,264.519,0x01C7,300,10,0x6000,0,65535,65535,1,33.5,12464,921,957,100,88,81,92,967,1105,65535,65535,15,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4163,4146,4156,0,12491,12518,919,916,917,0,383,380,381,0,1143,1189,33.2,33.5,-53.5,-53.5,-53.5,33.5,-273.2,967,1075,9447,11413,0,1543,SUCCESS 67,2023-05-05 15:08:51,268.526,0x01C7,300,10,0x6000,0,65535,65535,1,33.5,12465,911,947,100,88,81,92,968,1105,65535,65535,15,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4163,4146,4156,0,12494,12526,909,906,907,0,378,376,377,0,1132,1177,33.2,33.5,-53.5,-53.5,-53.5,33.5,-273.2,968,1075,9447,11413,0,1600,SUCCESS 68,2023-05-05 15:08:55,272.531,0x01C7,300,10,0x6000,0,65535,65535,1,33.4,12467,903,937,100,88,81,92,969,1105,65535,65535,15,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4164,4147,4157,0,12502,12528,900,902,899,0,375,374,374,0,1122,1165,33.1,33.4,-53.5,-53.5,-53.5,33.4,-273.2,969,1075,9447,11413,0,1609,SUCCESS 69,2023-05-05 15:08:59,276.546,0x01C7,300,10,0x6000,0,65535,65535,1,33.3,12468,894,928,100,88,81,92,971,1105,65535,65535,15,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4164,4148,4157,0,12504,12522,893,894,892,0,372,371,371,0,1112,1153,33.3,33.3,-53.5,-53.5,-53.5,33.3,-273.2,970,1075,9447,11413,0,1590,SUCCESS 70,2023-05-05 15:09:03,280.549,0x01C7,300,10,0x6000,0,65535,65535,1,33.2,12469,886,919,100,88,81,92,972,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4165,4148,4158,0,12503,12531,884,885,884,0,368,367,368,0,1102,1142,33.1,33.1,-53.5,-53.5,-53.5,33.1,-273.2,971,1075,9447,11413,0,1588,SUCCESS 71,2023-05-05 15:09:07,284.550,0x01C7,300,10,0x6000,0,65535,65535,1,33.1,12471,878,910,100,89,82,92,974,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4165,4148,4158,0,12506,12523,876,877,877,0,365,364,365,0,1092,1131,33.4,33.1,-53.5,-53.5,-53.5,33.1,-273.2,972,1075,9447,11413,0,1546,SUCCESS 72,2023-05-05 15:09:11,288.554,0x01C7,300,10,0x6000,0,65535,65535,1,33.0,12472,870,901,100,89,82,92,975,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4166,4149,4158,0,12500,12534,868,869,869,0,362,361,361,0,1083,1121,33.0,33.0,-53.5,-53.5,-53.5,33.0,-273.2,973,1075,9447,11413,0,1515,SUCCESS 73,2023-05-05 15:09:15,292.563,0x01C7,300,10,0x6000,0,65535,65535,1,32.9,12473,862,893,100,89,82,92,976,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4166,4149,4158,0,12509,12533,861,860,862,0,359,357,358,0,1074,1110,33.0,32.9,-53.5,-53.5,-53.5,32.9,-273.2,974,1075,9447,11413,0,1530,SUCCESS 74,2023-05-05 15:09:19,296.576,0x01C7,300,10,0x6000,0,65535,65535,1,33.0,12474,854,884,100,89,82,92,978,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4166,4150,4159,0,12510,12527,854,852,855,0,356,354,356,0,1064,1100,33.2,33.0,-53.5,-53.5,-53.5,33.0,-273.2,975,1075,9447,11413,0,1575,SUCCESS 75,2023-05-05 15:09:23,300.583,0x01C7,300,10,0x6000,0,65535,65535,1,32.9,12475,848,876,100,89,82,92,979,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4167,4150,4159,0,12503,12528,843,846,846,0,351,351,352,0,1055,1090,32.9,32.8,-53.5,-53.5,-53.5,32.8,-273.2,976,1075,9447,11413,0,1521,SUCCESS 76,2023-05-05 15:09:27,304.585,0x01C7,300,10,0x6000,0,65535,65535,1,32.8,12476,841,869,100,89,82,92,981,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4167,4150,4159,0,12503,12536,837,838,839,0,349,348,349,0,1047,1081,33.0,32.8,-53.5,-53.5,-53.5,32.8,-273.2,977,1075,9447,11413,0,1507,SUCCESS 77,2023-05-05 15:09:31,308.587,0x01C7,300,10,0x6000,0,65535,65535,1,32.7,12477,834,861,100,89,82,92,982,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4168,4151,4160,0,12514,12530,831,831,831,0,346,345,346,0,1038,1072,32.9,32.7,-53.5,-53.5,-53.5,32.7,-273.2,978,1075,9447,11413,0,1524,SUCCESS 78,2023-05-05 15:09:35,312.589,0x01C7,300,10,0x6000,0,65535,65535,1,32.8,12479,828,854,100,89,82,92,983,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4168,4151,4160,0,12506,12532,824,824,824,0,343,342,343,0,1031,1062,33.1,32.7,-53.5,-53.5,-53.5,32.7,-273.2,979,1075,9447,11413,0,1580,SUCCESS 79,2023-05-05 15:09:39,316.603,0x01C7,300,10,0x6000,0,65535,65535,1,32.8,12479,821,846,100,90,83,92,985,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4168,4152,4160,0,12515,12531,818,818,818,0,341,340,340,0,1022,1054,33.1,32.8,-53.5,-53.5,-53.5,32.8,-273.2,980,1075,9447,11413,0,1492,SUCCESS 80,2023-05-05 15:09:43,320.606,0x01C7,300,10,0x6000,0,65535,65535,1,32.9,12481,815,839,100,90,83,92,986,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4168,4152,4160,0,12509,12532,812,810,812,0,338,336,338,0,1015,1045,33.0,32.9,-53.5,-53.5,-53.5,32.9,-273.2,981,1075,9447,11413,0,1527,SUCCESS 81,2023-05-05 15:09:47,324.612,0x01C7,300,10,0x6000,0,65535,65535,1,32.9,12481,808,832,100,90,83,92,988,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4169,4153,4160,0,12509,12541,807,805,805,0,336,334,335,0,1007,1037,33.1,32.9,-53.5,-53.5,-53.5,32.9,-273.2,982,1075,9447,11413,0,1605,SUCCESS 82,2023-05-05 15:09:51,328.613,0x01C7,300,10,0x6000,0,65535,65535,1,33.0,12483,803,826,100,90,83,92,989,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4169,4153,4161,0,12519,12533,800,799,799,0,334,332,332,0,1000,1028,33.1,33.0,-53.5,-53.5,-53.5,33.0,-273.2,982,1075,9447,11413,0,1511,SUCCESS 83,2023-05-05 15:09:55,332.619,0x01C7,300,10,0x6000,0,65535,65535,1,33.1,12483,797,819,100,90,83,92,990,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4169,4154,4161,0,12518,12533,795,796,795,0,331,331,331,0,992,1020,33.2,33.1,-53.5,-53.5,-53.5,33.1,-273.2,983,1075,9447,11413,0,1484,SUCCESS 84,2023-05-05 15:09:59,336.621,0x01C7,300,10,0x6000,0,65535,65535,1,33.1,12484,791,813,100,90,83,92,992,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4169,4154,4162,0,12512,12544,790,790,790,0,329,328,329,0,985,1013,33.1,33.1,-53.5,-53.5,-53.5,33.1,-273.2,984,1075,9447,11413,0,1526,SUCCESS 85,2023-05-05 15:10:03,340.637,0x01C7,300,10,0x6000,0,65535,65535,1,33.1,12485,786,807,100,90,83,92,993,1105,65535,65535,14,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4170,4154,4162,0,12522,12542,785,785,785,0,327,326,327,0,979,1005,33.1,33.1,-53.5,-53.5,-53.5,33.1,-273.2,985,1075,9447,11413,0,1483,SUCCESS 86,2023-05-05 15:10:07,344.638,0x01C7,300,10,0x6000,0,65535,65535,1,33.0,12486,780,801,100,90,83,92,994,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4170,4155,4162,0,12519,12537,780,780,780,0,325,324,325,0,973,998,33.3,33.0,-53.5,-53.5,-53.5,33.0,-273.2,986,1075,9447,11413,0,1508,SUCCESS 87,2023-05-05 15:10:11,348.640,0x01C7,300,10,0x6000,0,65535,65535,1,32.9,12487,774,795,100,91,83,92,996,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4170,4155,4162,0,12522,12546,771,773,773,0,322,321,322,0,967,991,33.1,33.0,-53.5,-53.5,-53.5,33.0,-273.2,987,1075,9447,11413,0,1632,SUCCESS 88,2023-05-05 15:10:15,352.649,0x01C7,300,10,0x6000,0,65535,65535,1,33.0,12488,769,789,100,91,84,92,997,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4171,4155,4162,0,12523,12536,771,769,770,0,322,320,320,0,959,984,33.1,32.9,-53.5,-53.5,-53.5,32.9,-273.2,988,1075,9447,11413,0,1509,SUCCESS 89,2023-05-05 15:10:19,356.651,0x01C7,300,10,0x6000,0,65535,65535,1,32.8,12488,764,784,100,91,84,92,999,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4171,4156,4163,0,12515,12547,766,764,763,0,319,318,318,0,953,977,33.1,32.7,-53.5,-53.5,-53.5,32.7,-273.2,988,1075,9447,11413,0,1519,SUCCESS 90,2023-05-05 15:10:23,360.656,0x01C7,300,10,0x6000,0,65535,65535,1,32.7,12489,760,778,100,91,84,92,1000,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4171,4156,4163,0,12524,12547,759,760,758,0,317,316,316,0,947,970,33.2,32.8,-53.5,-53.5,-53.5,32.8,-273.2,989,1075,9447,11413,0,1604,SUCCESS 91,2023-05-05 15:10:27,364.657,0x01C7,300,10,0x6000,0,65535,65535,1,32.7,12489,754,773,100,91,84,92,1001,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4171,4156,4163,0,12526,12537,754,753,753,0,314,313,313,0,942,964,33.1,32.7,-53.5,-53.5,-53.5,32.7,-273.2,990,1075,9447,11413,0,1536,SUCCESS 92,2023-05-05 15:10:31,368.658,0x01C7,300,10,0x6000,0,65535,65535,1,32.7,12490,750,768,100,91,84,92,1003,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4171,4156,4163,0,12518,12547,750,750,749,0,313,312,312,0,936,957,33.0,32.7,-53.5,-53.5,-53.5,32.7,-273.2,991,1075,9447,11413,0,1572,SUCCESS 93,2023-05-05 15:10:35,372.661,0x01C7,300,10,0x6000,0,65535,65535,1,32.7,12491,746,764,100,91,84,92,1004,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4171,4157,4163,0,12518,12549,744,743,743,0,310,309,309,0,931,953,33.1,32.7,-53.5,-53.5,-53.5,32.7,-273.2,992,1075,9447,11413,0,1517,SUCCESS 94,2023-05-05 15:10:39,376.662,0x01C7,300,10,0x6000,0,65535,65535,1,32.7,12492,741,759,100,91,84,92,1005,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4172,4157,4164,0,12528,12549,740,740,742,0,309,308,309,0,926,947,33.3,32.7,-53.5,-53.5,-53.5,32.7,-273.2,992,1075,9447,11413,0,759,SUCCESS 95,2023-05-05 15:10:43,380.662,0x01C7,300,10,0x6000,0,65535,65535,1,32.6,12493,737,754,100,92,84,92,1007,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4172,4158,4164,0,12519,12541,737,738,737,0,307,307,307,0,921,941,33.1,32.6,-53.5,-53.5,-53.5,32.6,-273.2,993,1075,9447,11413,0,772,SUCCESS 96,2023-05-05 15:10:47,384.671,0x01C7,300,10,0x6000,0,65535,65535,1,32.6,12493,733,750,100,92,84,92,1008,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4172,4158,4164,0,12521,12550,733,733,732,0,306,305,305,0,916,935,33.1,32.6,-53.5,-53.5,-53.5,32.6,-273.2,994,1075,9447,11413,0,762,SUCCESS 97,2023-05-05 15:10:51,388.687,0x01C7,300,10,0x6000,0,65535,65535,1,32.6,12494,729,745,100,92,85,92,1009,1105,65535,65535,13,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4172,4158,4164,0,12530,12541,729,730,727,0,304,304,303,0,911,930,33.0,32.6,-53.5,-53.5,-53.5,32.6,-273.2,995,1075,9447,11413,0,779,SUCCESS 98,2023-05-05 15:10:55,392.701,0x01C7,300,10,0x6000,0,65535,65535,1,32.6,12494,725,741,100,92,85,92,1010,1105,65535,65535,12,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4172,4158,4164,0,12521,12543,725,725,723,0,302,301,301,0,906,924,33.0,32.5,-53.5,-53.5,-53.5,32.5,-273.2,996,1075,9447,11413,0,750,SUCCESS 99,2023-05-05 15:10:59,396.713,0x01C7,300,10,0x6000,0,65535,65535,1,32.5,12495,721,737,100,92,85,92,1011,1105,65535,65535,12,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4173,4158,4165,0,12523,12552,720,720,718,0,300,299,299,0,901,919,33.2,32.4,-53.5,-53.5,-53.5,32.4,-273.2,996,1075,9447,11413,0,751,SUCCESS 100,2023-05-05 15:11:03,400.721,0x01C7,300,10,0x6000,0,65535,65535,1,32.5,12496,717,732,100,92,85,92,1012,1105,65535,65535,12,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4173,4158,4165,0,12533,12543,717,716,716,0,299,298,298,0,896,914,33.0,32.5,-53.5,-53.5,-53.5,32.5,-273.2,997,1075,9447,11413,0,761,SUCCESS 101,2023-05-05 15:11:07,404.732,0x01C7,300,10,0x6000,0,65535,65535,1,32.5,12496,713,728,100,92,85,92,1013,1105,65535,65535,12,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4173,4159,4165,0,12524,12544,714,712,710,0,298,296,296,0,891,909,33.0,32.5,-53.5,-53.5,-53.5,32.5,-273.2,998,1075,9447,11413,0,751,SUCCESS 102,2023-05-05 15:11:11,408.743,0x01C7,300,10,0x6000,0,65535,65535,1,32.6,12497,710,724,100,92,85,92,1014,1105,65535,65535,12,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4173,4159,4165,0,12524,12553,709,709,707,0,296,295,294,0,887,904,32.9,32.6,-53.5,-53.5,-53.5,32.6,-273.2,999,1075,9447,11413,0,752,SUCCESS 103,2023-05-05 15:11:15,412.747,0x01C7,300,10,0x6000,0,65535,65535,1,32.6,12497,706,720,100,92,85,92,1015,1105,65535,65535,12,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4173,4159,4165,0,12527,12545,706,704,705,0,295,293,294,0,881,899,33.1,32.6,-53.5,-53.5,-53.5,32.6,-273.2,1000,1075,9447,11413,0,747,SUCCESS 104,2023-05-05 15:11:19,416.755,0x01C7,300,10,0x6000,0,65535,65535,1,32.6,12498,702,716,100,92,85,92,1016,1105,65535,65535,12,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4159,4165,0,12526,12554,701,701,700,0,293,292,292,0,877,894,33.1,32.6,-53.5,-53.5,-53.5,32.6,-273.2,1000,1075,9447,11413,0,756,SUCCESS 105,2023-05-05 15:11:23,420.759,0x01C7,300,10,0x6000,0,65535,65535,1,32.6,12499,699,713,100,93,85,92,1017,1105,65535,65535,12,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4160,4166,0,12534,12555,698,699,699,0,291,291,291,0,872,891,33.0,32.5,-53.5,-53.5,-53.5,32.5,-273.2,1001,1075,9447,11413,0,757,SUCCESS 106,2023-05-05 15:11:27,424.774,0x01C7,300,10,0x6000,0,65535,65535,1,32.5,12499,696,709,100,93,85,92,1018,1105,65535,65535,12,0,0,0x0080,63,0x01C7,0x0002,0x20,0x8018,0x10,0x02B0,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4174,4160,4166,0,12535,12547,694,696,695,0,290,290,290,0,869,886,33.1,32.5,-53.5,-53.5,-53.5,32.5,-273.2,1002,1075,9447,11413,0,765,SUCCESS
您好,请参考下面内容
I went back and checked the firmware again, I think there may be an issue with the EOC Smooth Current units, it is not in 1% or 0.1% rates, it is in 10% increments. So if you program 1% into the register it will actually be 100% of the design capacity for the threshold. This needs to be adjusted in the TRM, I believe the units should have been 10% increments, not 0.1%.
From the log this would also make sense, about 60s after the Design Capacity threshold is passed the SMOOTH bit gets set.