This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195输入电路问题

Other Parts Discussed in Thread: TL431

我不需要USB充电协议,不需要OTG功能,我用12V的适配器输入

1,请问我可以把下图输入电路中这部分去掉吗?

2,然后在VBUS输入前端接一个TVS管可以吗?

3,可以的话我后端系统(mcu)的供电全部由SYS提供可以吗

  • 亲;应该没有问题。只要SYS够输出电流;用它供电也是可以的。

  • 谢谢!

    1,那我是不是可以把图中的上拉的OTG脚,直接接地,手册上说OTG是USB电流限制和升压使能,我不使用PMID的输出那么我就可以给OTG接地关闭升压?

    2,sys的输出电流最大能达到多少?  我后端用到的是几个上拉,然后驱动一个双色led指示灯,然后一个TL431的2.5V基准原

  • 1,那我是不是可以把图中的上拉的OTG脚,直接接地,手册上说OTG是USB电流限制和升压使能,我不使用PMID的输出那么我就可以给OTG接地关闭升压?

    不使用升压,可以将OTG接地

    2 sys的输出电流最大能达到多少?  我后端用到的是几个上拉,然后驱���一个双色led指示灯,然后一个TL431的2.5V基准原

    可以达到几安培的电流。

    谢谢