在TPS65381的使用手册上有明确说明该芯片可支持两种供电模式,一种是输入电压范围为5.8至36V,可支持CAN、MCU Core和3.3V IO电压。另外一种输入电压范围为4.5至5.8V,仅可支持MCU Core和3.3V IO电压。但在使用手册上对输入电压范围为4.5至5.8V的详细用法并没有说明,请问该芯片在输入电压范围为4.5至5.8V条件下的使用方法与输入电压范围为5.8至36V有何不同?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yuan mao:
1. 在TPS65381的使用手册上有明确说明该芯片可支持两种供电模式,一种是输入电压范围为5.8至36V,可支持CAN、MCU Core和3.3V IO电压。另外一种输入电压范围为4.5至5.8V,仅可支持MCU Core和3.3V IO电压。但在使用手册上对输入电压范围为4.5至5.8V的详细用法并没有说明,请问该芯片在输入电压范围为4.5至5.8V条件下的使用方法与输入电压范围为5.8至36V有何不同?
在4.5V和5.8V范围内无法保证5V的原因是TPS65381Q1只能实现降压,正常工作时由内部前级BUCK电路降压到6V,然后通过LDO输出5V和其他3.3V,1.2V等。所以,当输入电压为5.8V以下时,由于内部MOSFET的存在压降,导致没有办法得到5V输出(汽车使用的高速CAN BUS标准电平5V)。但是能够保证3.3V和1.2V输出。(因为这两者距离最小4.5V输入压差更大)。
谢谢。