This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS73001的使用问题



问题描述:使用TPS73001   5V to 3V3 负载电流是70ma。   芯片容易出现故障。datasheet上是(5.5V MAX)。请教此颗芯片用在5V输入,是否会不稳定?

问题帖子链接:http://www.deyisupport.com/question_answer/analog/power_management/f/24/t/10968.aspx

解答问题的TI FAE:    

个人心得:首先是对于芯片的学习,TPS730xx系列低压降(LDO)低功耗线性稳压器具有高电源抑制比(PSRR),超低噪音,快速启动,以及卓越的电压和负载瞬态响应采用小型SOT23封装。 采用NanoStar™提供的超小占位面积封装,以及超低配置文件和包裹的重量,使得它非常适合便携式应用:如手机和PDA。在家庭中的每个装置是稳定的,具有小2.2μF陶瓷电容器上输出。该TPS730xx系列采用了先进的,专有的BiCMOS制造工艺产生的低压差电压(例如,为120mV时的200mA,TPS73030)。每个设备实现快速的启动时间(大约50μs的一个旁路电容0.001μF),而功耗低静态电流(170μA典型值)。 ,此外,当该设备处于置于待机模式下,电源电流小于1μA更长。该TPS73018具有约33μVRMS输出噪声电压在1.8V输出一个0.01μF旁路电容。模拟元件的应用是噪声敏感的那个,如便携式射频电子,受益于高PSRR,低噪音功能,以及快速的响应时间。

从芯片的技术手册上可以看出其输出电压的电阻分压取值及滤波电容的选择,还可知其输入输出电压的范围等

在此不知道输出纹波怎么样,还要对其加电感

在此11KHz是怎么计算得来的