This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电源中的整流二极管选择



问题描述:电源的频率为100K. 想要选择整流二极管,二极管的datasheet上面, 不同管子的测试条件不一样:有的是在,IF=8.0A,diF/dt=1000A/µs,VR=400V的, 有的是在IF = 1 A; -di/dt = 50 A/µs; VR= 30 V; , 请问对与1个二级管来说:是不是在反向电压越大, di/dt越大的时候,反向恢复时间越快啊? 如果在VR30V,的时候,反向恢复时间为50ns, 对于100Khz的电源, 整流以及开关MOS管的缓冲, 是不是都够用了呢?

问题帖子链接:http://www.deyisupport.com/question_answer/analog/power_management/f/24/t/74267.aspx

解答问题的TI FAE:  

个人心得:正向电流会影响反向恢复时间的测定,正向电流越大,对应的正向压降越大,结电容一定的情况下,Qrr越大,因此反向恢复时间越大。di/dt越大,反向电流到达IRM的时间越短,反向恢复时间越小

下面是提供的二极管的datasheet