This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: The problem I found when using BQ24610 is that when the charging voltage is 12.6V, it can be used normally; when I need to change the charging voltage to 13.2V, the battery is not charged, and the PG light is on; when I charge the battery, the bat

Part Number: BQ24610

The problem I found when using BQ24610 is that when the charging voltage is 12.6V, it can be used normally; when I need to change the charging voltage to 13.2V, the battery is not charged, and the PG light is on; when I charge the battery, the battery power is above 90%, the PG light is not on, and the chip cannot work normally. May I ask whether the PG or chip state is related to the charging voltage? This is my work email :zhuohangyu@wennyfly.com