This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74701-Q1: Several questions about LM74701-Q1 application

Part Number: LM74701-Q1

Hi, TI  Experts:

I am evaluating LM74701-Q1 for my project, and I tested your EVM these days. 

I have several questions about this part, waiting for your reply.

1. Full conduction mode:  I tested the EVM, the Voltage difference between Cathode and Anode is I * rds(on), not 50mV, and when load is up to 60mA, the Gate voltage is equeal wiht VCAP,  so I think the mosfet is full condution.

2.  Vds Clamp mode: if Anode is Negative votlage,  the voltage is under Anode POR threshold, How does the Mosfet be driven on?

3 . The absoute voltage of Anode is 65V, if we don't add TVS, how to pass ISO7637-2 2A /2B test?

Thanks

Torres Liu