This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: RSOC在加速变为0,变0后继续放一段时间才到设定的cell截至电压

Part Number: BQ40Z50-R2


可以看到从RSOC为5%之后,RSOC下降速度明显加快,而放电电流是基本恒定的,所以这个要怎么解决

  • 您好,电池在快放完时放电很快这是正常现象。

  • 可是这个就很不正常啊,他剩余容量按道理还是以伏安积分法的方式来计算的,现在是恒流放电,也就是说,应该不会出现这么大变化啊,现在这个似乎和设置的5%点有关,5%之前都还算正常,剩余容量按相同速率下降,斜率基本一样,然后之后就突然转折了,斜率陡峭,基本都可以算跳变了

    就是这边的参数(这个电脑现在没有连2400所以看不到数据,但那个FD那里set RSOC threshold是0%,对应的电压是2650mv,clear RSOC threshold是5%,对应的电压是2726mv),但是这里的参数又和实际放电时的电芯电压匹配不上,就很迷,这边设置的用意是什么呢,原本以为是当某一电芯电压达到设定电压时,RSOC就修正为相应的设定值

  • 您好,这几个参数表示FD旗标举起和清除的阀值,与放电速率无关。

    您可以看一下电量计精度,电量计上报的 RSOC 与真实的 RSOC 相比的误差。

    请参考下面文档3.3 如何评估电量计精度

    www.ti.com.cn/.../zhcaaf7.pdf