This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PIN4:COMP 采用
PIN5:CFB设计为高带宽的使用。
PIN7:LO,PIN9:HO,PIN10:BST,D1,D2,T1组成Two_switch拓扑结构。
PIN8:PVIN,PIN12:VIN。采用如下的接法
PIN11:VCC接大于0.47uf的电容。 设计采用1.0uf。
PIN13:EN外接电阻160KΩ,30KΩ。当电源输入低于1.26V*(160+30)/ 30 =7.98V电源停止输出。
PIN14:软启动接0.01uf。
次级的二极管:D4耐压大于24V,电流考虑到使用情况大于1A即可(芯片可以输出3A),可以采用原先的二极管代替。
源级的两个二极管,耐压24V,电流较小,也可以采用原先的二极管代替。
,依旧保留原先220uf.另,原先的原理图上R1和C1的限流作用,由 LM5015内部限流代替,可以去掉。反激式可以去掉L1电感。