Other Parts Discussed in Thread: GPCCHEM
Hi
我们现在使用bq40z50-R4的芯片,制作了一个双节的电池;Term Voltage 是 6000mV;
当电池电压过放达到 4.0 V(单节2.0 V),再次充电需要达到 7.6V 后,有时更高,Remaining Capacity才会增加;
这种现象正常吗?如果正常是为什么呢?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您的CHEM ID是否配置,并却学习是否成功。
您好, 是否方便将完整的数据发过来看一下。GPCCHEM 报告也发过来看一下。
您好,smooth功能是否使能。
您好,请将gg文件发过来看一下。
您好,正在查询,稍后回复。
您好,请参考下面内容
1- The FD and TD thresholds might be set a little bit too high. Please set them to the below recommended. 
Recommended
2- Make sure Impedance Track is enabled. I noticed, update status is 2. It should be set to 6
| Gas Gauging | State | Update Status | 2 |