Other Parts Discussed in Thread: BQ76930
BQ78350-R1A的设计中,DF的setting中,Manufacturing中的Mfg Status init的设置会自动清除掉,变成0000,请问大概是什么原因。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ78350-R1A的设计中,DF的setting中,Manufacturing中的Mfg Status init的设置会自动清除掉,变成0000,请问大概是什么原因。
您好, It is not unknown that LEDs draw current. I see that there's a 100Ohm resistor in the LED path, see below for the EVM schematic. The 100 Ohm might be current limiters, but could be dissipating power.
What can be done is increase the Deadband to 50mA. This will inform the gauge to report 0mA for current less than 50mA. It has no gauging effect since the coulomb count will reset as I see the current going positive and negative, so the accumulated charge cancels out.
Calibration | Current Deadband | Deadband | 3 | mA | U | 1 | 792 | 3 | 0 | 255 | ddd | x+0 | x | mA | 0x03 |