This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Charging MOS does not turn on 充电MOS打不开

Part Number: BQ40Z80

The actual application circuit has no pre-charge/discharge function, I have turned off the pre-charge function during configuration, but the charging MOS still does not turn on after configuring the parameters, do I need to Download the firmware?(If it needs to download firmware, please provide firmware)

实际应用电路无预充电/放电功能,配置时我已经把预充功能关闭了,但是配置完参数后充电MOS还是不打开,是否需要烧录固件?(如果需要烧录请帮忙提供固件)

6 series lithium battery 10A rated current

6串锂电池10A额定电流

BQ40Z80-6S10A.gg.csv