This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

将电压从7V升压至24V

Other Parts Discussed in Thread: LM2733, TPS61170, LMR64010, LM27313

你好,各位专家们,现在小的在项目中遇到这个的问题,问题描述如下:将电池组(电压范围为6.4~7.2)升压至24V。这个24V作用如下图:

通过单片机的IO口控制SET和RESET,时序如右图置位/复位,从而得到一个24V左右的正负脉冲。我的理解是:24V的电压值给5欧姆的电阻负载充放电,按照欧姆定律,其电流为5A左右,而传感器datasheet中采用的升压芯片为电荷泵类型芯片,最大输出电流为30mA。这个电流难道不是5A吗?

那么,问题来了:

1:相对于24V而言,这个电路所需的负载电流多大?传感器datasheet称是电容C92(4.7uF)电容放电,此处不甚理解(为什么不是电源24的输出电流),希望专家们多多指教。

2:比较了TI公司的几款升压芯片:LM27313,LMR64010,TPS61170,LM2733。发现有个LM2733有个指标:Duty Cycle (Max) (%):96%,较高。这个指标说明了什么?

3:LM2733能否满足6.4~7.2)转24V需求,使用时需要注意点什么?
谢谢回答,祝工作顺利。