我用两节干电池串联输入,输出5V给传感器供电,传感器电流30mA,为啥电压上不去?不是5V而是3V多,手册里说电感1uH,我加到4.7uH后还是不行。
另外,有个奇怪的现象,如果先把传感器断电,再打开TPS61240,等升压到5V后再接入传感器,这时电压能保持在5V,但电感有啸叫。问题是我传感器功耗太大吗?但30mA给这个芯片是够用的啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
怀疑输入不能稳压,将输入的2.2uF加大到10uF, 并且layout上尽量靠近电感的输入端。
Hi
电感在叫?
请问你的功率电感饱和电流是多少?