This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: 两相并联使用,高侧MOS管栅极驱动波形问题以及SYNCIN引脚RT电阻如何选择

Part Number: LM5122
Other Parts Discussed in Thread: TINA-TI

LM5122两相并联使用,输入25V,输出58V ,输出测试电流1A-2A,开关频率约200KHz,电感10uH。

我在使用中遇到问题,请问谁曾遇到类似问题?如何解决呢?谢谢!

1、在58V 1A输出时,我测量到下MOS管和上MOS管栅极对地的波形如下:

图中黄色是高侧MOS栅极波形,紫色是下侧MOS栅极波形。请问,黄色高侧波形的一个振荡波形是什么原因导致的呢?是由于电感能量没有完全释放导致的振荡吗?

2、我测量高侧MOS栅极和源极(SW)波形,两者竟然一致?我觉得此时高侧mos管没有导通,这个波形正常吗?

3、如果输出58V 2A,则高侧MOS管源极(SW)波形没有振荡,但是栅极和源极的波形仍然一致。这是啥原因呢?

4、如果多相并联使用,外部输入clock,此时SYNCIN引脚的电阻RT如何选择呢?RT值对芯片开关频率还有影响吗?如果RT值过大,测量发现SYNCIN引脚电压波形发生畸变。