This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: 不能对电池进行充电

Part Number: BQ25606


Hello Ti's expert team,

我们在使用BQ25606进行单节锂电池充电管理设计,我们目前遇到了问题,BQ25606不能按预设定的电流对电池进行充电,下面附上我们的设计图纸及调试过程,请帮忙提供解决思路,谢谢!

1. 电池组,3.7V/6000mAh,内置10K B-3435 NTC,连接到所附图纸的Bat_NTC网络;

2.OTG pin已修改为下拉到GND;

3. D+ D-已修改为悬空;

4. 电池组先做预处理放电至3V,然后在VBUS处加载5V/6A的直流电源,BQ25606未能能对电池组进行稳定输出充电,直流电源显示电流在0与0.5A(近似值)之间跳动;

5. 将D+/D-短接,现象相同;

6. 将D-接GND或+2.8V,现象相同;

7. 将D+接+2.8V,现象相同;

8. 将D+接GND,直流电源显示电流稳定在0.47A。

请问,如何才能将充电电流调整到我们预设的3A?

  • schematic review如下:

    1. Ilim设置为3.02A。 ICHG设置为2.99A。

    2. OTG通过拉至GND禁用。

    3.您打算使用D+/D-线吗? 如果它们是浮动的并且适配器被检测为未知,则输入电流限制将由Ilim引脚确定。

    我对这些问题的意见如下:

    设备可能处于预充电状态。 预充电时,充电电流为ICHG的5%。 要了解您是否处于预充电状态,请查看VBATLOWV_Fall和VBATLOWV_RISE。