在使用LMG1210芯片,利用LTspice进行仿真验证,采用PWM模式,与EPC2035组成半桥buck芯片,PWM为方波信号,此时输出HO和LO输出错误,并不是正常的方波信号,请问这是什么原因?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,非常感谢您的回复!我有两个问题:
1. 我尝试更改过HS_DAP引脚接法,不接会仿真会报错,接地的话输出时序会报错,同时LMG1210datasheet这里显示HS_DAP是接到HS端口,以下是LMG1210datasheet引脚说明和LMG1210_EVM的PCB的schematic连接示意,我确实不知道该如何修改了,还麻烦您解答一下,非常感谢!

2. LMG1210采用独立模式,DLH接LDO5, DHL通过电阻接地,是否可以HB和HS由外部给电平,然后输出HO控制GaN功率管, 接法如下: