This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6415 JTAG问题

Other Parts Discussed in Thread: TMS320C6415

电路板刚到,一上电,JTAG连不上,仿真工具是seed-xds560plus.

按照《TMS320C6415 Hardware Designer's Resource Guide》检查JTAG部分的设计没找到问题。


请问下一步该如何查找问题呢,谢谢。

  • 请问具体报什么错?

    JTAG口信号都量过正常么?

  • 报错情况如下:
    IDE:     CCS3.3
    仿真器:SEED XDS560PLUS
    操作系统:windows XP (32bit)
    1、将仿真器接入电脑,并将仿真器与目标板连接好;
    2、将目标板上电;
    3、打开CCS3.3,点击connect
    报错:
    Error connecting to the target: Error 0x80000240/-1004 Fatal Error during: Initialization, OCS,  Processor communication timeout. It is recommended to RESET EMULATOR. This will disconnect each target, perform an emulation reset, and then reconnect each target. Power cycle the target board before continuing.   Sequence ID: 0 Error Code: -1004 Error Class: 0x80000240
     
    4、以后再次点击retry,都会报相同的错误:
    Error connecting to the target: Error 0x80003240/-116 Fatal Error during: Initialization, OCS, Target, Control,  This error was generated by TI's USCIF driver.  SC_ERR_CTL_TRASH <-116> A bad parameter value was detected within an internal data-structure of Unified-SCIF. The controller or Unified-SCIF may be in an invalid state.   Sequence ID: 0 Error Code: -116 Error Class: 0x80003240
    JTAG信号用100MHz示波器测量没发现异常的,请问下一步该如何排查问题呢,谢谢。
  • ccs和合众达仿真器能否调试其他的板子?

    量一下sysclk4管脚看是否有正确的时钟输出?

  • 感谢您的解答。

    1、 您指的是AE6(CLKOUT4/GP1)管脚吗,上电默认是CLKOUT4功能吗?

    2、 外部晶振50MHz,CLKOUT4输出的频率大致是多少呢,100MHz的示波器可以测得到吗,谢谢。

  • 1. 是的,默认是CLKOUT4时钟输出。

    2. 是1/4 CPU clock。

  • CLKMODE1:0 = 0x10 , 即12倍频,外部输入晶振是50MHz,

    CLKOUT4的输出频率应该是150MHz,用示波器测不到该时钟,显示的测量点电压大约为500mV。

    这种情况好像是DSP没有工作,下一步应该检查哪些关键点呢,请指导下,谢谢。

    DSP上电有供电时序的要求吗?

  • 查一下供电电压是否正确?纹波要求在数据手册的范围内。

    CLKIN信号时序要满足手册要求。

    RESET信号的长度要从电压,CLKIN时钟输入信号都稳定后开始计算。

    C6415对上电顺序没有特殊要求,一般核电压和I/O电压上电时间差不要超过1s.