各位大神们:
现在我们小组正在使用K2E开发板实现10G网络的传输,那么当我们在后期制版的工作中,考虑到K2E开发板为XFI接口,我们使用66AK2E05搭建系统的时候,外挂的万兆网模块是否仅使用XFP光模块即可,或者需要外挂PHY接口及光模块?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大神们:
现在我们小组正在使用K2E开发板实现10G网络的传输,那么当我们在后期制版的工作中,考虑到K2E开发板为XFI接口,我们使用66AK2E05搭建系统的时候,外挂的万兆网模块是否仅使用XFP光模块即可,或者需要外挂PHY接口及光模块?
K2E 10GE是支持XFI的,可以直接连接XFP光模块,如果是走背板,比如两块K2E直联,可以直接XFI连接XFI。
需要注意的是K2E 10GE仅支持XFI,不支持SFI,因此需要长距离光纤通信时,需要外接XFI-SFP的转换芯片
几个概念澄清一下,下面3个是光模块
SFP:支持速率为1Gbps。
SFP+:同SFP类型,只是支持的速率提高到10Gbps。
XFP:XFP也是10Gbps光模块,跟SFP+相比,XFP内部多了CDR(Clock Data Recover)模块,个头比较大,
下面2个是协议:
XFI,SFI
所以您的问题其实是问K2E 10GE接口输出XFI,然后转换SFI(接SFP+光模块)吧?中间的转换器件可能需要问下TI模拟论坛的工程师,我不确定DS100DF410是否可以