最近采用6416进行定点运算,请问有官方IQMATH库吗?我查了下,只有c64+的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近采用6416进行定点运算,请问有官方IQMATH库吗?我查了下,只有c64+的
没有C64的IQMATH库,就用RTS库里的吧。
下面句子关于IQMATH的描述:
However, C64+ DSP core does not support floating point operations in hardware;floating point operations on this platform will take place in software such as a C program. The standard run time support library will allow you to do floating point operations in C code as it is, though if you are looking for additional performance beyond the standard RTS there is an IQMath library for the C64x+ available that may be of some help.