This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: linux内核升级到5.4.106, 系统启动后停止 Unhandled fault: external abort on non-linefetch (0x1008)

Part Number: AM3354
Other Parts Discussed in Thread: AM3352, TPS65910

TI fae及各位大侠好:

目前使用am3354芯片,进行linux内核升级工作。由之前使用的3.2.0内核,升级为5.4.106内核(sdk为ti-processor-sdk-linux-am335x-evm-07.03.00.005/board-support);

u-boot使用之前版本,即U-Boot 2012.10-svn25;来编译引导新的5.4.106内核;u-boot信息,参加如下截图:

引导系统启动失败后,内核启动信息如下:

I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
machine_type:iMac120
is 300:false
NAND: 512 MiB
lcd: is not 300
Configurou LCD 0x180020

NAND read: device 0 offset 0x200000, size 0x800
2048 bytes read: OK
logo data error display black!
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment

musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: 1st phy_id 7c0f1,devad ffffffff,regnum 4,val 1e1
2nd-1 phy_id 7c0f1,devad ffffffff,regnum 4,val de1
3rd phy_id 7c0f1,devad ffffffff,regnum 0,val 0
cpsw, usb_ether
Hit any key to stop autoboot: 0
mmc_send_cmd : timeout: No status update
Card did not respond to voltage select!
Booting from nand ...

NAND read: device 0 offset 0x580000, size 0x500000
63 bytes read: OK
bootargs=console=ttyO0,115200n8 quiet root=ubi0:rootfs rw ubi.mtd=7,2048 noinitrd rootfstype=ubifs ip=off
blopen close
Wrong Image Format for bootm command
ERROR: can't get kernel image!
ZQ1500# set bootargs noinitrd root=/dev/nfs rw nfsroot=192.168.7.170:/home/d/wangyuan/imac120/ti-processor-sdk-linux-am335x-evm-07.03.00.005/targetNFS ip=192.168.7.235:::::eth0:off console=ttyO0,115200n8 loglevel=8
ZQ1500# setenv ipaddr 192.168.7.235
ZQ1500# setenv gatewayip 192.168.7.1
ZQ1500# setenv serverip 192.168.7.47
ZQ1500# tftp 0x80007fc0 uImage
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 192.168.7.47; our IP address is 192.168.7.235
Filename 'uImage'.
Load address: 0x80007fc0
Loading: T T T
TFTP error: 'File not found' (1)
Not retrying...
ZQ1500# tftp 0x80007fc0 uImage
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 192.168.7.47; our IP address is 192.168.7.235
Filename 'uImage'.
Load address: 0x80007fc0
Loading: #################################################################
#################################################################
#################################################################
#################################################################
########################################################
done
Bytes transferred = 4629056 (46a240 hex)
ZQ1500# tftp 0x80F80000 am335x-evm.dtb
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 192.168.7.47; our IP address is 192.168.7.235
Filename 'am335x-evm.dtb'.
Load address: 0x80f80000
Loading: #####
done
Bytes transferred = 65984 (101c0 hex)
ZQ1500# bootm 0x80007fc0 - 0x80F80000
blopen close
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-5.4.106-g023faefa70
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4628992 Bytes = 4.4 MiB
Load Address: 80008000
Entry Point: 80008000
## Flattened Device Tree blob at 80f80000
Booting using the fdt blob at 0x80f80000
XIP Kernel Image ... OK
OK
Loading Device Tree to 8faf9000, end 8fb0c1bf ... OK

Starting zq kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.4.106-g023faefa70 (root@df131f57a6ff) (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.9)) #1 PREEMPT Wed Sep 1 18:01:52 CST 2021
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM335x EVM
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x8c800000
[ 0.000000] On node 0 totalpages: 65280
[ 0.000000] Normal zone: 574 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 65280 pages, LIFO batch:15
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 64706
[ 0.000000] Kernel command line: noinitrd root=/dev/nfs rw nfsroot=192.168.7.170:/home/d/wangyuan/imac120/ti-processor-sdk-linux-am335x-evm-07.03.00.005/targetNFS ip=192.168.7.235:::::eth0:off console=ttyO0,115200n8 loglevel=8
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 194160K/261120K available (9216K kernel code, 294K rwdata, 3064K rodata, 1024K init, 256K bss, 17808K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts
[ 0.000000] random: get_random_bytes called from start_kernel+0x2b0/0x45c with crng_init=0
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000020] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000046] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000058] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000388] timer_probe: no matching timers found
[ 0.000602] Console: colour dummy device 80x30
[ 0.000649] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000657] This ensures that you still see kernel messages. Please
[ 0.000663] update your kernel commandline.
[ 0.000720] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.118842] pid_max: default: 32768 minimum: 301
[ 0.119104] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.119123] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.120196] CPU: Testing write buffer coherency: ok
[ 0.120278] CPU0: Spectre v2: using BPIALL workaround
[ 0.121259] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.121431] rcu: Hierarchical SRCU implementation.
[ 0.121523] EFI services will not be available.
[ 0.121956] devtmpfs: initialized
[ 0.135641] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.136118] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.136146] futex hash table entries: 256 (order: -1, 3072 bytes, linear)
[ 0.140404] pinctrl core: initialized pinctrl subsystem
[ 0.141345] DMI not present or invalid.
[ 0.141900] NET: Registered protocol family 16
[ 0.144599] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.172815] l3-aon-clkctrl:0000:0: failed to disable
[ 0.175210] cpuidle: using governor ladder
[ 0.175251] cpuidle: using governor menu
[ 0.196372] No ATAGs?
[ 0.196386] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.215704] debugfs: Directory '49000000.edma' with parent 'dmaengine' already present!
[ 0.215749] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.216603] reg-fixed-voltage fixedregulator0: GPIO lookup for consumer (null)
[ 0.216620] reg-fixed-voltage fixedregulator0: using device tree for GPIO lookup
[ 0.216650] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator0[0]'
[ 0.216669] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator0[0]'
[ 0.216686] reg-fixed-voltage fixedregulator0: using lookup tables for GPIO lookup
[ 0.216699] reg-fixed-voltage fixedregulator0: No GPIO consumer (null) found
[ 0.217063] reg-fixed-voltage fixedregulator1: GPIO lookup for consumer (null)
[ 0.217079] reg-fixed-voltage fixedregulator1: using device tree for GPIO lookup
[ 0.217100] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator1[0]'
[ 0.217118] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator1[0]'
[ 0.217131] reg-fixed-voltage fixedregulator1: using lookup tables for GPIO lookup
[ 0.217142] reg-fixed-voltage fixedregulator1: No GPIO consumer (null) found
[ 0.217438] reg-fixed-voltage fixedregulator2: GPIO lookup for consumer (null)
[ 0.217453] reg-fixed-voltage fixedregulator2: using device tree for GPIO lookup
[ 0.217474] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator2[0]'
[ 0.217505] reg-fixed-voltage fixedregulator2: No GPIO consumer (null) found
[ 0.217611] reg-fixed-voltage fixedregulator-v1_8d: GPIO lookup for consumer (null)
[ 0.217624] reg-fixed-voltage fixedregulator-v1_8d: using device tree for GPIO lookup
[ 0.217645] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator-v1_8d[0]'
[ 0.217663] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-v1_8d[0]'
[ 0.217676] reg-fixed-voltage fixedregulator-v1_8d: using lookup tables for GPIO lookup
[ 0.217687] reg-fixed-voltage fixedregulator-v1_8d: No GPIO consumer (null) found
[ 0.217881] v1_8d: supplied by vbat
[ 0.218054] reg-fixed-voltage fixedregulator-v3_3d: GPIO lookup for consumer (null)
[ 0.218067] reg-fixed-voltage fixedregulator-v3_3d: using device tree for GPIO lookup
[ 0.218089] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator-v3_3d[0]'
[ 0.218107] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-v3_3d[0]'
[ 0.218120] reg-fixed-voltage fixedregulator-v3_3d: using lookup tables for GPIO lookup
[ 0.218132] reg-fixed-voltage fixedregulator-v3_3d: No GPIO consumer (null) found
[ 0.218304] v3_3d: supplied by vbat
[ 0.219734] iommu: Default domain type: Translated
[ 0.222435] SCSI subsystem initialized
[ 0.223002] mc: Linux media interface: v0.10
[ 0.223059] videodev: Linux video capture interface: v2.00
[ 0.223175] pps_core: LinuxPPS API ver. 1 registered
[ 0.223186] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.223213] PTP clock support registered
[ 0.223252] EDAC MC: Ver: 3.0.0
[ 0.224666] Advanced Linux Sound Architecture Driver Initialized.
[ 0.226135] clocksource: Switched to clocksource timer1
[ 0.235483] thermal_sys: Registered thermal governor 'fair_share'
[ 0.235494] thermal_sys: Registered thermal governor 'bang_bang'
[ 0.235519] thermal_sys: Registered thermal governor 'step_wise'
[ 0.235528] thermal_sys: Registered thermal governor 'user_space'
[ 0.235536] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.236606] NET: Registered protocol family 2
[ 0.237524] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes, linear)
[ 0.237559] TCP established hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.237592] TCP bind hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.237623] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.237745] UDP hash table entries: 256 (order: 0, 4096 bytes, linear)
[ 0.237769] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes, linear)
[ 0.237950] NET: Registered protocol family 1
[ 0.238635] RPC: Registered named UNIX socket transport module.
[ 0.238653] RPC: Registered udp transport module.
[ 0.238661] RPC: Registered tcp transport module.
[ 0.238668] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.238687] PCI: CLS 0 bytes, default 64
[ 0.239833] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.241348] Initialise system trusted keyrings
[ 0.241748] workingset: timestamp_bits=14 max_order=16 bucket_order=2
[ 0.247791] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.248717] NFS: Registering the id_resolver key type
[ 0.248772] Key type id_resolver registered
[ 0.248780] Key type id_legacy registered
[ 0.248832] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.249678] Key type asymmetric registered
[ 0.249696] Asymmetric key parser 'x509' registered
[ 0.249757] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 0.249770] io scheduler mq-deadline registered
[ 0.249779] io scheduler kyber registered
[ 0.255746] gpio gpiochip0: (gpio-0-31): added GPIO chardev (254:0)
[ 0.255862] gpiochip_setup_dev: registered GPIOs 0 to 31 on device: gpiochip0 (gpio-0-31)
[ 0.255920] OMAP GPIO hardware version 0.1
[ 0.284121] gpio gpiochip1: (gpio-32-63): added GPIO chardev (254:1)
[ 0.284240] gpiochip_setup_dev: registered GPIOs 32 to 63 on device: gpiochip1 (gpio-32-63)
[ 0.286741] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.303073] gpio gpiochip2: (gpio-64-95): added GPIO chardev (254:2)
[ 0.303189] gpiochip_setup_dev: registered GPIOs 64 to 95 on device: gpiochip2 (gpio-64-95)
[ 0.304770] gpio gpiochip3: (gpio-96-127): added GPIO chardev (254:3)
[ 0.304869] gpiochip_setup_dev: registered GPIOs 96 to 127 on device: gpiochip3 (gpio-96-127)
[ 0.314248] pinctrl-single 44e10800.pinmux: 142 pins, size 568
[ 0.318135] pwm-backlight backlight: GPIO lookup for consumer enable
[ 0.318159] pwm-backlight backlight: using device tree for GPIO lookup
[ 0.318193] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/backlight[0]'
[ 0.318212] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/backlight[0]'
[ 0.318230] pwm-backlight backlight: using lookup tables for GPIO lookup
[ 0.318243] pwm-backlight backlight: No GPIO consumer enable found
[ 0.318277] pwm-backlight backlight: backlight supply power not found, using dummy regulator
[ 0.376493] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.381834] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250
[ 1.369153] printk: console [ttyS0] enabled
[ 1.375107] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 37, base_baud = 3000000) is a 8250
[ 1.387327] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 1.396314] random: fast init done
[ 1.400048] random: crng init done
[ 1.422013] brd: module loaded
[ 1.433548] loop: module loaded
[ 1.443284] mdio_bus fixed-0: GPIO lookup for consumer reset
[ 1.449187] mdio_bus fixed-0: using lookup tables for GPIO lookup
[ 1.455317] mdio_bus fixed-0: No GPIO consumer reset found
[ 1.460897] libphy: Fixed MDIO Bus: probed
[ 1.469745] mdio_bus 4a101000.mdio: GPIO lookup for consumer reset
[ 1.475978] mdio_bus 4a101000.mdio: using device tree for GPIO lookup
[ 1.482573] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/interconnect@4a000000/segment@0/target-module@100000/ethernet@0/mdio@1000[0]'
[ 1.497368] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/interconnect@4a000000/segment@0/target-module@100000/ethernet@0/mdio@1000[0]'
[ 1.512060] mdio_bus 4a101000.mdio: using lookup tables for GPIO lookup
[ 1.518721] mdio_bus 4a101000.mdio: No GPIO consumer reset found
[ 1.576180] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.583879] libphy: 4a101000.mdio: probed
[ 1.588917] mdio_bus 4a101000.mdio:00: GPIO lookup for consumer reset
[ 1.595401] mdio_bus 4a101000.mdio:00: using device tree for GPIO lookup
[ 1.602253] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/interconnect@4a000000/segment@0/target-module@100000/ethernet@0/mdio@1000/ethernet-phy@0[0]'
[ 1.618412] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/interconnect@4a000000/segment@0/target-module@100000/ethernet@0/mdio@1000/ethernet-phy@0[0]'
[ 1.634448] mdio_bus 4a101000.mdio:00: using lookup tables for GPIO lookup
[ 1.641420] mdio_bus 4a101000.mdio:00: No GPIO consumer reset found
[ 1.648346] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[ 1.657775] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.664164] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.669546] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.676823] cpsw 4a100000.ethernet: Detected MACID = b0:7e:11:b4:ad:ae
[ 1.685567] i2c /dev entries driver
[ 1.692452] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.700038] sdhci: Secure Digital Host Controller Interface driver
[ 1.706310] sdhci: Copyright(c) Pierre Ossman
[ 1.712276] omap_hsmmc 47810000.mmc: GPIO lookup for consumer cd
[ 1.718381] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup
[ 1.724966] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/target-module@47810000/mmc@0[0]'
[ 1.735567] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/target-module@47810000/mmc@0[0]'
[ 1.746072] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup
[ 1.752822] omap_hsmmc 47810000.mmc: No GPIO consumer cd found
[ 1.758701] omap_hsmmc 47810000.mmc: GPIO lookup for consumer wp
[ 1.764734] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup
[ 1.771494] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/target-module@47810000/mmc@0[0]'
[ 1.782100] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/target-module@47810000/mmc@0[0]'
[ 1.792600] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup
[ 1.799348] omap_hsmmc 47810000.mmc: No GPIO consumer wp found
[ 1.816514] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.823729] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.834845] pinctrl-single 44e10800.pinmux: pin PIN67 already requested by 4a100000.ethernet; cannot claim for 4803c000.mcasp
[ 1.846409] pinctrl-single 44e10800.pinmux: pin-67 (4803c000.mcasp) status -22
[ 1.853673] pinctrl-single 44e10800.pinmux: could not request pin 67 (PIN67) from group mcasp1_pins on device pinctrl-single
[ 1.865083] davinci-mcasp 4803c000.mcasp: Error applying setting, reverse things back
[ 1.873019] davinci-mcasp: probe of 4803c000.mcasp failed with error -22
[ 1.880925] NET: Registered protocol family 10
[ 1.886938] Segment Routing with IPv6
[ 1.890739] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.897614] NET: Registered protocol family 17
[ 1.902521] Key type dns_resolver registered
[ 1.907148] omap_voltage_late_init: Voltage driver support not added
[ 1.914238] Loading compiled-in X.509 certificates
[ 1.934119] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.939506] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.945682] gpiochip_find_base: found new base at 510
[ 1.951165] gpio gpiochip4: (omap-gpmc): added GPIO chardev (254:4)
[ 1.957618] gpiochip_setup_dev: registered GPIOs 510 to 511 on device: gpiochip4 (omap-gpmc)
[ 1.967413] omap2-nand 8000000.nand: GPIO lookup for consumer rb
[ 1.973467] omap2-nand 8000000.nand: using device tree for GPIO lookup
[ 1.980139] of_get_named_gpiod_flags: parsed 'rb-gpios' property of node '/ocp/gpmc@50000000/nand@0,0[0]' - status (0)
[ 1.991142] nand: device found, Manufacturer ID: 0xc2, Chip ID: 0xdc
[ 1.997548] nand: Macronix MX30LF4G18AC
[ 2.001404] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[ 2.009198] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 2.014665] 10 fixed-partitions partitions found on MTD device omap2-nand.0
[ 2.021693] Creating 10 MTD partitions on "omap2-nand.0":
[ 2.027140] 0x000000000000-0x000000020000 : "NAND.SPL"
[ 2.034386] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
[ 2.041926] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
[ 2.049352] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
[ 2.056775] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
[ 2.064352] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
[ 2.071704] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
[ 2.079042] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
[ 2.087048] 0x000000200000-0x000000a00000 : "NAND.kernel"
[ 2.097732] 0x000000a00000-0x000010000000 : "NAND.file-system"
[ 2.221569] reg-fixed-voltage fixedregulator2: GPIO lookup for consumer (null)
[ 2.228913] reg-fixed-voltage fixedregulator2: using device tree for GPIO lookup
[ 2.236382] of_get_named_gpiod_flags: can't parse 'gpios' property of node '/fixedregulator2[0]'
[ 2.245239] of_get_named_gpiod_flags: parsed 'gpio' property of node '/fixedregulator2[0]' - status (0)
[ 2.254779] gpio gpiochip1: Persistence not supported for GPIO 16
[ 2.286426] tps65910 0-002d: No interrupt support, no core IRQ
[ 2.292517] tps65910-gpio tps65910-gpio: ti,en-gpio-sleep not specified
[ 2.299245] gpiochip_find_base: found new base at 504
[ 2.310914] gpiochip_setup_dev: registered GPIOs 504 to 509 on device: gpiochip5 (tps65910)
[ 2.323596] vrtc: supplied by vbat
[ 2.328546] vio: supplied by vbat
[ 2.333632] vdd_mpu: supplied by vbat
[ 2.339104] vdd_core: supplied by vbat
[ 2.345531] vdig1: supplied by vbat
[ 2.350404] vdig2: supplied by vbat
[ 2.355238] vpll: supplied by vbat
[ 2.360031] vdac: supplied by vbat
[ 2.364769] vaux1: supplied by vbat
[ 2.369618] vaux2: supplied by vbat
[ 2.374447] vaux33: supplied by vbat
[ 2.379399] vmmc: supplied by vbat
[ 2.384052] vbb: supplied by vbat
[ 2.388084] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 2.396277] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
[ 2.402427] 8<--- cut here ---
[ 2.405511] Unhandled fault: external abort on non-linefetch (0x1008) at 0xd02e6000
[ 2.413208] pgd = 0e6a9de4
[ 2.415925] [d02e6000] *pgd=8c148811, *pte=4a326653, *ppte=4a326453
[ 2.422236] Internal error: : 1008 [#1] PREEMPT ARM
[ 2.427134] Modules linked in:
[ 2.430211] CPU: 0 PID: 14 Comm: kworker/0:1 Not tainted 5.4.106-g023faefa70 #1
[ 2.437549] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 2.443699] Workqueue: events deferred_probe_work_func
[ 2.448876] PC is at sysc_probe+0xb40/0x117c
[ 2.453178] LR is at omap_reset_deassert+0xd0/0x218
[ 2.458074] pc : [<c0463ed4>] lr : [<c04e42dc>] psr: 60000013
[ 2.464365] sp : cc14de08 ip : 00000001 fp : cb0775c0
[ 2.469610] r10: 00000028 r9 : 00000000 r8 : cc16d010
[ 2.474857] r7 : c0a2c7d4 r6 : c0f03048 r5 : 00000000 r4 : cb06b240
[ 2.481410] r3 : d02e6000 r2 : 00000000 r1 : 00026000 r0 : 00000000
[ 2.487966] Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none
[ 2.495131] Control: 10c5387d Table: 80004019 DAC: 00000051
[ 2.500901] Process kworker/0:1 (pid: 14, stack limit = 0x0918fb60)
[ 2.507194] Stack: (0xcc14de08 to 0xcc14e000)
[ 2.511576] de00: 00000001 00000000 c0f0ae20 c0c6ea1c c0c1a138 c0a2c314
[ 2.519792] de20: c0c1a0f8 c0c1a03c 00000001 00000001 00000030 c4cb5378 00000009 00000000
[ 2.528010] de40: cc16d010 c0f1fd70 c0f804f0 c0f1fd70 00000009 00000000 c0f0d4ac c05c5e7c
[ 2.536227] de60: c0f804ec cc16d010 00000000 c05c40b4 cc16d010 c0f1fd70 c05c4520 c0f03048
[ 2.544445] de80: 00000001 00000000 c0f303b8 c05c436c c0f1fd70 cc14deec cc16d010 00000000
[ 2.552662] dea0: cc14deec c05c4520 c0f03048 00000001 00000000 c0f303b8 c0f0d4ac c05c2340
[ 2.560880] dec0: c0f30390 cc03b1dc cc297634 c4cb5378 c0f303b8 c0f03048 cc16d010 cc16d054
[ 2.569097] dee0: c0f30390 c05c3e38 cc14df4c cc16d010 00000001 c4cb5378 cc16d010 cc16d010
[ 2.577315] df00: c0f305e8 c0f30390 00000000 c05c3194 cc16d010 c0f30384 c0f30384 c05c3628
[ 2.585534] df20: c0f303b4 cc03aa80 00000000 cfc6d200 00000000 c01412d0 cc14c000 c0f14d20
[ 2.593752] df40: cc03aa80 cc03aa94 c0f0d4ac cc14c000 c0f14d20 c0f0d4c0 00000008 c0141ce0
[ 2.601969] df60: 00000000 cc128f40 cc14c000 cc128f00 00000000 cc03aa80 c0141a54 cc061ec0
[ 2.610187] df80: cc128f58 c01473a4 00000000 cc128f00 c0147254 00000000 00000000 00000000
[ 2.618404] dfa0: 00000000 00000000 00000000 c01010e8 00000000 00000000 00000000 00000000
[ 2.626620] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 2.634837] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000
[ 2.643077] [<c0463ed4>] (sysc_probe) from [<c05c5e7c>] (platform_drv_probe+0x6c/0xa4)
[ 2.651036] [<c05c5e7c>] (platform_drv_probe) from [<c05c40b4>] (really_probe+0x208/0x348)
[ 2.659341] [<c05c40b4>] (really_probe) from [<c05c436c>] (driver_probe_device+0x60/0x16c)
[ 2.667646] [<c05c436c>] (driver_probe_device) from [<c05c2340>] (bus_for_each_drv+0x74/0xb8)
[ 2.676214] [<c05c2340>] (bus_for_each_drv) from [<c05c3e38>] (__device_attach+0xe0/0x14c)
[ 2.684518] [<c05c3e38>] (__device_attach) from [<c05c3194>] (bus_probe_device+0x84/0x8c)
[ 2.692737] [<c05c3194>] (bus_probe_device) from [<c05c3628>] (deferred_probe_work_func+0x64/0x90)
[ 2.701751] [<c05c3628>] (deferred_probe_work_func) from [<c01412d0>] (process_one_work+0x160/0x47c)
[ 2.710932] [<c01412d0>] (process_one_work) from [<c0141ce0>] (worker_thread+0x28c/0x620)
[ 2.719154] [<c0141ce0>] (worker_thread) from [<c01473a4>] (kthread+0x150/0x180)
[ 2.726590] [<c01473a4>] (kthread) from [<c01010e8>] (ret_from_fork+0x14/0x2c)
[ 2.733841] Exception stack(0xcc14dfb0 to 0xcc14dff8)
[ 2.738915] dfa0: 00000000 00000000 00000000 00000000
[ 2.747132] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 2.755348] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 2.761998] Code: e3130004 1a00002b e5943014 e0833001 (e5930000)
[ 2.768124] ---[ end trace cba680c691ee3340 ]---