我们将在春节假期期间对网站进行维护,可能暂时无法访问,同时工程师回复将有所延迟,敬请谅解.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] [TDA4VL] 通过 DP 端口无法显示电路板

问题 1

我使用的是 TDA4VL 电路板和 8.0.3 SDK,按默认设置构建和制作 SD 卡后,它可以正常启动,但通过 DP 端口无法显示,而且无法通过命令 modetest -M tidss -p 获取有关显示驱动器的任何信息,

 您能帮我解决这个问题吗? 

 

1

请查看随附的补丁,它可以在 TDA4VL 器件上启用 eDP 显示。请在 ti-processor-sdk-rtos-j721s2-evm-08_00_03_05\vision_apps 文件夹中应用补丁 Display_On_J721S2.patch,重新编译 SDK 并将其安装到 SD 卡上,然后将 k3-j721s2-vision-apps.dtbo 复制到 SD 卡的 rootfs/boot 文件夹。 

/cfs-file/__key/communityserver-discussions-components-files/791/8032.Display.zip

 

问题 2

我根据您的提示应用了补丁并安装了 SD 卡,但问题仍然存在,我需要您的进一步支持。 

2

您在 EVM 上检查了吗?因为做出上述更改后,我能够在 EVM 上看到 eDP 显示。

问题 3

是的,我按如下步骤在 EVM 上进行了检查:

  1. 在 ti-processor-sdk-rtos-j721s2-evm-08_00_03_05\vision_apps 中应用该补丁;
  2. 创建 vision_apps -j4;
  3. 创建linux_fs_install_sd;
  4. 将 k3-j721s2-vision-apps.dtbo 复制到 SD 卡的 rootfs/boot 文件夹;

5.将 SD 卡插入 EVM,给 EVM 上电; 

完成这些步骤后,我可以通过 minicom 捕获引导日志,但显示器上没有显示任何内容。 

我将检查主电路板是否存在硬件问题

 

3

您使用的 eDP 显示是什么? 

不同的一点是,我更改后只测试了 HP 显示器。对于其他显示,我们可能需要更改更多,尤其是在电路板上启用 eDP_PWN 信号。这可以通过配置由 i2c1 控制的 IO 扩展器来完成。但由于某些 i2c 问题,目前在 vision apps 的 apps_utils_soc.c 文件中禁用了此功能。

 

问题 4

我使用的是 DELL 显示器。

为了测试此问题,我更换了主板,但仍然会出现问题。

您是否需要一些其他信息来调试此问题?我在下面附上了引导日志,可能有助于调试此问题。谢谢!

U-Boot SPL 2021.01-g139f16e4c6 (Dec 09 2021 - 16:27:18 +0000)                  

SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.0--w2021.33-j721s2 (Terrif')         

SPL initial stack usage: 13440 bytes                                           

Trying to boot from MMC2                                                       

Starting ATF on ARM64 core...                                                   

                                                                               

NOTICE:  BL31: v2.5(release):08.00.00.004-dirty                                

NOTICE:  BL31: Built : 16:15:40, Dec  9 2021                                    

                                                                               

U-Boot SPL 2021.01-g139f16e4c6 (Dec 09 2021 - 16:23:11 +0000)                  

SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.0--w2021.33-j721s2 (Terrif')         

Trying to boot from MMC2                                                       

                                                                               

                                                                                

U-Boot 2021.01-g139f16e4c6 (Dec 09 2021 - 16:23:11 +0000)                      

                                                                               

SoC:   J721S2 SR1.0                                                            

Model: Texas Instruments J721S2 EVM                                            

ti_i2c_eeprom_am6_parse_record: Ignoring record id 17                          

ti_i2c_eeprom_am6_parse_record: Ignoring record id 17                          

Board: J721S2X-PM1-SOM rev E1                                                  

DRAM:  16 GiB                                                                  

Flash: 0 Bytes                                                                  

MMC:   mmc@4f80000: 0, mmc@4fb0000: 1                                          

Loading Environment from MMC...OK                                             

In:    serial@2880000                                                           

Out:   serial@2880000                                                          

Err:   serial@2880000                                                          

Net:   am65_cpsw_nuss_slave ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cp0

eth1: ethernet@46000000                                                        

Hit any key to stop autoboot:  0                                               

switch to partitions #0, OK                                                    

mmc1 is current device                                                         

SD/MMC found on device 1                                                       

Failed to load 'boot.scr'                                                      

484 bytes read in 4 ms (118.2 KiB/s)                                           

Loaded env from uEnv.txt                                                       

Importing environment from mmc1 ...                                            

Running uenvcmd ...                                                             

1 bytes read in 5 ms (0 Bytes/s)                                               

Already setup.                                                                 

## Error: "main_cpsw0_qsgmii_phyinit" not defined                              

k3_r5f_rproc r5f@41000000: Core 1 is already in use.No rproc commands work    

k3_r5f_rproc r5f@41400000: Core 2 is already in use.No rproc commands work    

912520 bytes read in 26 ms (33.5 MiB/s)                                        

Load Remote Processor 2 with data@addr=0x82000000 912520 bytes: Success!       

293836 bytes read in 13 ms (21.6 MiB/s)                                        

Load Remote Processor 3 with data@addr=0x82000000 293836 bytes: Success!       

Failed to load '/lib/firmware/j721s2-main-r5f1_0-fw'                           

Failed to load '/lib/firmware/j721s2-main-r5f1_1-fw'                           

13627456 bytes read in 131 ms (99.2 MiB/s)                                      

Load Remote Processor 6 with data@addr=0x82000000 13627456 bytes: Success!     

9965496 bytes read in 51 ms (186.3 MiB/s)                                      

Load Remote Processor 7 with data@addr=0x82000000 9965496 bytes: Success!       

19268096 bytes read in 415 ms (44.3 MiB/s)                                     

58082 bytes read in 7 ms (7.9 MiB/s)                                           

9534 bytes read in 5 ms (1.8 MiB/s)                                            

## Flattened Device Tree blob at 88000000                                      

   Booting using the fdt blob at 0x88000000                                    

   Loading Device Tree to 000000008feee000, end 000000008fffffff ...OK        

                                                                                

Starting kernel ...                                                            

                                                                               

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]         

[    0.000000] Linux version 5.10.65-g12f38abe68 (oe-user@oe-host) (aarch64-non1

[    0.000000] Machine model: Texas Instruments J721S2 EVM                     

[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002880000 (options '')   

[    0.000000] printk: bootconsole [ns16550a0] enabled                         

[    0.000000] efi: UEFI not found.                                            

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a01000l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a11000l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a21000l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a41000l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a61000l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a71000l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-dma-memory@l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-memory@a810l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000aa000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@aal

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000aa100000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-c71_0-memory@aa10l

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000b4000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@b40000l

[    0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, t

[    0.000000] Reserved memory: created DMA memory pool at 0x00000000da000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-l

[    0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, B

[    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-l

[    0.000000] Zone ranges:                                                    

[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]          

[    0.000000]   DMA32    empty                                                

[    0.000000]   Normal   [mem 0x0000000100000000-0x0000000bfffeffff]          

[    0.000000] Movable zone start for each node                                 

[    0.000000] Early memory node ranges                                        

[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]         

[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000b0ffffff]         

[    0.000000]   node   0: [mem 0x00000000b1000000-0x00000000b1ffffff]         

[    0.000000]   node   0: [mem 0x00000000b2000000-0x00000000fbffffff]         

[    0.000000]   node   0: [mem 0x00000000fc000000-0x00000000fffeffff]          

[    0.000000]   node   0: [mem 0x0000000880000000-0x000000088fffffff]         

[    0.000000]   node   0: [mem 0x0000000890000000-0x0000000bfffeffff]         

[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x0000000bfffeffff]

[    0.000000] On node 0, zone Normal: 1 pages in unavailable ranges           

[    0.000000] cma: Failed to reserve 512 MiB                                  

[    0.000000] psci: probing for conduit method from DT.                       

[    0.000000] psci: PSCIv1.1 detected in firmware.                            

[    0.000000] psci: Using standard PSCI v0.2 function IDs                     

[    0.000000] psci: Trusted OS migration not required                         

[    0.000000] psci: SMC Calling Convention v1.2                               

[    0.000000] percpu: Embedded 2 pages/cpu s49880 r8192 d73000 u131072        

[    0.000000] Detected PIPT I-cache on CPU0                                   

[    0.000000] CPU features: detected: GIC system register CPU interface       

[    0.000000] CPU features: detected: EL2 vector hardening                    

[    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923 

[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 261886   

[    0.000000] Kernel command line: console=ttyS10,115200n8 earlycon=ns16550a,mt

[    0.000000] Dentry cache hash table entries: 2097152 (order: 8, 16777216 byt)

[    0.000000] Inode-cache hash table entries: 1048576 (order: 7, 8388608 bytes)

[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off         

[    0.000000] software IO TLB: mapped [mem 0x000000009a800000-0x000000009e8000)

[    0.000000] Memory: 14869952K/16777088K available (10880K kernel code, 1344K)

[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1      

[    0.000000] rcu: Preemptible hierarchical RCU implementation.               

[    0.000000] rcu:     RCU event tracing is enabled.                          

[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. 

[    0.000000]  Trampoline variant of Tasks RCU enabled.                       

[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 ji.

[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2    

[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0                  

[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode                     

[    0.000000] GICv3: 960 SPIs implemented                                     

[    0.000000] GICv3: 0 Extended SPIs implemented                              

[    0.000000] GICv3: Distributor has no Range Selector support                

[    0.000000] GICv3: 16 PPIs implemented                                      

[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000  

[    0.000000] ITS [mem 0x01820000-0x0182ffff]                                 

[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS   

[    0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @8a0800000 (fl)

[    0.000000] ITS: using cache flushing for cmd queue                         

[    0.000000] GICv3: using LPI property table @0x00000008a00b0000             

[    0.000000] GIC: using cache flushing for LPI property table                

[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008a00c000

[    0.000000] random: get_random_bytes called from start_kernel+0x31c/0x4c4 wi0

[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).          

[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycless

[    0.000002] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398s

[    0.008323] Console: colour dummy device 80x25                              

[    0.012890] Calibrating delay loop (skipped), value calculated using timer f)

[    0.023561] pid_max: default: 32768 minimum: 301                            

[    0.028312] LSM: Security Framework initializing                            

[    0.033080] Mount-cache hash table entries: 32768 (order: 2, 262144 bytes, l)

[    0.040854] Mountpoint-cache hash table entries: 32768 (order: 2, 262144 byt)

[    0.050081] rcu: Hierarchical SRCU implementation.                          

[    0.055163] Platform MSI: msi-controller@1820000 domain created             

[    0.061340] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controllerd

[    0.070624] EFI services will not be available.                             

[    0.075378] smp: Bringing up secondary CPUs ...                             

[    0.080475] Detected PIPT I-cache on CPU1                                   

[    0.080503] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000  

[    0.080515] GICv3: CPU1: using allocated LPI pending table @0x00000008a00d000

[    0.080557] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]      

[    0.080622] smp: Brought up 1 node, 2 CPUs                                   

[    0.109973] SMP: Total of 2 processors activated.                           

[    0.114778] CPU features: detected: 32-bit EL0 Support                      

[    0.120032] CPU features: detected: CRC32 instructions                      

[    0.134404] CPU: All CPU(s) started at EL2                                  

[    0.138606] alternatives: patching kernel code                              

[    0.143678] devtmpfs: initialized                                           

[    0.150073] KASLR disabled due to lack of seed                              

[    0.154751] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, ms

[    0.164720] futex hash table entries: 512 (order: -1, 32768 bytes, linear)  

[    0.171879] pinctrl core: initialized pinctrl subsystem                     

[    0.177451] DMI not present or invalid.                                     

[    0.181670] NET: Registered protocol family 16                              

[    0.186725] DMA: preallocated 2048 KiB GFP_KERNEL pool for atomic allocations

[    0.194389] DMA: preallocated 2048 KiB GFP_KERNEL|GFP_DMA pool for atomic als

[    0.202702] DMA: preallocated 2048 KiB GFP_KERNEL|GFP_DMA32 pool for atomic s

[    0.211092] thermal_sys: Registered thermal governor 'step_wise'            

[    0.211094] thermal_sys: Registered thermal governor 'power_allocator'      

[    0.217436] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.   

[    0.231077] ASID allocator initialised with 65536 entries                   

[    0.247556] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages    

[    0.254414] HugeTLB registered 512 MiB page size, pre-allocated 0 pages     

[    0.261171] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages    

[    0.269105] cryptd: max_cpu_qlen set to 1000                                

[    0.275269] k3-chipinfo 43000014.chipid: Family:J721S2 rev:SR1.0 JTAGID[0x0bd

[    0.284168] vsys_3v3: supplied by evm_12v0                                   

[    0.288564] vsys_5v0: supplied by evm_12v0                                  

[    0.293193] iommu: Default domain type: Translated                          

[    0.298326] SCSI subsystem initialized                                      

[    0.302421] mc: Linux media interface: v0.10                                

[    0.306802] videodev: Linux video capture interface: v2.00                  

[    0.312436] pps_core: LinuxPPS API ver.1 registered                        

[    0.317507] pps_core: Software ver.5.3.6 - Copyright 2005-2007 Rodolfo Giom>

[    0.326844] PTP clock support registered                                    

[    0.330865] EDAC MC: Ver: 3.0.0                                             

[    0.334600] FPGA manager framework                                           

[    0.338119] Advanced Linux Sound Architecture Driver Initialized.           

[    0.344764] clocksource: Switched to clocksource arch_sys_counter           

[    0.351227] VFS: Disk quotas dquot_6.6.0                                     

[    0.355293] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes)

[    0.365176] Carveout Heap: Exported 512 MiB at 0x00000000ba000000           

[    0.371477] NET: Registered protocol family 2                                

[    0.376275] IP idents hash table entries: 262144 (order: 5, 2097152 bytes, l)

[    0.387376] tcp_listen_portaddr_hash hash table entries: 8192 (order: 1, 131)

[    0.396283] TCP established hash table entries: 131072 (order: 4, 1048576 by)

[    0.404979] TCP bind hash table entries: 65536 (order: 4, 1048576 bytes, lin)

[    0.413038] TCP: Hash tables configured (established 131072 bind 65536)     

[    0.419921] UDP hash table entries: 8192 (order: 2, 262144 bytes, linear)   

[    0.427019] UDP-Lite hash table entries: 8192 (order: 2, 262144 bytes, linea)

[    0.434653] NET: Registered protocol family 1                               

[    0.439436] RPC: Registered named UNIX socket transport module.             

[    0.445508] RPC: Registered udp transport module.                           

[    0.450314] RPC: Registered tcp transport module.                           

[    0.455117] RPC: Registered tcp NFSv4.1 backchannel transport module.       

[    0.461705] PCI: CLS 0 bytes, default 64                                    

[    0.466083] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counte

[    0.476561] Initialise system trusted keyrings                              

[    0.481195] workingset: timestamp_bits=46 max_order=18 bucket_order=0       

[    0.489458] squashfs: version 4.0 (2009/01/31) Phillip Lougher              

[    0.495718] NFS: Registering the id_resolver key type                       

[    0.500900] Key type id_resolver registered                                 

[    0.505173] Key type id_legacy registered                                   

[    0.509295] nfs4filelayout_init: NFSv4 File Layout Driver Registering...    

[    0.516143] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registerin.

[    0.523791] 9p: Installing v9fs 9p2000 file system support                  

[    0.549301] Key type asymmetric registered                                  

[    0.553489] Asymmetric key parser 'x509' registered                          

[    0.558493] Block layer SCSI generic (bsg) driver version 0.4 loaded (major )

[    0.566053] io scheduler mq-deadline registered                             

[    0.570678] io scheduler kyber registered                                   

[    0.575749] pinctrl-single 4301c000.pinctrl: 94 pins, size 376              

[    0.581877] pinctrl-single 11c000.pinctrl: 72 pins, size 288                

[    0.589702] k3-ringacc 2b800000.ringacc: Failed to get MSI domain           

[    0.595973] k3-ringacc 3c000000.ringacc: Failed to get MSI domain           

[    0.603696] Serial: 8250/16550 driver, 16 ports, IRQ sharing enabled        

[    0.616089] brd: module loaded                                              

[    0.622285] loop: module loaded                                             

[    0.625827] sysfs: cannot create duplicate filename '/devices/platform/dma_b'

[    0.633758] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 5.10.65-g12f38abe68 #1

[    0.640957] Hardware name: Texas Instruments J721S2 EVM (DT)                

[    0.646735] Call trace:                                                     

[    0.649236]  dump_backtrace+0x0/0x1a0                                       

[    0.652972]  show_stack+0x18/0x68                                            

[    0.656355]  dump_stack+0xd0/0x12c                                          

[    0.659825]  sysfs_warn_dup+0x60/0x80                                       

[    0.663560]  sysfs_create_dir_ns+0xe0/0xf8                                   

[    0.667741]  kobject_add_internal+0x98/0x288                                

[    0.672098]  kobject_add+0x94/0x100                                         

[    0.675658]  device_add+0xe0/0x740                                          

[    0.679128]  platform_device_add+0x100/0x238                                

[    0.683485]  platform_device_register_full+0xcc/0x150                       

[    0.688643]  dma_buf_phys_init+0x6c/0x9c                                    

[    0.692644]  do_one_initcall+0x54/0x1b8                                     

[    0.696559]  kernel_init_freeable+0x220/0x2a0                               

[    0.701006]  kernel_init+0x14/0x114                                         

[    0.704563]  ret_from_fork+0x10/0x34                                        

[    0.708231] kobject_add_internal failed for dma_buf_phys with -EEXIST, don't.

[    0.721413] megasas: 07.714.04.00-rc1                                       

[    0.726257] libphy: Fixed MDIO Bus: probed                                  

[    0.730921] tun: Universal TUN/TAP device driver, 1.6                       

[    0.736321] igbvf: Intel(R) Gigabit Virtual Function Network Driver         

[    0.742730] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.             

[    0.748801] sky2: driver version 1.30                                       

[    0.753007] VFIO - User Level meta-driver version: 0.3                      

[    0.758672] i2c /dev entries driver                                          

[    0.762742] sdhci: Secure Digital Host Controller Interface driver          

[    0.769069] sdhci: Copyright(c) Pierre Ossman                               

[    0.773662] sdhci-pltfm: SDHCI platform and OF driver helper                

[    0.779879] ledtrig-cpu: registered to indicate activity on CPUs            

[    0.786216] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....       

[    0.793325] optee: probing for conduit method.                               

[    0.797890] optee: revision 3.12 (3d47a131)                                 

[    0.798161] optee: initialized driver                                       

[    0.807184] NET: Registered protocol family 17                               

[    0.811802] 9pnet: Installing 9P2000 support                                

[    0.816194] Key type dns_resolver registered                                

[    0.820647] Loading compiled-in X.509 certificates                          

[    0.828360] k3-ringacc 2b800000.ringacc: Failed to get MSI domain           

[    0.834735] k3-ringacc 3c000000.ringacc: Failed to get MSI domain           

[    0.842374] ti-sci 44083000.system-controller: ABI: 3.1 (firmware rev 0x0015)

[    0.868121] omap_i2c 42120000.i2c: bus 0 rev0.12 at 100 kHz                 

[    0.874264] omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz                 

[    0.880344] omap_i2c 40b10000.i2c: bus 2 rev0.12 at 100 kHz                 

[    0.886589] pca953x 3-0021: supply vcc not found, using dummy regulator     

[    0.893413] pca953x 3-0021: using no AI                                     

[    0.921356] gpio-505 (CANUART_MUX1_SEL0): hogged as output/high             

[    0.927605] gpio-506 (CANUART_MUX2_SEL0): hogged as output/high             

[    0.933749] random: fast init done                                          

[    0.937324] gpio-507 (CANUART_MUX_SEL1): hogged as output/high              

[    0.943472] pca953x 3-0020: supply vcc not found, using dummy regulator     

[    0.950284] pca953x 3-0020: using no AI                                     

[    0.954837] pca953x 3-0022: supply vcc not found, using dummy regulator     

[    0.961644] pca953x 3-0022: using AI                                         

[    0.965962] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz                  

[    0.972115] pca953x 4-0020: supply vcc not found, using dummy regulator     

[    0.978935] pca953x 4-0020: using no AI                                      

[    1.005082] omap_i2c 2030000.i2c: bus 4 rev0.12 at 400 kHz                  

[    1.011440] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 125 d

[    1.019994] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Rod

[    1.029326] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 227 d

[    1.037911] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domaind

[    1.046801] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, 2

[    1.056687] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled     

[    1.063447] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies4

[    1.072374] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024,9

[    1.082530] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled     

[    1.089294] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies4

[    1.097292] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 15, base_baud =0

[    1.106797] 2880000.serial: ttyS10 at MMIO 0x2880000 (irq = 25, base_baud = 0

[    1.115636] printk: console [ttyS10] enabled                                

[    1.115636] printk: console [ttyS10] enabled                                

[    1.124249] printk: bootconsole [ns16550a0] disabled                        

[    1.124249] printk: bootconsole [ns16550a0] disabled                        

[    1.172777] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 0

[    1.180432] libphy: 46000f00.mdio: probed                                   

[    1.185780] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, dri7

[    1.194089] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss ve0

[    1.208028] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010c, freq:200000000, ad0

[    1.216926] mmc0: CQHCI version 5.10                                        

[    1.224012] vdd_mmc1: supplied by vsys_3v3                                  

[    1.228826] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fca100      

[    1.235654] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fca100      

[    1.242463] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fca100      

[    1.249269] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fca100       

[    1.256392] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan:)

[    1.261358] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 6t

[    1.273172] ti-udma 31150000.dma-controller: Channels: 50 (tchan: 25, rchan:)

[    1.284959] spi-nor spi0.0: s28hs512t (65536 Kbytes)                        

[    1.289936] 7 cmdlinepart partitions found on MTD device 47040000.spi.0     

[    1.296535] Creating 7 MTD partitions on "47040000.spi.0":                  

[    1.302008] 0x000000000000-0x000000080000 : "ospi.tiboot3"                  

[    1.308099] 0x000000080000-0x000000280000 : "ospi.tispl"                    

[    1.313834] 0x000000280000-0x000000680000 : "ospi.u-boot"                   

[    1.319697] 0x000000680000-0x0000006c0000 : "ospi.env"                      

[    1.325262] 0x0000006c0000-0x000000700000 : "ospi.env.backup"               

[    1.331470] 0x000000800000-0x000003fc0000 : "ospi.rootfs"                   

[    1.337281] 0x000003fc0000-0x000004000000 : "ospi.phypattern"               

[    1.348754] spi-nor spi1.0: mt25qu512a (65536 Kbytes)                       

[    1.360348] mmc0: Command Queue Engine enabled                              

[    1.364801] mmc0: new HS400 MMC card at address 0001                        

[    1.370073] mmcblk0: mmc0:0001 S0J56X 14.8 GiB                              

[    1.374721] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB             

[    1.380737] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB             

[    1.386748] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (237)

[    1.392778] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 0

[    1.395064]  mmcblk0: p1 p2                                                 

[    1.401686] libphy: 46000f00.mdio: probed                                   

[    1.409789] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, dri7

[    1.418107] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss ve0

[    1.431366] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48       

[    1.438200] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 14

[    1.445415] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64             

[    1.451756] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:50000

[    1.462328] mmc1: CQHCI version 5.10                                        

[    1.469014] ALSA device list:                                                

[    1.471973]   No soundcards found.                                          

[    1.513424] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 6t

[    1.521291] Waiting for root device PARTUUID=2dca5157-02...                 

[    1.577467] mmc1: new ultra high speed DDR50 SDXC card at address aaaa      

[    1.584334] mmcblk1: mmc1:aaaa SN64G 59.5 GiB                               

[    1.591411]  mmcblk1: p1 p2                                                 

[    1.816668] EXT4-fs (mmcblk1p2): recovery complete                          

[    1.822378] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode.)

[    1.830500] VFS: Mounted root (ext4 filesystem) on device 179:98.           

[    1.840632] devtmpfs: mounted                                               

[    1.843889] Freeing unused kernel memory: 1856K                             

[    1.848455] Run /sbin/init as init process                                  

[    2.019267] systemd[1]: System time before build time, advancing clock.     

[    2.075227] NET: Registered protocol family 10                              

[    2.080207] Segment Routing with IPv6                                       

[    2.097386] systemd[1]: systemd 244.5+ running in system mode.(+PAM -AUDIT )

[    2.119156] systemd[1]: Detected architecture arm64.                        

                                                                               

Welcome to Arago 2021.09!                                                       

                                                                               

[    2.161407] systemd[1]: Set hostname to <j721s2-evm>.                       

[    2.343985] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= r.

[    2.420579] random: systemd: uninitialized urandom read (16 bytes read)     

[    2.427335] systemd[1]: system-getty.slice: unit configures an IP firewall, .

[    2.439663] systemd[1]: (This warning is only shown for the first unit using)

[    2.449743] systemd[1]: Created slice system-getty.slice.                   

[  OK  ] Created slice system-getty.slice.                                     

[    2.472851] random: systemd: uninitialized urandom read (16 bytes read)     

[    2.480184] systemd[1]: Created slice system-serial\x2dgetty.slice.         

[  OK  ] Created slice system-serial\x2dgetty.slice.                           

[    2.500837] random: systemd: uninitialized urandom read (16 bytes read)     

[    2.508120] systemd[1]: Created slice system-syslog\x2dng.slice.            

[  OK  ] Created slice system-syslog\x2dng.slice.                              

[    2.529549] systemd[1]: Created slice User and Session Slice.               

[  OK  ] Created slice User and Session Slice.                                 

[    2.552978] systemd[1]: Started Dispatch Password Requests to Console Direct.

[  OK  ] Started Dispatch Password �…ts to Console Directory Watch.            

[    2.576886] systemd[1]: Started Forward Password Requests to Wall Directory .

[  OK  ] Started Forward Password R�…uests to Wall Directory Watch.            

[    2.600893] systemd[1]: Reached target Paths.                               

[  OK  ] Reached target Paths.                                                 

[    2.620816] systemd[1]: Reached target Remote File Systems.                 

[  OK  ] Reached target Remote File Systems.                                   

[    2.640809] systemd[1]: Reached target Slices.                              

[  OK  ] Reached target Slices.                                                

[    2.660814] systemd[1]: Reached target Swap.                                

[  OK  ] Reached target Swap.                                                   

[    2.682360] systemd[1]: Listening on RPCbind Server Activation Socket.      

[  OK  ] Listening on RPCbind Server Activation Socket.                        

[    2.704847] systemd[1]: Reached target RPC Port Mapper.                      

[  OK  ] Reached target RPC Port Mapper.                                       

[    2.727148] systemd[1]: Listening on Process Core Dump Socket.              

[  OK  ] Listening on Process Core Dump Socket.                                 

[    2.748965] systemd[1]: Listening on initctl Compatibility Named Pipe.      

[  OK  ] Listening on initctl Compatibility Named Pipe.                        

[    2.783234] systemd[1]: Condition check resulted in Journal Audit Socket bei.

[    2.791630] systemd[1]: Listening on Journal Socket (/dev/log).             

[  OK  ] Listening on Journal Socket (/dev/log).                               

[    2.813128] systemd[1]: Listening on Journal Socket.                        

[  OK  ] Listening on Journal Socket.                                          

[    2.829158] systemd[1]: Listening on Network Service Netlink Socket.        

[  OK  ] Listening on Network Service Netlink Socket.                          

[    2.853054] systemd[1]: Listening on udev Control Socket.                   

[  OK  ] Listening on udev Control Socket.                                     

[    2.872942] systemd[1]: Listening on udev Kernel Socket.                    

[  OK  ] Listening on udev Kernel Socket.                                      

[    2.895861] systemd[1]: Mounting Huge Pages File System...                  

         Mounting Huge Pages File System...                                    

[    2.915438] systemd[1]: Mounting POSIX Message Queue File System...         

         Mounting POSIX Message Queue File System...                           

[    2.939618] systemd[1]: Mounting Kernel Debug File System...                

         Mounting Kernel Debug File System...                                   

[    2.963955] systemd[1]: Mounting Temporary Directory (/tmp)...              

         Mounting Temporary Directory (/tmp)...                                

[    2.983730] systemd[1]: Starting Create list of static device nodes for the .

         Starting Create list of st�…odes for the current kernel...            

[    3.012127] systemd[1]: Starting RPC Bind...                                

         Starting RPC Bind...                                                  

[    3.024932] systemd[1]: Condition check resulted in File System Check on Roo.

[    3.037205] systemd[1]: Starting Journal Service...                         

         Starting Journal Service...                                           

[    3.057023] systemd[1]: Starting Load Kernel Modules...                     

         Starting Load Kernel Modules...                                       

[    3.075365] systemd[1]: Starting Remount Root and Kernel File Systems...    

         Starting Remount Root and Kernel File Systems   3.082614] cryptodev: l.

[0m...                                                                         

[    3.090424] EXT4-fs (mmcblk1p2): re-mounted.Opts: (null)                   

[    3.104088] cryptodev: driver 1.10 loaded.                                  

[    3.105350] systemd[1]: Starting udev Coldplug all Devices...               

         Starting udev Coldplug all Devices...                                 

[    3.127532] systemd[1]: Started RPC Bind.                                   

[  OK  ] Started RPC Bind.                                                     

[    3.141175] systemd[1]: Started Journal Service.                            

[  OK  ] Started Journal Service.                                               

[  OK  ] Mounted Huge Pages File System.                                       

[  OK  ] Mounted POSIX Message Queue File System.                              

[  OK  ] Mounted Kernel Debug File System.                                      

[  OK  ] Mounted Temporary Directory (/tmp).                                   

[  OK  ] Started Create list of sta�… nodes for the current kernel.            

[  OK  ] Started Load Kernel Modules.                                          

[  OK  ] Started Remount Root and Kernel File Systems.                         

         Mounting Kernel Configuration File System...                          

         Starting Flush Journal to Persistent Storage...                       

         Starting Apply Kernel Variables...                                    

[    3.311740] systemd-journald[152]: Received client request to flush runtime .

         Starting Create Static Device Nodes in /dev...                        

[  OK  ] Mounted Kernel Configuration File System.                             

[  OK  ] Started Flush Journal to Persistent Storage.                          

[  OK  ] Started Apply Kernel Variables.                                       

[  OK  ] Started Create Static Device Nodes in /dev.                           

[  OK  ] Started udev Coldplug all Devices.                                    

[  OK  ] Reached target Local File Systems (Pre).                              

         Mounting /media/ram...                                                 

         Mounting /var/volatile...                                             

         Starting udev Wait for Complete Device Initialization...              

         Starting udev Kernel Device Manager...                                 

[  OK  ] Mounted /media/ram.                                                   

[  OK  ] Mounted /var/volatile.                                                

         Starting Load/Save Random Seed...                                     

[  OK  ] Reached target Local File Systems.                                    

         Starting Create Volatile Files and Directories...                     

[  OK  ] Started Create Volatile Files and Directories.                        

[  OK  ] Started udev Kernel Device Manager.                                   

         Starting Network Time Synchronization...                              

         Starting Update UTMP about System Boot/Shutdown...                    

[  OK  ] Started Update UTMP about System Boot/Shutdown.                       

[  OK  ] Started Network Time Synchronization.                                 

[  OK  ] Reached target System Time Set.                                       

[  OK  ] Reached target System Time Synchronized.                              

[    3.830115] CAN device driver interface                                     

[    3.863247] k3-dsp-rproc 64800000.dsp: assigned reserved memory node vision-0

[    3.877386] wave5: module is from the staging directory, the quality is unkn.

[    3.886728] k3-dsp-rproc 64800000.dsp: configured DSP for IPC-only mode     

[    3.909238] remoteproc remoteproc0: 64800000.dsp is available               

[    3.996743] remoteproc remoteproc0: attaching to 64800000.dsp               

[    4.007209] remoteproc remoteproc0: unsupported resource 65538              

[    4.024924] k3-dsp-rproc 64800000.dsp: DSP initialized in IPC-only mode     

[    4.051972] vdec 4210000.video-codec:                                        

[    4.051972] _vpu INIT start!!!                                              

[    4.060378] vdec 4210000.video-codec: enum product_id : 00000000            

[    4.066478]  remoteproc0#vdev0buffer: assigned reserved memory node vision-a0

[    4.076203] vdec 4210000.video-codec: fw_version : 00000000(r227733)        

[    4.112643] platform 41000000.r5f: R5F core may have been powered on by a di)

[    4.129678] virtio_rpmsg_bus virtio0: rpmsg host is online                   

[    4.135267] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd

[    4.154273]  remoteproc0#vdev0buffer: registered virtio0 (type 7)           

[    4.160489] remoteproc remoteproc0: remote processor 64800000.dsp is now attd

[    4.168936] platform 41000000.r5f: configured R5F for IPC-only mode         

[    4.177379] platform 41000000.r5f: assigned reserved memory node vision-apps0

[    4.187603] k3-dsp-rproc 65800000.dsp: assigned reserved memory node vision-0

[    4.197844] k3-dsp-rproc 65800000.dsp: configured DSP for IPC-only mode     

[    4.201368] remoteproc remoteproc1: 41000000.r5f is available               

[    4.204528] remoteproc remoteproc2: 65800000.dsp is available               

[    4.217872] remoteproc remoteproc2: attaching to 65800000.dsp               

[    4.223801] remoteproc remoteproc2: unsupported resource 65538              

[    4.229737] k3-dsp-rproc 65800000.dsp: DSP initialized in IPC-only mode     

[    4.236364]  remoteproc2#vdev0buffer: assigned reserved memory node vision-a0

[    4.265123] virtio_rpmsg_bus virtio1: rpmsg host is online                  

[    4.272968]  remoteproc2#vdev0buffer: registered virtio1 (type 7)           

[    4.281188] remoteproc remoteproc2: remote processor 65800000.dsp is now attd

[    4.342285] remoteproc remoteproc1: attaching to 41000000.r5f               

[    4.361177] platform 41000000.r5f: R5F core initialized in IPC-only mode    

[    4.373714]  remoteproc1#vdev0buffer: assigned reserved memory node vision-a0

[    4.395551] virtio_rpmsg_bus virtio2: rpmsg host is online                  

[    4.407702]  remoteproc1#vdev0buffer: registered virtio2 (type 7)           

[    4.413904] virtio_rpmsg_bus virtio2: creating channel ti.ipc4.ping-pong addd

[    4.424112] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xe

[    4.434153] remoteproc remoteproc1: remote processor 41000000.r5f is now attd

[    4.465286] m_can_platform 26a1000.can: m_can device registered (irq=36, ver)

[    4.479179] m_can_platform 2731000.can: m_can device registered (irq=32, ver)

[    4.495699] m_can_platform 40528000.can: m_can device registered (irq=19, ve)

[    4.511189] m_can_platform 2751000.can: m_can device registered (irq=34, ver)

[    4.522338] m_can_platform 40568000.can: m_can device registered (irq=21, ve)

[    4.572818] platform 5c00000.r5f: configured R5F for IPC-only mode          

[    4.579207] platform 5c00000.r5f: assigned reserved memory node vision-apps-0

[    4.588547] remoteproc remoteproc3: 5c00000.r5f is available                

[    4.594346] remoteproc remoteproc3: attaching to 5c00000.r5f                

[    4.600285] platform 5c00000.r5f: R5F core initialized in IPC-only mode     

[    4.607052]  remoteproc3#vdev0buffer: assigned reserved memory node vision-a0

[    4.616989] virtio_rpmsg_bus virtio3: rpmsg host is online                  

[    4.622826]  remoteproc3#vdev0buffer: registered virtio3 (type 7)           

[    4.628985] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xd

[    4.636846] remoteproc remoteproc3: remote processor 5c00000.r5f is now attad

[    4.870796] platform 5d00000.r5f: configured R5F for IPC-only mode          

[    4.883976] platform 5d00000.r5f: assigned reserved memory node vision-apps-0

[    4.893573] remoteproc remoteproc4: 5d00000.r5f is available                

[    4.899537] remoteproc remoteproc4: attaching to 5d00000.r5f                

[    4.907706] platform 5d00000.r5f: R5F core initialized in IPC-only mode     

[    4.914610]  remoteproc4#vdev0buffer: assigned reserved memory node vision-a0

[    4.927618] virtio_rpmsg_bus virtio4: rpmsg host is online                  

[    4.935756]  remoteproc4#vdev0buffer: registered virtio4 (type 7)            

[    4.944401] remoteproc remoteproc4: remote processor 5d00000.r5f is now attad

[    4.957288] platform 5e00000.r5f: configured R5F for remoteproc mode        

[    4.966551] platform 5e00000.r5f: assigned reserved memory node vision-apps-0

[    4.977995] remoteproc remoteproc5: 5e00000.r5f is available                

[    4.988855] remoteproc remoteproc5: Direct firmware load for j721s2-main-r5f2

[    4.998734] remoteproc remoteproc5: powering up 5e00000.r5f                 

[    5.005144] platform 5f00000.r5f: configured R5F for remoteproc mode        

[    5.011616] remoteproc remoteproc5: Direct firmware load for j721s2-main-r5f2

[    5.021059] remoteproc remoteproc5: request_firmware failed: -2             

[    5.031316] platform 5f00000.r5f: assigned reserved memory node vision-apps-0

[    5.049853] remoteproc remoteproc6: 5f00000.r5f is available                

[    5.063125] remoteproc remoteproc6: Direct firmware load for j721s2-main-r5f2

[    5.072562] remoteproc remoteproc6: powering up 5f00000.r5f                 

[    5.079804] remoteproc remoteproc6: Direct firmware load for j721s2-main-r5f2

[    5.089214] remoteproc remoteproc6: request_firmware failed: -2             

[    5.836796] random: crng init done                                          

[    5.840195] random: 7 urandom warning(s) missed due to ratelimiting         

[  OK  ] Started Load/Save Random Seed.                                        

[    6.238809] usbcore: registered new interface driver usbfs                  

[  OK  ] Created slice system-systemd\x2dfsc[    6.319339] usbcore: registered b

k.slice.                                                                       

[    6.460999] usbcore: registered new device driver usb                       

[  OK  ] Found device /dev/mmcblk0p2.                                          

[  OK  ] Found device /dev/mmcblk1p1.                                          

[  OK  ] Started udev Wait for Complete Device Initialization.                 

[  OK  ] Found device /dev/mmcblk0p1.                                          

[  OK  ] Started Hardware RNG Entropy Gatherer Daemon.                         

[  OK  ] Reached target System Initialization.                                 

[  OK  ] Started Daily rotation of log files.                                  

[  OK  ] Started Daily Cleanup of Temporary Directories.                       

[  OK  ] Reached target Timers.                                                 

[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.               

[  OK  ] Listening on D-Bus System Message Bus Socket.                         

         Starting Docker Socket for the API.                                    

[  OK  ] Listening on dropbear.socket.                                         

         Starting Reboot and dump vmcore via kexec...                          

         Starting File System Check on /dev/mmcblk0p1...                        

         Starting File System Check on /dev/mmcblk0p2...                       

         Starting File System Check on /dev/mmcblk1p1...                       

[  OK  ] Listening on Docker Socket for the API.                               

[  OK  ] Started Reboot and dump vmcore via kexec.                             

[  OK  ] Reached target Sockets.                                               

[  OK  ] Reached target Basic System.                                           

[  OK  ] Started Job spooling tools.                                           

[  OK  ] Started Periodic Command Scheduler.                                   

[  OK  ] Started D-Bus System Message Bus.                                      

         Starting Ethernet Bridge Filtering Tables...                          

         Starting Print notice about GPLv3 packages...                         

         Starting IPv6 Packet Filtering Framework...                           

         Starting IPv4 Packet Filtering Framework...                           

[  OK  ] Started irqbalance daemon.                                            

         Starting Telephony service...                                         

         Starting System Logger Daemon "default" instance...                   

         Starting Login Service...                                             

         Starting telnetd.service...                                           

[  OK  ] Started IPv6 Packet Filtering Framework.                              

[  OK  ] Started IPv4 Packet Filtering Framework.                              

[  OK  ] Reached target Network (Pre).                                         

         Starting Network Service...                                            

[    7.310860] TI DP83867 46000f00.mdio:00: attached PHY driver [TI DP83867] (m)

[  OK  ] Started Network Service.                                              

[  OK  ] Started File System Check on /dev/m[    7.342708] am65-cpsw-nuss 46000n

mcblk0p1.                                                                      

[  OK  ] Started File System Check on /dev/mmcblk0p2.                          

[  OK  ] Started File System Check on /dev/mmcblk1p1.                           

[  OK  ] Started Ethernet Bridge Filtering Tables.                             

[  OK  ] Started telnetd.service.                                              

[  OK  ] Started Telephony service.                                            

         Mounting /run/media/mmcblk0p1...                                      

         Mounting /run/media/mmcblk0p2...                                      

         Mounting /run/media/mmcblk1p1...                                      

         Starting syslog.service...                                            

         Starting Wait for Network to be Configured...                         

         Starting Network Name Resoluti[    7.409515] Bluetooth: Core ver 2.22 

on...                                                                           

[    7.416882] NET: Registered protocol family 31                              

[  OK  ] Listening on Load/Save RF �…itch S[    7.427542] Bluetooth: HCI devic d

tatus /dev/rfkill Watch.                                                        

[    7.445789] Bluetooth: HCI socket layer initialized                         

[    7.455254] Bluetooth: L2CAP socket layer initialized                       

[    7.466108] Bluetooth: SCO socket layer initialized                         

[  OK  ] Mounted /run/media/mmcblk0p1.                                         

[    7.486447] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode.)

[  OK  ] Started System Logger Daemon "default" instance.                       

[  OK  ] Mounted /run/media/mmcblk0p2.                                         

[  OK  ] Mounted /run/media/mmcblk1p1.                                         

[  OK  ] Started syslog.service.                                                

[  OK  ] Started Login Service.                                                

[  OK  ] Started Network Name Resolution.                                      

[  OK  ] Reached target Network.                                               

[  OK  ] Reached target Host and Network Name Lookups.                         

         Starting Avahi mDNS/DNS-SD Stack...                                   

         Starting Enable and configure wl18xx bluetooth stack...               

[  OK  ] Started NFS status monitor for NFSv2/3 locking..                      

         Starting Simple Network Ma�…ent Protocol (SNMP) Daemon....            

         Starting Permit User Sessions...                                      

[  OK  ] Started Vsftpd ftp daemon.                                            

[  OK  ] Started Permit User Sessions.                                         

[  OK  ] Started Getty on tty1.                                                

[  OK  ] Started Serial Getty on ttyS10.                                       

[  OK  ] Reached target Login Prompts.                                         

         Starting Synchronize System and HW clocks...                          

[  OK  ] Started Enable and configure wl18xx bluetooth stack.                  

[FAILED] Failed to start Synchronize System and HW clocks.                     

See 'systemctl status sync-clocks.service' for details.                        

[  OK  ] Started Avahi mDNS/DNS-SD Stack.                                       

[  OK  ] Started Simple Network Man�…ement Protocol (SNMP) Daemon..            

[    8.511598] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xd

***************************************************************                 

***************************************************************                

NOTICE: This file system contains the following GPLv3 packages:                

        autoconf                                                               

        bash-dev                                                               

        bash                                                                   

        bc                                                                      

        binutils                                                               

        cifs-utils                                                             

        coreutils-stdbuf                                                        

        coreutils                                                              

        cpio                                                                   

        cpp-symlinks                                                            

        cpp                                                                    

        dosfstools                                                             

        elfutils                                                               

        g++-symlinks                                                           

        g++                                                                    

        gawk                                                                    

        gcc-symlinks                                                           

        gcc                                                                    

        gdb                                                                     

        gdbserver                                                              

        gettext                                                                

        gstreamer1.0-libav-dev                                                  

        gstreamer1.0-libav                                                     

        gzip                                                                   

        less                                                                    

        libasm1                                                                

        libbfd                                                                 

        libdw1                                                                 

        libelf1                                                                

        libgdbm-compat4                                                        

        libgdbm-dev                                                            

        libgdbm6                                                               

        libgettextlib                                                          

        libgettextsrc                                                          

        libgmp-dev                                                              

        libgmp10                                                               

        libgmpxx4                                                              

        libidn2-0                                                               

        libidn2-dev                                                            

        libmpc3                                                                

        libmpfr6                                                               

        libreadline-dev                                                        

        libreadline8                                                           

        libunistring-dev                                                       

        libunistring2                                                          

        m4-dev                                                                 

        m4                                                                      

        make                                                                   

        nettle-dev                                                             

        nettle                                                                  

        parted                                                                 

        python3-rfc3987                                                        

        python3-strict-rfc3339                                                  

        tar                                                                    

        which                                                                  

        zeromq                                                                  

                                                                               

If you do not wish to distribute GPLv3 components please remove                

the above packages prior to distribution.  This can be done using              

the opkg remove command.  i.e.:                                                

    opkg remove <package>                                                      

Where <package> is the name printed in the list above                          

                                                                                

NOTE: If the package is a dependency of another package you                    

      will be notified of the dependent packages.  You should                  

      use the --force-removal-of-dependent-packages option to                  

      also remove the dependent packages as well                               

***************************************************************                

***************************************************************                

[  OK  ] Started Print notice about GPLv3 packages.                            

                                                                               

 _____                    _____           _         _                          

|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_                        

|     |  _| .'| .| .|  |   __|  _| .| | | -_|  _|  _|                       

|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|                         

              |___|                    |___|                                   

                                                                               

Arago Project http://arago-project.org j721s2-evm ttyS10                       

                                                                               

Arago 2021.09 j721s2-evm ttyS10                                                

                                                                                

j721s2-evm login: root                                                         

root@j721s2-evm:~#

 

答 4:

您能对代码进行一些小改动,然后再尝试一下吗? 

在 ti-processor-sdk-rtos-j721s2-evm-08_00_03_05\vision_apps\utils\dss\src\app_dss_soc.c 文件中,您能否按照下面所示更改 appDssConfigureDP API,重新编译 SDK 并尝试 eDP 显示?

void appDssConfigureDP(void)
{
#if defined (SOC_J721E) || defined (SOC_J721S2)
    Board_STATUS b_status;
    Board_IoExpCfg_t ioExpCfg;

    appLogPrintf("DSS: Turning on DP_PWR pin for eDP adapters ...!!!\n");

    #if defined (SOC_J721S2)
    ioExpCfg.i2cInst = 4U;
    #else
    ioExpCfg.i2cInst = 1U;
    #endif
    ioExpCfg.socDomain = BOARD_SOC_DOMAIN_MAIN;
    ioExpCfg.slaveAddr = 0x20;
    ioExpCfg.enableIntr = false;
    ioExpCfg.ioExpType = ONE_PORT_IOEXP;
    ioExpCfg.portNum = PORTNUM_0;
    ioExpCfg.pinNum = PIN_NUM_0;
    ioExpCfg.signalLevel = GPIO_SIGNAL_LEVEL_HIGH;

    b_status = Board_control(BOARD_CTRL_CMD_SET_IO_EXP_PIN_OUT, (void *)(&ioExpCfg));

    if (b_status == BOARD_SOK)
    {
        appLogPrintf("DSS: Turning on DP_PWR pin for eDP adapters ...Done!!!\n");
    }
    else
    {
        appLogPrintf("DSS: ERROR: Turning on DP_PWR pin for eDP adapters failed !!!\n");
    }
#endif
}

 

问题 5

 我应用了您的补丁,但仍然会出现这个问题。您有没有其他方法来确认显示驱动器一切正常?

5

您是在进行上述更改后重新编译 SDK 了吗?因为完成上述更改后需要重新编译 SDK。

如果仍然不起作用,那么您是否确定所使用的显示支持标准 1080p 信号?您能检查一下吗?

 

问题 6

我按照以下步骤在 SDK 中应用您的补丁:

  1. 在 ti-processor-sdk-rtos-j721s2-evm-08_00_03_05/vision_apps/ 中创建 vision_apps -j4;
  2. 在 ti-processor-sdk-rtos-j721s2-evm-08_00_03_05/vision_apps/ 中创建 linux_fs_install_sd;
  3. 按 SD 卡模式引导 EVM;但显示器不显示任何内容。

我的操作有什么错误吗?

 我还将子板和 SD 卡连接到其他主板来测试此问题,结果是一样的。您需要一些关于这个问题的日志吗?

 

6

我看不出导致失败的任何其他原因。您使用的显示设备是否支持 1080p 分辨率?如果可能的话,您能否将显示设备连接到笔记本电脑,读取 EDID 并检查它是否支持 1080p 分辨率? 

问题 7

显示器支持 1080p 分辨率,我的笔记本电脑可以连接它并正常工作。

问题 8

我检查了一些配置文件,我不确定 app_cfg_mcu2_0.h 是否更改正确,能将您工程中的这个文件分享给我吗?谢谢!

8

当然可以,您可以尝试使用随附的文件、重新编译 SDK,再试一次吗?

/cfs-file/__key/communityserver-discussions-components-files/791/app_5F00_cfg_5F00_mcu2_5F00_0.h