TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: ETHERNET提示已经连接,但是无法获取IP,数据也抓取不到

Part Number: PROCESSOR-SDK-AM335X

你好,

 最近在AM335X的SDK上遇到了ETHERNET问题,可以看到连接或者断开的,但是无法获取IP,wireshark 也抓取不到DHCP发送的数据包.

同一个HW上,我使用之前的kernel 4.4.41,测试就没有问题,所以可以排除板子跟ROOT FS的问题

kernel 版本 5.10.100

相关的log和dts

[ 2.624868] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 2.635414] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver SMSC LAN8710/LAN8720
[ 2.645350] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 2.651747] cpsw 4a100000.ethernet: ALE Table size 1024
[ 2.657199] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 2.664432] cpsw 4a100000.ethernet: Detected MACID = 68:c9:0b:f0:17:24
[ 2.674519] am335x-phy-driver 47401300.usb-phy: supply vcc not found, using dummy regulator
[ 2.696014] am335x-phy-driver 47401b00.usb-phy: supply vcc not found, using dummy regulator

Starting network: [ 6.665106] cpsw 4a100000.ethernet: initializing cpsw version 1.12 (0)
[ 6.776572] cpsw 4a100000.ethernet: phy found:phy_id 0x7c0f1,on slave 0
[ 6.783302] SMSC LAN8710/LAN8720 4a101000.mdio:01: attached PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=4a101000.mdio:01, irq=POLL)
[ 6.815468] libphy: PHY not found
[ 6.820529] cpsw 4a100000.ethernet: phy "" not found on slave 1, err -19
udhcpc: started, v1.35.0
udhcpc: broadcasting discover
[ 8.925676] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off
[ 8.933788] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
udhcpc: no lease, forking to background
OK

DTS:

cpsw_default: cpsw_default {
pinctrl-single,pins = <
/* Slave 1 */
AM33XX_PADCONF(AM335X_PIN_GPMC_A0, PIN_OUTPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A1, PIN_INPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A2, PIN_OUTPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A3, PIN_OUTPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A4, PIN_OUTPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A5, PIN_OUTPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A6, PIN_INPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A7, PIN_INPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A8, PIN_INPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A9, PIN_INPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A10, PIN_INPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_A11, PIN_INPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_WAIT0, PIN_INPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_WPN, PIN_INPUT_PULLDOWN, MUX_MODE1)
AM33XX_PADCONF(AM335X_PIN_GPMC_BEN1, PIN_INPUT_PULLDOWN, MUX_MODE1)
>;
};

cpsw_sleep: cpsw_sleep {
pinctrl-single,pins = <
/* Slave 1 reset value */
AM33XX_PADCONF(AM335X_PIN_GPMC_A0, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A1, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A2, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A3, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A4, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A5, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A6, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A7, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A8, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A9, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A10, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_A11, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_WAIT0, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_WPN, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_GPMC_BEN1, PIN_INPUT_PULLDOWN, MUX_MODE7)
>;
};

davinci_mdio_default: davinci_mdio_default {
pinctrl-single,pins = <
/* MDIO */
AM33XX_PADCONF(AM335X_PIN_MDIO, PIN_INPUT_PULLUP | SLEWCTRL_FAST, MUX_MODE0)
AM33XX_PADCONF(AM335X_PIN_MDC, PIN_OUTPUT_PULLUP, MUX_MODE0)
>;
};

davinci_mdio_sleep: davinci_mdio_sleep {
pinctrl-single,pins = <
/* MDIO reset value */
AM33XX_PADCONF(AM335X_PIN_MDIO, PIN_INPUT_PULLDOWN, MUX_MODE7)
AM33XX_PADCONF(AM335X_PIN_MDC, PIN_INPUT_PULLDOWN, MUX_MODE7)
>;
};

&mac {
active_slave = <1>;
pinctrl-names = "default";
pinctrl-0 = <&cpsw_default>;
status = "okay";
};

&davinci_mdio {
pinctrl-names = "default";
pinctrl-0 = <&davinci_mdio_default>;
status = "okay";

ethphy1: ethernet-phy@1 {
reg = <1>;
};
};

&cpsw_emac0 {
status = "disabled";
};

&cpsw_emac1 {
/*mac-address = [ 00 12 4E 02 AE 68 ];*/
/*phy-handle = <&ethphy1>;*/
phy_id = <&davinci_mdio>, <1>;
phy-mode = "mii";
status = "okay";
};

root@am335x:~#ifconfig
eth0 Link encap:Ethernet HWaddr 68:C9:0B:F0:17:24
inet6 addr: fe80::6ac9:bff:fef0:1724/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:25 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:5926 (5.7 KiB)

lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

root@am335x:~#ethtool eth0
Settings for eth0:
Supports Wake-on: d
Wake-on: d
Current message level: 0x00000000 (0)

Link detected: yes

root@am335x:~#ethtool -S eth0
NIC statistics:
Good Rx Frames: 0
Broadcast Rx Frames: 0
Multicast Rx Frames: 0
Pause Rx Frames: 0
Rx CRC Errors: 0
Rx Align/Code Errors: 0
Oversize Rx Frames: 0
Rx Jabbers: 0
Undersize (Short) Rx Frames: 0
Rx Fragments: 0
Rx Octets: 0
Good Tx Frames: 0
Broadcast Tx Frames: 0
Multicast Tx Frames: 0
Pause Tx Frames: 0
Deferred Tx Frames: 0
Collisions: 0
Single Collision Tx Frames: 0
Multiple Collision Tx Frames: 0
Excessive Collisions: 0
Late Collisions: 0
Tx Underrun: 0
Carrier Sense Errors: 0
Tx Octets: 0
Rx + Tx 64 Octet Frames: 0
Rx + Tx 65-127 Octet Frames: 0
Rx + Tx 128-255 Octet Frames: 0
Rx + Tx 256-511 Octet Frames: 0
Rx + Tx 512-1023 Octet Frames: 0
Rx + Tx 1024-Up Octet Frames: 0
Net Octets: 0
Rx Start of Frame Overruns: 0
Rx Middle of Frame Overruns: 0
Rx DMA Overruns: 0
Rx DMA chan 0: head_enqueue: 1
Rx DMA chan 0: tail_enqueue: 127
Rx DMA chan 0: pad_enqueue: 0
Rx DMA chan 0: misqueued: 0
Rx DMA chan 0: desc_alloc_fail: 0
Rx DMA chan 0: pad_alloc_fail: 0
Rx DMA chan 0: runt_receive_buf: 0
Rx DMA chan 0: runt_transmit_bu: 0
Rx DMA chan 0: empty_dequeue: 0
Rx DMA chan 0: busy_dequeue: 0
Rx DMA chan 0: good_dequeue: 0
Rx DMA chan 0: requeue: 0
Rx DMA chan 0: teardown_dequeue: 0
Tx DMA chan 0: head_enqueue: 26
Tx DMA chan 0: tail_enqueue: 54
Tx DMA chan 0: pad_enqueue: 0
Tx DMA chan 0: misqueued: 0
Tx DMA chan 0: desc_alloc_fail: 0
Tx DMA chan 0: pad_alloc_fail: 0
Tx DMA chan 0: runt_receive_buf: 0
Tx DMA chan 0: runt_transmit_bu: 0
Tx DMA chan 0: empty_dequeue: 25
Tx DMA chan 0: busy_dequeue: 0
Tx DMA chan 0: good_dequeue: 25
Tx DMA chan 0: requeue: 0
Tx DMA chan 0: teardown_dequeue: 0
root@am335x:~#