TDA4VM:J721EXSKG01EVM开发板
我想要刷写linuxSDK ti-processor-sdk-linux-j7-evm-07_03_00_05-Linux-x86以及RTOS SDK ti-processor-sdk-rtos-j721e-evm-07_03_00_07 这两个SDK
但是当我按着linux SDK 的setup操作,在写ubboot部分的时候遇到了需要连接开发板的提示,可是我串口以及网口都连着开发板,导致我无法继续下去,linux SDK 无法刷写成功。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TDA4VM:J721EXSKG01EVM开发板
我想要刷写linuxSDK ti-processor-sdk-linux-j7-evm-07_03_00_05-Linux-x86以及RTOS SDK ti-processor-sdk-rtos-j721e-evm-07_03_00_07 这两个SDK
但是当我按着linux SDK 的setup操作,在写ubboot部分的时候遇到了需要连接开发板的提示,可是我串口以及网口都连着开发板,导致我无法继续下去,linux SDK 无法刷写成功。
我是按照这个get started运行的。
我想要把linux SDK刷写到SD卡,然后把7.3 的RTOS SDK 刷写进去。
问题处在刷写linx SDK的时候
请看下面e2e工程师的回复。
It seems like /dev/ttyUSB instance is wrong. So can you redo this step with the right ttyUSB instance?
You can not have x at the end.