请问一下,这里的 instruction type为4 cycle,是不是表示执行这条指令时,1条指令占用4个机器周期?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
截图是来自哪个文档?我从文档c66x文档中中获取到关于Four-cycle的解释,是指使用流水线的 E1 到 E4 阶段来完成它们的指令。
操作.

您好,感谢回答。截图来自《TMS320C67x/C67x+ DSP CPU and Instruction Set Reference Guide》3-262
。

对于Four-Cycle Instructions我能不能这么理解,执行该条指令一共需要PG、PS、PW、PR、DP、DC、E1、E2、E3、E4这10个子阶段,每个子阶段消耗1个CPU cycle,所以执行这一条指令所用时间为10个CPU cycle?另外不知道这CPU cycle与时钟周期的倍数关系是如何的?
对于Four-Cycle Instructions我能不能这么理解,执行该条指令一共需要PG、PS、PW、PR、DP、DC、E1、E2、E3、E4这10个子阶段
我理解是这样,我参考了如下帖子:
个子阶段消耗1个CPU cycle,所以执行这一条指令所用时间为10个CPU cycle?另外不知道这CPU cycle与时钟周期的倍数关系是如何的?
是的,CPU cyle就是1/cpu frequency。