U-Boot 2013.01.01-00123-g2830d15-dirty (Dec 24 2014 - 10:02:17)
I2C: ready
DRAM: 512 MiB
WARNING: Caches not enabled
NAND: 256 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - bad CRC, using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
214 bytes read in 4 ms (51.8 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc ...
Running uenvcmd ...
reading uImage
4173984 bytes read in 724 ms (5.5 MiB/s)
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-3.2.0-00244-gcf99001-dirty
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4173920 Bytes = 4 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0-00244-gcf99001-dirty (root@xlj-virtual-machine) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #1 Fri Dec 19 10:58:09 CST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] ------------[ cut here ]------------
[ 0.000000] WARNING: at arch/arm/mach-omap2/clkt_clksel.c:194 omap2_clksel_recalc+0xd8/0x108()
[ 0.000000] clock: Could not find fieldval 0 for clock dpll_core_m6_ck parent dpll_core_x2_ck
[ 0.000000] Modules linked in:
[ 0.000000] Backtrace:
[ 0.000000] [<c00176e8>] (dump_backtrace+0x0/0x114) from [<c05a5334>] (dump_stack+0x20/0x24)
[ 0.000000] r6:000000c2 r5:c002fd6c r4:c07dde80 r3:c08031e0
[ 0.000000] [<c05a5314>] (dump_stack+0x0/0x24) from [<c0042738>] (warn_slowpath_common+0x5c/0x74)
[ 0.000000] [<c00426dc>] (warn_slowpath_common+0x0/0x74) from [<c004280c>] (warn_slowpath_fmt+0x40/0x48)
[ 0.000000] r8:c07e62bc r7:00000001 r6:c05b3468 r5:00000100 r4:c07f45e8
[ 0.000000] r3:00000009
[ 0.000000] [<c00427cc>] (warn_slowpath_fmt+0x0/0x48) from [<c002fd6c>] (omap2_clksel_recalc+0xd8/0x108)
[ 0.000000] r3:00000000 r2:c06dae34
[ 0.000000] [<c002fc94>] (omap2_clksel_recalc+0x0/0x108) from [<c003405c>] (propagate_rate+0x3c/0x5c)
[ 0.000000] r7:c07e62bc r6:c0b9e840 r5:c07f44e8 r4:c07f45e8
[ 0.000000] [<c0034020>] (propagate_rate+0x0/0x5c) from [<c0034068>] (propagate_rate+0x48/0x5c)
[ 0.000000] r5:c07f448c r4:c07f44d4
[ 0.000000] [<c0034020>] (propagate_rate+0x0/0x5c) from [<c0034068>] (propagate_rate+0x48/0x5c)
[ 0.000000] r5:c07f43d4 r4:c07f4478
[ 0.000000] [<c0034020>] (propagate_rate+0x0/0x5c) from [<c0034068>] (propagate_rate+0x48/0x5c)
[ 0.000000] r5:c07f42c0 r4:c07f43c0
[ 0.000000] [<c0034020>] (propagate_rate+0x0/0x5c) from [<c00341e4>] (recalculate_root_clocks+0x48/0x60)
[ 0.000000] r5:c0802334 r4:c07f42ac
[ 0.000000] [<c003419c>] (recalculate_root_clocks+0x0/0x60) from [<c0793a58>] (am33xx_clk_init+0x8c/0xa8)
[ 0.000000] r5:c07f413c r4:c07f413c
[ 0.000000] [<c07939cc>] (am33xx_clk_init+0x0/0xa8) from [<c0793788>] (omap3xxx_clk_init+0xe0/0x324)
[ 0.000000] r5:c087fdbc r4:00003517
[ 0.000000] [<c07936a8>] (omap3xxx_clk_init+0x0/0x324) from [<c078e45c>] (am33xx_init_early+0x3c/0x40)
[ 0.000000] r7:c07e62bc r6:c0b9e840 r5:c087fdbc r4:c07b7dc0
[ 0.000000] [<c078e420>] (am33xx_init_early+0x0/0x40) from [<c078ae04>] (setup_arch+0x700/0x7f0)
[ 0.000000] [<c078a704>] (setup_arch+0x0/0x7f0) from [<c0787574>] (start_kernel+0x78/0x2dc)
[ 0.000000] [<c07874fc>] (start_kernel+0x0/0x2dc) from [<80008040>] (0x80008040)
[ 0.000000] r6:c07b9300 r5:c07de044 r4:10c53c7d
[ 0.000000] ---[ end trace 1b75b31a2719ed1c ]---
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 androidboot.console=ttyO0 mem=256M root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait init=/init ip=off
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 250008k/250008k available, 12136k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0787000 (7676 kB)
[ 0.000000] .init : 0xc0787000 - 0xc07dc000 ( 340 kB)
[ 0.000000] .data : 0xc07dc000 - 0xc08458f0 ( 423 kB)
[ 0.000000] .bss : 0xc0845914 - 0xc099d650 (1376 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000152] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.118957] pid_max: default: 32768 minimum: 301
[ 0.119110] Security Framework initialized
[ 0.119201] Mount-cache hash table entries: 512
[ 0.119659] CPU: Testing write buffer coherency: ok
[ 0.119750] ftrace: allocating 22040 entries in 65 pages
[ 0.192535] omap_hwmod: pruss: failed to hardreset
[ 0.193450] print_constraints: dummy:
[ 0.193725] NET: Registered protocol family 16
[ 0.194946] OMAP GPIO hardware version 0.1
[ 0.196136] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.197357] omap_i2c.1: alias fck already exists
[ 0.197967] omap2_mcspi.1: alias fck already exists
[ 0.198089] omap2_mcspi.2: alias fck already exists
[ 0.198242] edma.0: alias fck already exists
[ 0.198272] edma.0: alias fck already exists
[ 0.198303] edma.0: alias fck already exists
[ 0.209350] bio: create slab <bio-0> at 0
[ 0.210449] SCSI subsystem initialized
[ 0.211395] usbcore: registered new interface driver usbfs
[ 0.211517] usbcore: registered new interface driver hub
[ 0.211669] usbcore: registered new device driver usb
[ 0.212036] registerd cppi-dma Intr @ IRQ 17
[ 0.212036] Cppi41 Init Done Qmgr-base(d087a000) dma-base(d0878000)
[ 0.212036] Cppi41 Init Done
[ 0.212066] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.212249] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.212738] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.213592] tps65910 1-002d: could not be detected
[ 0.214172] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.214813] Bluetooth: Core ver 2.16
[ 0.214904] NET: Registered protocol family 31
[ 0.214904] Bluetooth: HCI device and connection manager initialized
[ 0.214904] Bluetooth: HCI socket layer initialized
[ 0.214935] Bluetooth: L2CAP socket layer initialized
[ 0.214965] Bluetooth: SCO socket layer initialized
[ 0.215179] Switching to clocksource gp timer
[ 0.235137] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.235473] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.235717] MUSB0 controller's USBSS revision = 4ea20800
[ 0.235748] musb0: Enabled SW babble control
[ 0.236724] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using DMA, IRQ 18
[ 0.236999] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.237182] MUSB1 controller's USBSS revision = 4ea20800
[ 0.237213] musb1: Enabled SW babble control
[ 0.237701] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.237823] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.237976] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.238006] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.238006] usb usb1: Product: MUSB HDRC host driver
[ 0.238006] usb usb1: Manufacturer: Linux 3.2.0-00244-gcf99001-dirty musb-hcd
[ 0.238037] usb usb1: SerialNumber: musb-hdrc.1
[ 0.238616] hub 1-0:1.0: USB hub found
[ 0.238647] hub 1-0:1.0: 1 port detected
[ 0.239074] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 using DMA, IRQ 19
[ 0.239501] NET: Registered protocol family 2
[ 0.239715] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.240173] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.240325] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.240417] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.240417] TCP reno registered
[ 0.240447] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.240478] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.240692] NET: Registered protocol family 1
[ 0.241027] RPC: Registered named UNIX socket transport module.
[ 0.241027] RPC: Registered udp transport module.
[ 0.241058] RPC: Registered tcp transport module.
[ 0.241058] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.241363] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.362060] ashmem: initialized
[ 0.362365] VFS: Disk quotas dquot_6.5.2
[ 0.362426] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.363342] fuse init (API version 7.17)
[ 0.363616] msgmni has been set to 488
[ 0.364715] io scheduler noop registered
[ 0.364746] io scheduler deadline registered
[ 0.364837] io scheduler cfq registered (default)
[ 0.365570] Could not set LED4 to fully on
[ 0.366912] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 1.227935] console [ttyO0] enabled
[ 1.232177] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 1.240020] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 1.247772] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 1.255493] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 1.263244] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 1.271240] [drm] Initialized drm 1.1.0 20060810
[ 1.282379] brd: module loaded
[ 1.289093] loop: module loaded
[ 1.292633] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.299224] i2c-core: driver [tsl2550] using legacy resume method
[ 1.305725] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.365905] No daughter card found on AM335x EVM
[ 1.370819] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.380249] The board is a AM335x Starter Kit.
[ 1.385620] omap_hsmmc.0: alias fck already exists
[ 1.391021] omap_hsmmc.1: alias fck already exists
[ 1.396942] sucess to register LCDC device xlj
[ 1.401702] da8xx_lcdc.0: alias fck already exists
[ 1.407104] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
[ 1.427215] davinci-mcasp.1: alias fck already exists
[ 1.432830] am335xevm: bt init
[ 1.436981] _regulator_get: l3_main.0 supply vdd_core not found, using dummy regulator
[ 1.445465] am335x_opp_update: physical regulator not present for core(-22)
[ 1.453094] (stk) :sysfs entries created
[ 1.457336] (stk) : debugfs entries created
[ 1.461700] (hci_tty): inside hci_tty_init
[ 1.466461] (hci_tty): allocated 251, 0
[ 1.470550] _regulator_get: 1-0018 supply Vdd not found, using dummy regulator
[ 1.478240] _regulator_get: 1-0018 supply Vdd_IO not found, using dummy regulator
[ 1.506835] lis3lv02d: unknown sensor type 0x87
[ 1.511688] lis3lv02d_i2c: probe of 1-0018 failed with error -22
[ 1.518707] NFC Driver for TI WiLink
[ 1.523284] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.530517] omap2-nand driver initializing
[ 1.534912] OneNAND driver initializing
[ 1.539520] CAN device driver interface
[ 1.543579] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.595886] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.602416] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[ 1.609375] usb 1-1: new high-speed USB device number 2 using musb-hdrc
[ 1.617279] davinci_mdio.0: probed
[ 1.620880] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[ 1.628448] PPP generic driver version 2.4.2
[ 1.633148] PPP BSD Compression module registered
[ 1.638153] PPP Deflate Compression module registered
[ 1.643615] usbcore: registered new interface driver cdc_ether
[ 1.649871] usbcore: registered new interface driver cdc_eem
[ 1.655914] usbcore: registered new interface driver dm9601
[ 1.661834] usbcore: registered new interface driver cdc_subset
[ 1.668151] cdc_ncm: 04-Aug-2011
[ 1.671630] usbcore: registered new interface driver cdc_ncm
[ 1.677734] usbcore: registered new interface driver cdc_acm
[ 1.683715] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 1.692169] Initializing USB Mass Storage driver...
[ 1.697479] usbcore: registered new interface driver usb-storage
[ 1.703796] USB Mass Storage support registered.
[ 1.708862] usbcore: registered new interface driver usbserial
[ 1.715087] USB Serial support registered for generic
[ 1.856109] usb 1-1: New USB device found, idVendor=0424, idProduct=2514
[ 1.863189] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 1.871398] hub 1-1:1.0: USB hub found
[ 1.875427] hub 1-1:1.0: 4 ports detected
[ 1.880615] usbcore: registered new interface driver usbserial_generic
[ 1.887542] usbserial: USB Serial Driver core
[ 1.892211] USB Serial support registered for GSM modem (1-port)
[ 1.898803] usbcore: registered new interface driver option
[ 1.904663] option: v0.7.2:USB Driver for GSM modems
[ 1.911773] gadget: Mass Storage Function, version: 2009/09/11
[ 1.918090] gadget: Number of LUNs=1
[ 1.921966] lun0: LUN: removable file: (no medium)
[ 1.927368] gadget: android_usb ready
[ 1.931335] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 1.937042] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 1.944976] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 1.952178] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.959808] usb usb2: Product: MUSB HDRC host driver
[ 1.965026] usb usb2: Manufacturer: Linux 3.2.0-00244-gcf99001-dirty musb-hcd
[ 1.972595] usb usb2: SerialNumber: musb-hdrc.0
[ 1.977905] hub 2-0:1.0: USB hub found
[ 1.981872] hub 2-0:1.0: 1 port detected
[ 1.986907] mousedev: PS/2 mouse device common for all mice
[ 1.993652] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input0
[ 2.002441] using rtc device, am33xx-rtc, for alarms
[ 2.007598] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[ 2.014984] i2c /dev entries driver
[ 2.018920] Linux video capture interface: v2.00
[ 2.024139] usbcore: registered new interface driver uvcvideo
[ 2.030242] USB Video Class driver (1.1.1)
[ 2.036651] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 2.043304] device-mapper: uevent: version 1.0.3
[ 2.048461] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com
[ 2.057403] Bluetooth: HCI UART driver ver 2.2
[ 2.062103] Bluetooth: HCI H4 protocol initialized
[ 2.067169] Bluetooth: HCILL protocol initialized
[ 2.072143] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0
[ 2.079620] _regulator_get: deviceless supply vdd_mpu not found, using dummy regulator
[ 2.088287] cpuidle: using governor ladder
[ 2.092773] cpuidle: using governor menu
[ 2.101867] usbcore: registered new interface driver usbhid
[ 2.107818] usbhid: USB HID core driver
[ 2.112457] logger: created 256K log 'log_main'
[ 2.117401] logger: created 256K log 'log_events'
[ 2.122467] logger: created 256K log 'log_radio'
[ 2.127502] logger: created 256K log 'log_system'
[ 2.133117] tiadc tiadc: attached adc driver
[ 2.138122] usbcore: registered new interface driver snd-usb-audio
[ 2.146026] _regulator_get: 1-001b supply IOVDD not found, using dummy regulator
[ 2.153930] _regulator_get: 1-001b supply DVDD not found, using dummy regulator
[ 2.161712] _regulator_get: 1-001b supply AVDD not found, using dummy regulator
[ 2.169494] _regulator_get: 1-001b supply DRVDD not found, using dummy regulator
[ 2.285705] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok
[ 2.293060] ALSA device list:
[ 2.296234] #0: AM335X EVM
[ 2.299285] oprofile: hardware counters not available
[ 2.304626] oprofile: using timer interrupt.
[ 2.309356] Netfilter messages via NETLINK v0.30.
[ 2.314483] nf_conntrack version 0.5.0 (3906 buckets, 15624 max)
[ 2.321228] ctnetlink v0.93: registering with nfnetlink.
[ 2.326965] NF_TPROXY: Transparent proxy support initialized, version 4.1.0
[ 2.334289] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
[ 2.340850] xt_time: kernel timezone is -0000
[ 2.345703] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 2.351593] arp_tables: (C) 2002 David S. Miller
[ 2.356567] TCP cubic registered
[ 2.360168] NET: Registered protocol family 10
[ 2.365722] Mobile IPv6
[ 2.368408] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 2.374328] IPv6 over IPv4 tunneling driver
[ 2.379455] NET: Registered protocol family 17
[ 2.384216] NET: Registered protocol family 15
[ 2.388946] can: controller area network core (rev 20090105 abi 8)
[ 2.395629] NET: Registered protocol family 29
[ 2.400329] can: raw protocol (rev 20090105)
[ 2.404846] can: broadcast manager protocol (rev 20090105 t)
[ 2.411102] Bluetooth: RFCOMM TTY layer initialized
[ 2.416320] Bluetooth: RFCOMM socket layer initialized
[ 2.421752] Bluetooth: RFCOMM ver 1.11
[ 2.425720] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.431335] Bluetooth: BNEP filters: protocol multicast
[ 2.436889] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.443298] Registering the dns_resolver key type
[ 2.448394] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 2.456512] ThumbEE CPU extension supported.
[ 2.461120] mux: Failed to setup hwmod io irq -22
[ 2.466888] Power Management for AM33XX family
[ 2.471832] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 2.478759] Copied the M3 firmware to UMEM
[ 2.483215] Cortex M3 Firmware Version = 0x181
[ 2.492889] clock: disabling unused clocks to save power
[ 2.500366] Detected MACID=1c:ba:8c:af:19:13
[ 2.507537] input: gpio-keys as /devices/platform/gpio-keys/input/input1
[ 2.515014] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[ 2.524688] Waiting for root device /dev/mmcblk0p2...
[ 2.566925] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 2.577575] mmc0: new high speed SDHC card at address 1234
[ 2.583923] mmcblk0: mmc0:1234 SA04G 3.63 GiB
[ 2.590911] mmcblk0: p1 p2 p3 p4
[ 3.276184] (stk) :line disc installation timed out
[ 5.396453] (stk) :line disc installation timed out
[ 6.538879] EXT4-fs (mmcblk0p2): recovery complete
[ 6.547363] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 6.555999] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 6.562988] Freeing init memory: 340K
[ 6.596832] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
[ 6.690673] init: cannot open '/initlogo.rle'
[ 7.516784] (stk) :line disc installation timed out
[ 9.637054] (stk) :line disc installation timed out
[ 11.458374] EXT4-fs (mmcblk0p3): recovery complete
[ 11.468139] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,errors=panic
[ 11.521545] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
[ 11.543792] android_usb: already disabled
[ 11.557769] android_usb: already disabled
[ 11.563720] android_usb: already disabled
[ 11.570617] adb_bind_config
[ 11.575897] adb_bind_config
[ 11.757080] (stk) :line disc installation timed out
[ 12.670349] adb_open
[ 12.980560] Disabling lock debugging due to kernel taint
[ 13.155853] warning: `rild' uses 32-bit capabilities (legacy support in use)
[ 13.877075] (stk) :line disc installation timed out
[ 14.877197] Bluetooth: st_register failed -22
root@android:/ # [ 19.786346] init: untracked pid 73 exited
[ 59.424438] request_suspend_state: wakeup (3->0) at 59377345328 (2000-01-01 00:00:57.391623779 UTC)
[ 60.213531] net eth0: CPSW phy found : id is : 0x4dd074
[ 60.219940] PHY 0:01 not found
[ 60.247344] ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 60.850128] acc_open
[ 60.852478] acc_release
[ 86.149749] init: sys_prop: permission denied uid:1003 name:service.bootanim.exit
以上为串口消息,求指点下,如何加快启动速度。这速度没法忍了、