This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 6.1 单步执行按钮呈现灰色

Other Parts Discussed in Thread: ENERGYTRACE

如题

我是新下载安装的CCSV6.1,安装后自己新建了一个只有几行代码的小测试工程。芯片是C6748,编译器C6000,仿真器用的是XDS 100V2,XDS560PLUS两种。遇到了仿真器挂载后单步执行的按钮呈灰色。请问这是什么原因?

  • 截个屏上来吧,看看具体是什么情况。

  • 点右上角的CCS_Debug试试

  • 试过了,没用的

  • 帮我看看这是什么情况啊

  • CCS V5.5,和CCS V6.1,哪一个稳定些?之前用的CCS3.3,现在换电脑了直接就升级到最新版本的6.1了。现在仿真器这一步测试那个按钮老是灰色的,该肿么办哦? Tang给个招吧。

  • 这个会和操作系统有关系么?我是64位的win7操作系统

  • 跟系统无关,我就是使用的64bit的win7和ubuntu,都没有问题。

    要不你先降低一下版本试试。

  • 好吧,请问你现在用的是什么版本的?

  • weihua li 说:

    好吧,请问你现在用的是什么版本的?

    我是用的5.5

  • 好吧,我试试

  • 我原来装的6.0.1,现在刚装上6.1,调试界面如下,有单步等按钮,不是灰的。我的也是WIN7 64位系统。

    所以你的问题可能是什么原因呢?会不会是因为CCS License的问题?

  • 经确认,这是CCS6.1的bug, bug ID 是 SDSCM00051770 ,将会在6.1.1修复。

    不过我装的是6.1.0.00104看上去没问题啊。

     

  • 我卸载重新安装了CCS  5.5就好了!

  • 6.1目前有几个版本?我在官网上看见只有6.1.0.00104这一个6.1的版本啊

  • 还有个问题想问一下。CCS5.5在安装的时候回有两个选项

    Custom

    Complete Feature Set

    这两个选项的安装有什么不同?

  • custom是自定义安装,可以选择需要的部件进行安装。

    complete feature set是全部安装。

    很多其它软件安装时也一样的有这种选项的啊。

  • 6.1还没发布,我说的是“将”修复。

    另外,上面那个bug还跟程序相关,程序太简单才会出现那种灰色按钮情况。

  • 那怎么办?就不能用了吗?CCS就可以扔了吗?

  • 什么怎么办?上面的问题已经解决了啊。

  • ccs6.1依然出现了这个问题,不止我一个人

  • 从6.1.2的release notes里看,这个bug修复了,更新到CCS 6.1.2吧。

    http://software-dl.ti.com/ccs/esd/CCSv6/latest/exports/ReleaseNote.htm

    Bug Fixes

    dbid

    Id

    Component

    Headline

    33606192

    SDSCM00051760

    C2000 Code Generation Tools

    Compiler error for missing brace "}" at end of source is not reported in Problems view

    33594903

    SDSCM00040471

    DVT

    Show profile data in call graph

    33606099

    SDSCM00051667

    DVT

    Graph export/import should save/restore autoscale and y-axis range settings.

    33606155

    SDSCM00051723

    DVT

    symbol names not show for EnergyTrace on MSP430

    33606293

    SDSCM00051861

    DVT

    Improve EnergyTrace UI for power graph to clearly show whether measurements are relative or absolute

    33602008

    SDSCM00047576

    IDE

    Unable to generate code coverage data via DSS

    33602046

    SDSCM00047614

    IDE

    Scripting Console: Button to open/load a javascript file

    33602176

    SDSCM00047744

    IDE

    legacy format header files not handled correctly

    33602266

    SDSCM00047834

    IDE

    DS initiated progress dialog should consider the dialog option "Always Run on Background"

    33602278

    SDSCM00047846

    IDE

    Once I start a CCS debug session, build all will popup a modal progress box

    33602500

    SDSCM00048068

    IDE

    [C28 Flash] Flash programming does not work with "Auto Run on Reset" option on

    33602584

    SDSCM00048152

    IDE

    Importing a SYS/BIOS project created with older version of CCS causes migration errors

    33602609

    SDSCM00048177

    IDE

    Scan compiler options files to improve conditional formatting

    33602657

    SDSCM00048225

    IDE

    Flash programming sometimes results in error "Timed out while writing to Flash memory"

    33602680

    SDSCM00048248

    IDE

    Breakpoint on a single source line causes the debugger to break twice before resuming execution

    33602690

    SDSCM00048258

    IDE

    Importing a CCS3.3 library project with project dependencies results in java.lang.NullPointerException

    33602697

    SDSCM00048265

    IDE

    In the compiler selection drop-down the listing for gcc should include the executable name

    33602741

    SDSCM00048309

    IDE

    Missing .ebss and .reset directive highlights for C2000 cmd file

    33602776

    SDSCM00048344

    IDE

    Class members are not shown in Variables view for code built with GCC

    33602789

    SDSCM00048357

    IDE

    MSP430 Trace View does not refresh properly when decoding instructions

    33602816

    SDSCM00048384

    IDE

    Project import tool sometimes does not resolve paths correctly

    33602820

    SDSCM00048388

    IDE

    Provide more precise error messages in Import CCS Project wizard

    33602840

    SDSCM00048408

    IDE

    Switching between two projects can sometime get GUI Composer out of sync

    33602849

    SDSCM00048417

    IDE

    The compiler option -v that specifies the silicon version is retained when switching device variants

    33602878

    SDSCM00048446

    IDE

    Flashing fails on Stellaris TM4C129X devices

    33602894

    SDSCM00048462

    IDE

    Makefile validation errors prevent makefile re-generation

    33602900

    SDSCM00048468

    IDE

    The Location of local variables is sometimes displayed incorrectly for GCC ELF files

    33602985

    SDSCM00048553

    IDE

    Include paths using "workspace_loc: variable are not passed to the compiler if the path does not exist

    33603000

    SDSCM00048568

    IDE

    Request to have LCD option for meter widget

    33603001

    SDSCM00048569

    IDE

    Request to have an out of range indicator option for gauges and meters

    33603044

    SDSCM00048612

    IDE

    CCS fails to program certain .out files when "Auto ECC generation" is enabled in Flash Settings

    33603191

    SDSCM00048759

    IDE

    Deadlock due to "buddy" classloading

    33603338

    SDSCM00048906

    IDE

    Invoking gmake with -s option causes the Problems view to not update after errors have been corrected

    33603350

    SDSCM00048918

    IDE

    Would like a method to disable Optimization Advice

    33603434

    SDSCM00049002

    IDE

    App center in installer shows MSP430 content even when MSP not selected

    33603485

    SDSCM00049053

    IDE

    Request fpr Memory Allocation view to show UNION sections

    33605396

    SDSCM00050964

    IDE

    Hex Utility (and GNU Objcopy in the case of GNU tools) should run before post build steps in CCS

    33605484

    SDSCM00051052

    IDE

    When using SW breakpoints in source file, the LDR instruction does not work correctly on a Cortex-A8 (AM335x)

    33605678

    SDSCM00051246

    IDE

    User is prompted to terminate existing debug session when running a multi-session DSS script from the Console

    33605704

    SDSCM00051272

    IDE

    The CCS Online Help content for "Data File Formats" is outdated

    33605866

    SDSCM00051434

    IDE

    Multiple copies of the same header file are opened when clicking on a error/warning in the Problems view

    33605961

    SDSCM00051529

    IDE

    Debugserver should release files that are opened in the target application when a debug session is terminated

    33606052

    SDSCM00051620

    IDE

    TI-RTOS template project fails to build with GNU build tools

    33606056

    SDSCM00051624

    IDE

    DefaultToolChain property on Device XML files is not being properly acknowledged by the Project wizard

    33606059

    SDSCM00051627

    IDE

    Passing XDCROOT as a parameter to batch file in post build step does not work as expected

    33606063

    SDSCM00051631

    IDE

    CCS crash in a gcc compiled C++ program when expanding a class pointer

    33606075

    SDSCM00051643

    IDE

    Tiva E device support does not get installed

    33606136

    SDSCM00051704

    IDE

    90 day eval license activation is broken

    33606202

    SDSCM00051770

    IDE

    Closing and restarting CCS when in CCS Simple mode causes debugger to no longer work (all debug functions are grayed out)