我使用的是TQ335x开发版,编译TI_Android_JB_4_2_2_DevKit_4_1_1.bin源代码,根据文档“TI-Android-JB-4.2.2-DevKit-4.1.1 DeveloperGuide”操作
u-boot:将EEPROM去掉,选择am335x_evm_config;
kernel:也将EEPROM去掉,并选择am335x_evm_android_defconfig;
android filesystem: make TARGET_PRODUCT=am335xevm OMAPES=4.x -j4
编译之后制作成SD/MMC启动,启动日志如下,现象是LCD屏为白的,没有图片显示,是不是LCD没有驱动起来,要驱动LCD的话,要修改那个地方?
U-Boot SPL 2013.01.01-00123-g2830d15-dirty (Jul 10 2015 - 11:30:30)
hejx debug:enable_board_pin_mux(struct am335x_baseboard_id *header)
hejx debug:8 header.name =
header.name =
header.version =
header.serial =
header.config =
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
OMAP SD/MMC: 0
reading u-boot.img
reading u-boot.img
U-Boot 2013.01.01-00123-g2830d15-dirty (Jul 10 2015 - 11:30:30)
I2C: ready
DRAM: 512 MiB
hejx debug: board_init_r*******************************
WARNING: Caches not enabled
hejx debug: monitor flash len: 000591CC
hejx debug: nand_init*******************************
NAND: hejx debug: nand_init(void)*******************************
hejx debug: nand_init_chip(int i)*******************************
hejx debug:17 board_nand_init(struct nand_chip *nand)*********
hejx debug:test5************************************
hejx debug:elm_init(void)************************************
hejx debug:elm_init************************************
hejx debug:test1************************************
hejx debug: nand_scan(struct mtd_info *mtd, int maxchips)****************
dev_id = 211
hejx debug: if (!ret)**************************************
1024 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - bad CRC, using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
214 bytes read in 11 ms (18.6 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc ...
Running uenvcmd ...
reading uImage
4173736 bytes read in 418 ms (9.5 MiB/s)
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-3.2.0-00244-gcf99001-dirty
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 4173672 Bytes = 4 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0-00244-gcf99001-dirty (root@hejx-Lenovo) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #1 Fri Jul 10 11:42:5
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
[ 0.000000] Kernel command line: console=ttyO0,115200n8 androidboot.console=ttyO0 mem=512M root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait init=/inif
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 512MB = 512MB total
[ 0.000000] Memory: 509904k/509904k available, 14384k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0787000 (7676 kB)
[ 0.000000] .init : 0xc0787000 - 0xc07dc000 ( 340 kB)
[ 0.000000] .data : 0xc07dc000 - 0xc08458f0 ( 423 kB)
[ 0.000000] .bss : 0xc0845914 - 0xc099d650 (1376 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] omap_dm_timer_switch_src: Switching to HW default clocksource(sys_clkin_ck) for timer1, this may impact timekeeping in low power state
[ 0.000000] OMAP clocksource: GPTIMER1 at 24000000 Hz
[ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000182] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.087690] pid_max: default: 32768 minimum: 301
[ 0.087808] Security Framework initialized
[ 0.087865] Mount-cache hash table entries: 512
[ 0.088231] CPU: Testing write buffer coherency: ok
[ 0.088286] ftrace: allocating 22040 entries in 65 pages
[ 0.144423] omap_hwmod: pruss: failed to hardreset
[ 0.145135] print_constraints: dummy:
[ 0.145321] NET: Registered protocol family 16
[ 0.146235] OMAP GPIO hardware version 0.1
[ 0.147094] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.148064] omap_i2c.1: alias fck already exists
[ 0.148504] omap2_mcspi.1: alias fck already exists
[ 0.148590] omap2_mcspi.2: alias fck already exists
[ 0.148704] edma.0: alias fck already exists
[ 0.148718] edma.0: alias fck already exists
[ 0.148731] edma.0: alias fck already exists
[ 0.156546] bio: create slab <bio-0> at 0
[ 0.157370] SCSI subsystem initialized
[ 0.158137] usbcore: registered new interface driver usbfs
[ 0.158234] usbcore: registered new interface driver hub
[ 0.158353] usbcore: registered new device driver usb
[ 0.158624] registerd cppi-dma Intr @ IRQ 17
[ 0.158634] Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000)
[ 0.158642] Cppi41 Init Done
[ 0.158664] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.158789] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.159163] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.160266] tps65910 1-002d: JTAGREVNUM 0x0
[ 0.162376] print_constraints: VRTC:
[ 0.163676] print_constraints: VIO: at 1500 mV
[ 0.165822] print_constraints: VDD1: 600 <--> 1500 mV at 1325 mV normal
[ 0.167956] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[ 0.168821] print_constraints: VDD3: 5000 mV
[ 0.170087] print_constraints: VDIG1: at 1800 mV
[ 0.171375] print_constraints: VDIG2: at 1800 mV
[ 0.172646] print_constraints: VPLL: at 1800 mV
[ 0.173922] print_constraints: VDAC: at 1800 mV
[ 0.175200] print_constraints: VAUX1: at 1800 mV
[ 0.176490] print_constraints: VAUX2: at 3300 mV
[ 0.177763] print_constraints: VAUX33: at 3300 mV
[ 0.179047] print_constraints: VMMC: at 3300 mV
[ 0.179269] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.179735] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.180235] Bluetooth: Core ver 2.16
[ 0.180294] NET: Registered protocol family 31
[ 0.180302] Bluetooth: HCI device and connection manager initialized
[ 0.180314] Bluetooth: HCI socket layer initialized
[ 0.180322] Bluetooth: L2CAP socket layer initialized
[ 0.180356] Bluetooth: SCO socket layer initialized
[ 0.180518] Switching to clocksource gp timer
[ 0.195307] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.195491] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.195652] MUSB0 controller's USBSS revision = 4ea20800
[ 0.195678] musb0: Enabled SW babble control
[ 0.196386] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using DMA, IRQ 18
[ 0.196604] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.196732] MUSB1 controller's USBSS revision = 4ea20800
[ 0.196752] musb1: Enabled SW babble control
[ 0.197119] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.197201] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 0.197319] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.197331] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.197340] usb usb1: Product: MUSB HDRC host driver
[ 0.197349] usb usb1: Manufacturer: Linux 3.2.0-00244-gcf99001-dirty musb-hcd
[ 0.197358] usb usb1: SerialNumber: musb-hdrc.1
[ 0.197765] hub 1-0:1.0: USB hub found
[ 0.197789] hub 1-0:1.0: 1 port detected
[ 0.198132] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using DMA, IRQ 19
[ 0.198442] NET: Registered protocol family 2
[ 0.198621] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.198963] TCP established hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.199179] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.199306] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.199316] TCP reno registered
[ 0.199326] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.199354] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.199522] NET: Registered protocol family 1
[ 0.199764] RPC: Registered named UNIX socket transport module.
[ 0.199774] RPC: Registered udp transport module.
[ 0.199781] RPC: Registered tcp transport module.
[ 0.199787] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.199999] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.295405] ashmem: initialized
[ 0.295624] VFS: Disk quotas dquot_6.5.2
[ 0.295671] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.296380] fuse init (API version 7.17)
[ 0.296574] msgmni has been set to 995
[ 0.297424] io scheduler noop registered
[ 0.297434] io scheduler deadline registered
[ 0.297489] io scheduler cfq registered (default)
[ 0.298000] Could not set LED4 to fully on
[ 0.331175] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 1.038414] console [ttyO0] enabled
[ 1.042504] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 1.050120] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 1.057753] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 1.065527] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 1.073177] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 1.080936] [drm] Initialized drm 1.1.0 20060810
[ 1.090273] brd: module loaded
[ 1.095871] loop: module loaded
[ 1.099309] i2c-core: driver [tsl2550] using legacy suspend method
[ 1.105818] i2c-core: driver [tsl2550] using legacy resume method
[ 1.112252] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.126156] Detected a daughter card on AM335x EVM..
[ 1.131178] Unknown CPLD version found
[ 1.135307] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 1.240548] The board is a AM335x Starter Kit.
[ 1.245711] omap_hsmmc.0: alias fck already exists
[ 1.250981] omap_hsmmc.1: alias fck already exists
[ 1.256669] da8xx_lcdc.0: alias fck already exists
[ 1.261970] da8xx_lcdc da8xx_lcdc.0: GLCD: Found NHD-4.3-ATXI#-T-1 panel
[ 1.277627] davinci-mcasp.1: alias fck already exists
[ 1.283201] am335xevm: bt init
[ 1.288676] (stk) :sysfs entries created
[ 1.292842] (stk) : debugfs entries created
[ 1.297166] (hci_tty): inside hci_tty_init
[ 1.301790] (hci_tty): allocated 251, 0
[ 1.305848] _regulator_get: 1-0018 supply Vdd not found, using dummy regulator
[ 1.313467] _regulator_get: 1-0018 supply Vdd_IO not found, using dummy regulator
[ 1.340594] usb 1-1: new high-speed USB device number 2 using musb-hdrc
[ 1.347742] lis3lv02d: unknown sensor type 0x87
[ 1.352566] lis3lv02d_i2c: probe of 1-0018 failed with error -22
[ 1.359322] NFC Driver for TI WiLink
[ 1.363674] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.370756] omap2-nand driver initializing
[ 1.375081] OneNAND driver initializing
[ 1.379500] CAN device driver interface
[ 1.383536] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.430562] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.437029] davinci_mdio davinci_mdio.0: detected phy mask ffffffde
[ 1.444735] davinci_mdio.0: probed
[ 1.448295] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[ 1.455696] davinci_mdio davinci_mdio.0: phy[5]: device 0:05, driver unknown
[ 1.463114] PPP generic driver version 2.4.2
[ 1.467729] PPP BSD Compression module registered
[ 1.472663] PPP Deflate Compression module registered
[ 1.478045] usbcore: registered new interface driver cdc_ether
[ 1.484198] usbcore: registered new interface driver cdc_eem
[ 1.490149] usbcore: registered new interface driver dm9601
[ 1.496020] usbcore: registered new interface driver cdc_subset
[ 1.502254] cdc_ncm: 04-Aug-2011
[ 1.505665] usbcore: registered new interface driver cdc_ncm
[ 1.511657] usbcore: registered new interface driver cdc_acm
[ 1.517569] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 1.525948] Initializing USB Mass Storage driver...
[ 1.531146] usbcore: registered new interface driver usb-storage
[ 1.537421] USB Mass Storage support registered.
[ 1.542383] usbcore: registered new interface driver usbserial
[ 1.548512] USB Serial support registered for generic
[ 1.570804] usb 1-1: New USB device found, idVendor=1a40, idProduct=0101
[ 1.577816] usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0
[ 1.585288] usb 1-1: Product: USB 2.0 Hub
[ 1.589912] hub 1-1:1.0: USB hub found
[ 1.593916] hub 1-1:1.0: 4 ports detected
[ 1.598693] usbcore: registered new interface driver usbserial_generic
[ 1.605539] usbserial: USB Serial Driver core
[ 1.610131] USB Serial support registered for GSM modem (1-port)
[ 1.616581] usbcore: registered new interface driver option
[ 1.622416] option: v0.7.2:USB Driver for GSM modems
[ 1.628953] gadget: Mass Storage Function, version: 2009/09/11
[ 1.635187] gadget: Number of LUNs=1
[ 1.639014] lun0: LUN: removable file: (no medium)
[ 1.644310] gadget: android_usb ready
[ 1.648240] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 1.653858] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 1.661682] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 1.668783] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.676344] usb usb2: Product: MUSB HDRC host driver
[ 1.681538] usb usb2: Manufacturer: Linux 3.2.0-00244-gcf99001-dirty musb-hcd
[ 1.688997] usb usb2: SerialNumber: musb-hdrc.0
[ 1.694131] hub 2-0:1.0: USB hub found
[ 1.698059] hub 2-0:1.0: 1 port detected
[ 1.702802] mousedev: PS/2 mouse device common for all mice
[ 1.709289] input: ti-tsc as /devices/platform/omap/ti_tscadc/tsc/input/input0
[ 1.717741] using rtc device, am33xx-rtc, for alarms
[ 1.722839] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc0
[ 1.730121] i2c /dev entries driver
[ 1.733944] Linux video capture interface: v2.00
[ 1.739044] usbcore: registered new interface driver uvcvideo
[ 1.745076] USB Video Class driver (1.1.1)
[ 1.801266] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.807785] device-mapper: uevent: version 1.0.3
[ 1.812810] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com
[ 1.821657] Bluetooth: HCI UART driver ver 2.2
[ 1.826303] Bluetooth: HCI H4 protocol initialized
[ 1.831317] Bluetooth: HCILL protocol initialized
[ 1.836231] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0
[ 1.845026] cpuidle: using governor ladder
[ 1.849413] cpuidle: using governor menu
[ 1.857331] usbcore: registered new interface driver usbhid
[ 1.863221] usbhid: USB HID core driver
[ 1.972375] logger: created 256K log 'log_main'
[ 1.977179] logger: created 256K log 'log_events'
[ 1.982192] logger: created 256K log 'log_radio'
[ 1.987094] logger: created 256K log 'log_system'
[ 1.992508] tiadc tiadc: attached adc driver
[ 1.997300] usbcore: registered new interface driver snd-usb-audio
[ 2.004800] _regulator_get: 1-001b supply IOVDD not found, using dummy regulator
[ 2.012624] _regulator_get: 1-001b supply DVDD not found, using dummy regulator
[ 2.020306] _regulator_get: 1-001b supply AVDD not found, using dummy regulator
[ 2.027988] _regulator_get: 1-001b supply DRVDD not found, using dummy regulator
[ 2.038339] asoc: tlv320aic3x-hifi <-> davinci-mcasp.1 mapping ok
[ 2.045412] ALSA device list:
[ 2.048515] #0: AM335X EVM
[ 2.051550] oprofile: hardware counters not available
[ 2.056831] oprofile: using timer interrupt.
[ 2.061465] Netfilter messages via NETLINK v0.30.
[ 2.066488] nf_conntrack version 0.5.0 (7967 buckets, 31868 max)
[ 2.073110] ctnetlink v0.93: registering with nfnetlink.
[ 2.078722] NF_TPROXY: Transparent proxy support initialized, version 4.1.0
[ 2.086020] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
[ 2.092415] xt_time: kernel timezone is -0000
[ 2.097166] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 2.102916] arp_tables: (C) 2002 David S. Miller
[ 2.107802] TCP cubic registered
[ 2.111330] NET: Registered protocol family 10
[ 2.116655] Mobile IPv6
[ 2.119246] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 2.125073] IPv6 over IPv4 tunneling driver
[ 2.129978] NET: Registered protocol family 17
[ 2.134686] NET: Registered protocol family 15
[ 2.139327] can: controller area network core (rev 20090105 abi 8)
[ 2.145909] NET: Registered protocol family 29
[ 2.150569] can: raw protocol (rev 20090105)
[ 2.155030] can: broadcast manager protocol (rev 20090105 t)
[ 2.161159] Bluetooth: RFCOMM TTY layer initialized
[ 2.166319] Bluetooth: RFCOMM socket layer initialized
[ 2.171709] Bluetooth: RFCOMM ver 1.11
[ 2.175624] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.181184] Bluetooth: BNEP filters: protocol multicast
[ 2.186644] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.192976] Registering the dns_resolver key type
[ 2.197956] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 2.205996] ThumbEE CPU extension supported.
[ 2.210514] mux: Failed to setup hwmod io irq -22
[ 2.216050] Power Management for AM33XX family
[ 2.220921] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 2.227592] Copied the M3 firmware to UMEM
[ 2.231982] Cortex M3 Firmware Version = 0x181
[ 2.240496] clock: disabling unused clocks to save power
[ 2.247447] Detected MACID=d0:39:72:8a:21:c6
[ 2.253990] input: gpio-keys as /devices/platform/gpio-keys/input/input1
[ 2.261357] omap_rtc am33xx-rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
[ 2.270754] Waiting for root device /dev/mmcblk0p2...
[ 2.353617] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 2.366036] mmc0: new high speed SDHC card at address e624
[ 2.372220] mmcblk0: mmc0:e624 SU08G 7.40 GiB
[ 2.378587] mmcblk0: p1 p2 p3 p4
[ 2.970578] (stk) :line disc installation timed out
[ 3.418133] EXT4-fs (mmcblk0p2): recovery complete
[ 3.425572] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.434110] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 3.440817] Freeing init memory: 340K
[ 3.464069] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
[ 3.536237] init: cannot open '/initlogo.rle'
[ 3.972126] EXT4-fs (mmcblk0p3): recovery complete
[ 3.979342] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,errors=panic
[ 4.109001] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
[ 4.166340] Disabling lock debugging due to kernel taint
[ 4.172549] Compat-wireless backport release: ol_R5.SP3.03
[ 4.178286] Backport based on wl12xx.git ol_R5.SP3.03
[ 4.277967] cfg80211: Calling CRDA to update world regulatory domain
[ 4.412535] wl12xx: driver version: rowboat-jb-am335x-4.1.2-244-gcf99001-dirty
[ 4.420102] wl12xx: compilation time: Thu Jul 9 17:20:56 2015
[ 4.429360] android_usb: already disabled
[ 4.438403] android_usb: already disabled
[ 4.442846] android_usb: already disabled
[ 4.447240] mtp_bind_config
[ 4.450200] adb_bind_config
root@android:/ # [ 4.531903] adb_open
[ 4.686629] warning: `rild' uses 32-bit capabilities (legacy support in use)
[ 5.090627] (stk) :line disc installation timed out
[ 7.210642] (stk) :line disc installation timed out
[ 9.330569] (stk) :line disc installation timed out
[ 11.450594] (stk) :line disc installation timed out
[ 13.570628] (stk) :line disc installation timed out
[ 14.570611] Bluetooth: st_register failed -22
[ 47.601416] request_suspend_state: wakeup (3->0) at 47580852841 (2000-01-01 00:00:45.830206173 UTC)
[ 48.247257] net eth0: CPSW phy found : id is : 0x1cc915
[ 48.253551] PHY 0:01 not found
[ 48.266731] ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 48.717654] acc_open
[ 48.719972] acc_release
root@android:/ # [ 88.181857] mtp_bind_config
[ 88.184819] adb_bind_config
[ 88.188218] adb_release
[ 88.277207] init: untracked pid 90 exited
[ 88.288782] adb_open
[ 88.347198] init: sys_prop: permission denied uid:1003 name:service.bootanim.exit
[ 98.315698] (hci_tty): inside hci_tty_open (df3ca0a8, cddb28c0)
[ 99.441923] (stk) :line disc installation timed out
[ 101.560616] (stk) :line disc installation timed out
[ 103.680577] (stk) :line disc installation timed out
[ 105.800569] (stk) :line disc installation timed out
[ 107.920595] (stk) :line disc installation timed out
[ 110.040573] (stk) :line disc installation timed out
[ 111.040593] (hci_tty): st_register failed -22
root@android:/ #
root@android:/ #