1、在AM335X EVM 15x15 Baseboard中,AM335X的电源复位引脚PORZ是由VDDSHV6(3.3V)管理的,但是原理图中复位电压由VRTC决定的,当复位电压处于高电平时,只有1.8V,介于PORZ认可的高、低电平之间,即既不属于高电平也不属于低电平,这里会不会有问题?
2、根据AM335X的datasheet,PORZ的复位需要至少1ms时间保证的,但是在AM335X EVM 15x15 Baseboard中如何保证?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、在AM335X EVM 15x15 Baseboard中,AM335X的电源复位引脚PORZ是由VDDSHV6(3.3V)管理的,但是原理图中复位电压由VRTC决定的,当复位电压处于高电平时,只有1.8V,介于PORZ认可的高、低电平之间,即既不属于高电平也不属于低电平,这里会不会有问题?
2、根据AM335X的datasheet,PORZ的复位需要至少1ms时间保证的,但是在AM335X EVM 15x15 Baseboard中如何保证?
(1)AM335x手册上注明RTC_PORZ至少需要1ms,但是AM335X EVM 15x15 Baseboard中是TPS65910通过GPIO_SYNCLK脚连接一个与门后连接到AM335X的RTC_PORZ管脚上的,但是在TPS65910的User's guide上没有关于GPIO_SYNCLK的时序说明。AM335X EVM 15x15 Baseboard的原理图中GPIO_SYNCLK还是断开的,也就是说在AM335X EVM 15x15 Baseboard中RTC_PORZ是直接拉高的,没办法满足手册中要求的1ms.
(2)AM335X PORZ信号是VDDSVH6(3.3V)供电,高电平最低2V,但是AM335X EVM 15x15 Baseboard中PORZ信号时通过sn74lvc1g08输出的,sn74lvc1g08的供电为VRTC(1.8V),输出的PORZ信号高电平为1.8V,不满足高电平最低2V的需要。
谢谢!
1. 这个时序,你可以找我们的power fae详细看看,不过tps65910是evm板上所使用的pmic,所以时序是经过验证可以保证的。
2. 请问你在什么地方看到的VDDSVH6必须在2v以上,datasheet上写的都是1.8v和3.3v都是可选的
谢谢 Yaoming Qin的回答。
evm板上使用的vaux2给VDDSVH6供电的,tps65910的user guide上说明了在从EEPROM启动时,vaux2输出就是3.3V
原理图是错的,ti有个文档 am335x general purpose evm errata 你可以看一下。
我在用的时候,感觉这个很麻烦,就没有按照ti的evm板做,参考了一下beaglebone的图纸。evm这样设计应该是要porz一定不能早于rtc_porz有效,这个是335的手册中要求的。实际上tps65910电源芯片就已经保证了 先是rtc_porz有效(tps65910 ug for am335x手册里面没对这个说明),然后porz有效,所以我就直接把pmic_porz经过一个与门后直接接到处理器porz上。测试的结果也证明,这样是对的。
你好!在VDDSHV6接3.3v电源时,PWRONRSTn也可以接1.8V,具体说明可以查看如下链接:http://e2e.ti.com/support/arm/sitara_arm/f/791/t/227178.aspx