我按照 MMWAVE DFP User Guidess手册中的执行完visual studio的程序以后,在采集板的ssd中找到了捕获后的数据,有8个bin文件,如下图所示:
但是我想使用mmwavestudio进行处理, 使用post processes可视化结果,需要一个log文件,但是没有看到在哪生成这个log文件,我应该怎么进行数据的解析以及可视化呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您是不是没有点trigger frame? user guide中有如下描述。
Click on “TDAxx ARM” with any one of the device selected. This should be done only once for a capture session. By default, the framing status (refer the below screenshot) is “NOT FRAMING” for all the devices
你好,
建议你参考一下:C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\MatlabExamples\4chip_cascade_MIMO_example\utils\dataParse\read_ADC_bin_TDA2_separateFiles.m