This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: 编译driver_vital_signs(xwr16xx_vitalSignsDemo_lab)出错

Part Number: AWR1843
Other Parts Discussed in Thread: MATHLIB, IWR6843,

参考官方的指导,Migrating to xWR68xx and xWR18xx Millimeter Wave Sensors(https://www.ti.com/lit/an/swra656b/swra656b.pdf )

以及:C:\ti\mmwave_automotive_toolbox_3_4_0\labs\incabinsensing\driver_vital_signs中说明

想要实现把xwr16xx_vitalSigns这个Demo移植到AWR 1843板子上,在编译过程中出现下述错误:

分析原因为SDK的版本与driver_vital_signs中release note中要求的不一致导致的错误。

driver_vital_signs中release note要求SDK 1.1.0.2:

但是在移植文件中又要求SDK 3.3.0或者更高的版本:

两个文件中的要求前后产生了矛盾,请问应该如何选择呢?

目前我是选择了使用mmwave_sdk_03_03_00_03,从而出现了图一红框中的错误。移植driver_vital_signs这个demo到AWR 1843板子上的这个事情困扰我两天了,还请官方人员帮忙说明一个详细有效的处理步骤。

  • 建议用工程编译,在ccs导入工程。

  • 您好,我按照移植指导表格中的要求进行修改,并在CCS导入工程的方式进行编译, 在编译dss工程过程中出现下述错误:


    **** Build of configuration Debug for project vitalSigns_16xx_dss ****

    "C:\\ti\\ccs1100\\ccs\\utils\\bin\\gmake" -k -j 8 all -O

    rm -f C:/Users/17377/workspace_vital_signs/vitalSigns_16xx_dss/xwr16xx_vitalSignsDemo_dss.bin
    makefile:187: recipe for target 'pre-build' failed
    process_begin: CreateProcess(NULL, rm -f C:/Users/17377/workspace_vital_signs/vitalSigns_16xx_dss/xwr16xx_vitalSignsDemo_dss.bin, ...) failed.
    make (e=2): 系统找不到指定的文件。

    gmake[1]: [pre-build] Error 2 (ignored)

    Building file: "../dss_data_path.c"
    Invoking: C6000 Compiler
    "C:/ti/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="C:/Users/17377/workspace_vital_signs/vitalSigns_16xx_dss" --include_path="C:/ti/mmwave_sdk_03_04_00_03/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR18XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="dss_data_path.d_raw" --cmd_file="configPkg/compiler.opt" "../dss_data_path.c"

    >> Compilation failure
    subdir_rules.mk:9: recipe for target 'dss_data_path.oe674' failed
    "..\dss_mmw.h", line 233: error #20: identifier "Mailbox_Handle" is undefined
    "../dss_data_path.c", line 101: fatal error #1965: cannot open source file "ti/demo/utils/rx_ch_bias_measure.h"
    1 error and 1 catastrophic error detected in the compilation of "../dss_data_path.c".
    Compilation terminated.
    gmake[1]: *** [dss_data_path.oe674] Error 1
    Building file: "../dss_main.c"
    Invoking: C6000 Compiler
    "C:/ti/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="C:/Users/17377/workspace_vital_signs/vitalSigns_16xx_dss" --include_path="C:/ti/mmwave_sdk_03_04_00_03/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR18XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --diag_wrap=off --diag_warning=225 --display_error_number --gen_func_subsections=on --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="dss_main.d_raw" --cmd_file="configPkg/compiler.opt" "../dss_main.c"

    >> Compilation failure
    subdir_rules.mk:9: recipe for target 'dss_main.oe674' failed
    "..\dss_mmw.h", line 233: error #20: identifier "Mailbox_Handle" is undefined
    "../dss_main.c", line 115: error #20: identifier "SOC_XWR18XX_DSS_HSRAM_SIZE" is undefined
    "../dss_main.c", line 819: error #20: identifier "Mailbox_Handle" is undefined
    "../dss_main.c", line 945: error #137: struct "MmwDemo_output_message_header_t" has no field "subFrameNumber"
    "../dss_main.c", line 1312: error #20: identifier "SOC_XWR18XX_DSS_ADCBUF_SIZE" is undefined
    5 errors detected in the compilation of "../dss_main.c".
    gmake[1]: *** [dss_main.oe674] Error 1
    gmake[1]: Target 'main-build' not remade because of errors.
    gmake: *** [all] Error 2
    makefile:153: recipe for target 'all' failed

    **** Build Finished ****

    随后,在编译mss工程中出现下述错误:

    **** Build of configuration Debug for project vitalSigns_16xx_mss ****

    "C:\\ti\\ccs1100\\ccs\\utils\\bin\\gmake" -k -j 8 all -O

    rm -f C:/Users/17377/workspace_vital_signs/vitalSigns_16xx_mss/xwr16xx_vitalSignsDemo_mss.bin
    makefile:186: recipe for target 'pre-build' failed
    process_begin: CreateProcess(NULL, rm -f C:/Users/17377/workspace_vital_signs/vitalSigns_16xx_mss/xwr16xx_vitalSignsDemo_mss.bin, ...) failed.
    make (e=2): 系统找不到指定的文件。

    gmake[1]: [pre-build] Error 2 (ignored)

    Building file: "../cli.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=32 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/17377/workspace_vital_signs/vitalSigns_16xx_mss" --include_path="C:/ti/mmwave_sdk_03_04_00_03" --include_path="C:/ti/mmwave_sdk_03_04_00_03/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=_LITTLE_ENDIAN --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_SIZE=0x40000 --define=DebugP_ASSERT_ENABLED -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=packed --abi=eabi --preproc_with_compile --preproc_dependency="cli.d_raw" --cmd_file="configPkg/compiler.opt" "../cli.c"

    >> Compilation failure
    subdir_rules.mk:9: recipe for target 'cli.obj' failed
    "..\mss_mmw.h", line 196: error #20: identifier "Mailbox_Handle" is undefined
    "../cli.c", line 573: warning #225-D: function "MMWDEMO_SATURATE_HIGH" declared implicitly
    "../cli.c", line 574: warning #225-D: function "MMWDEMO_SATURATE_LOW" declared implicitly
    1 error detected in the compilation of "../cli.c".
    gmake[1]: *** [cli.obj] Error 1
    Building file: "../mss_main.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=32 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/17377/workspace_vital_signs/vitalSigns_16xx_mss" --include_path="C:/ti/mmwave_sdk_03_04_00_03" --include_path="C:/ti/mmwave_sdk_03_04_00_03/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=_LITTLE_ENDIAN --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_SIZE=0x40000 --define=DebugP_ASSERT_ENABLED -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=packed --abi=eabi --preproc_with_compile --preproc_dependency="mss_main.d_raw" --cmd_file="configPkg/compiler.opt" "../mss_main.c"

    >> Compilation failure
    subdir_rules.mk:9: recipe for target 'mss_main.obj' failed
    "..\mss_mmw.h", line 196: error #20: identifier "Mailbox_Handle" is undefined
    "../mss_main.c", line 192: error #20: identifier "rlRfInitomplete_t" is undefined
    "../mss_main.c", line 192: error #20: identifier "ptrRFInitCompleteMessage" is undefined
    "../mss_main.c", line 196: error #29: expected an expression
    "../mss_main.c", line 196: error #66: expected a ";"
    "../mss_main.c", line 526: error #20: identifier "Mailbox_Handle" is undefined
    "../mss_main.c", line 562: warning #169-D: argument of type "int32_t *" is incompatible with parameter of type "MMWave_CalibrationData *"
    "../mss_main.c", line 562: error #167: too few arguments in function call
    7 errors detected in the compilation of "../mss_main.c".
    gmake[1]: *** [mss_main.obj] Error 1
    gmake[1]: Target 'main-build' not remade because of errors.
    gmake: *** [all] Error 2
    makefile:152: recipe for target 'all' failed

    **** Build Finished ****

    这些错误与我使用SDK makefile的方式提示的类似,也是存在一些变量未定义,例如"Mailbox_Handle" is undefined

    这是代表源代码缺少引用相关的头文件而导致的错误?还是我之前猜测的SDK版本不对所导致的错误呢?

  • 请尝试用mmwave_automotive_toolbox_2_9_1和SDK 2.0.0.4编译。

    mmwave_automotive_toolbox_2_9_1\labs\lab0001-driver-vital-signs\vitalSigns_target and was able to build with SDK 2.0.0.4. 
    https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/982790/iwr1642boost-driver-s-vital-signs-lab-used-on-iwr1642

  • 您好,SDK 2.0.0.4只支持1642,而我的是1843

  • 你好,

    你可以参考industrial toolbox里IWR6843的vital sign代码么?

  • 您好,IWR6843可以在AWR1843板子上运行吗?我试试这个Demo吧

  • 你好,

    IWR6843的代码不能直接在AWR1843上运行,你可以根据你参考的移植文档来移植。IWR6843基于的是sdk3.5.

  • 请问移植文档在哪里,移植文档并没有IWR6843移植到AWR1843的说明

  • 移植文档并没有IWR6843移植到AWR1843的说明

    是的。但是移植需要修改的东西是类似,可以参考。