Other Parts Discussed in Thread: UNIFLASH
我基于people counting的demo进行代码编写,发现当bin文件超过908KB的时候,虽然可以用uniflash下载到板子上,但是程序无法运行。然而利用CCS的调试功能是可以让程序运行的。当我稍微降低代码量,让bin小于908KB的时候就可以运行。请问这是怎么回事?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我基于people counting的demo进行代码编写,发现当bin文件超过908KB的时候,虽然可以用uniflash下载到板子上,但是程序无法运行。然而利用CCS的调试功能是可以让程序运行的。当我稍微降低代码量,让bin小于908KB的时候就可以运行。请问这是怎么回事?
在bin文件烧录进去后,将板子SOP跳线帽调为功能模式,然后用CCS对DSP和ARM进行load symbols,出现如下报错:
Cortex_R4_0: Trouble Setting Breakpoint with the Action "Process CIO" at 0x1d372: (Error -1065 @ 0x1D374) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129) Cortex_R4_0: Breakpoint Manager: Retrying with a AET breakpoint Cortex_R4_0: Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0x1f15c: (Error -1065 @ 0x1F15E) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129) Cortex_R4_0: Breakpoint Manager: Retrying with a AET breakpoint CS_DAP_0: GEL Output: --->> DSS is under application controlled reset. Prior to connecting this reset must be released. CS_DAP_0: GEL Output: --->> The debugger will enable "Halt On Reset" and release the application-extended reset CS_DAP_0: GEL Output: --->> "Halt On Reset" has been enabled on the C674X_0CS_DAP_0: GEL Output: --->> ERROR : timeout while waiting for DSS to power on C674X_0: Error connecting to the target: (Error -6305) PRSC module failed to write to a router register. (Emulation package 9.4.0.00129)