This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: XIWR6843 与IWR6843烧写相同程序,XIWR6843程序正常起来,IWR6843程序跑不起来?

Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: ALP, IWR6843AOP, IWR6843

IWR6843AOPEVM板子上的主芯片型号丝印为XIWR6843 QG ALP,烧写mmwave_industrial_toolbox_4_11_0中的demo程序,程序可以正常跑起来。

然后我们自己开发的板子,用的是IWR6843AOP,主芯片型号丝印为IWR6843 QG ALP,烧写相同的demo程序,程序跑不起来。

请问下是什么原因导致的?

经过对比调试发现,通过Jtag,Debug的方式,IWR6843AOPEVM板上的MSS端程序可以成功的load到从0x00000000地址起始的ram上,但是我们自己开发的板子是不可以load到0x00000000起始的这段内存。

查看18xx/16xx/14xx/68xx  Technical Reference Manual发现0x00000000是一个TCMA的不可访问的地址。

但是为啥IWR6843AOPEVM板子又可以访问呢?