Other Parts Discussed in Thread: OPT3101
您好!
我购买了TI官方的OPT3101EVM评估板,插到PC的USB口能识别到两个虚拟串口com4和com5,然后打开Latte软件,也能正常显示测量波形和相关数据,也可以正常修改配置。但是当我想用MSP430Flasher.exe更新EVM时,出现了PC无法识别USB FETs的问题。
C:\ti\MSPFlasher_1.3.20>.\MSP430Flasher.exe -w "C:\workspace\proj-OPT3101\OPT3101\software\sbac203b-OPT3101-SDK-v0.9.1\bac203b\release_0p9p1\OPT3101_SDK\Debug\OPT3101_SDK.txt" -v -e ERASE_MAIN
* -----/|-------------------------------------------------------------------- *
* / |__ *
* /_ / MSP Flasher v1.3.20 *
* | / *
* -----|/-------------------------------------------------------------------- *
*
* Evaluating triggers...done
* Checking for available FET debuggers:
* Couldn't find any connected USB FETs!
* Powering down...done
* Disconnecting from device...done
*
* ----------------------------------------------------------------------------
* Driver : closed (MSP DebugStack not initialized)
* ----------------------------------------------------------------------------
*/
C:\ti\MSPFlasher_1.3.20>
用CCS能成功编译官网提供的OPT3101 SDK v0.9.1 (Rev. B),得到了最终的固件OPT3101_SDK.txt,但是使用PC CMD工具执行烧录指令时出错。
请问是什么原因导致这个现象?我有如下几个疑问:
1. 是否有其他升级相关的驱动要装?
2. 升级时需要先按下EVM上的SW1升级按键再系统上电是吗?此时会发现PC设备管理器多了几个HID的设备,这是否正常?
感谢您的答复,谢谢!