Other Parts Discussed in Thread: AWR2243,
您好!
芯片手册上说是76GHz 至 81GHz 的覆盖范围,具有 4GHz 的可 用带宽,想请教的是能用到5G带宽吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
AWR1243只能到4GHz。可以考虑用AWR2243,可以到5GHz。请看数据手册说明。
76- to 81-GHz coverage with 5 GHz available bandwidth
https://www.ti.com/lit/ds/symlink/awr2243.pdf