Other Parts Discussed in Thread: AWR2243
在PROC054E_AWR_Pull_Resistors.SchDoc中,AWR2243的SPI_MOSI通过R183接到GND。但是在AWR2243的规格书中,该引脚默认是上拉的。能否麻烦确认一下,该引脚是接上拉电阻还是下拉电阻?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在PROC054E_AWR_Pull_Resistors.SchDoc中,AWR2243的SPI_MOSI通过R183接到GND。但是在AWR2243的规格书中,该引脚默认是上拉的。能否麻烦确认一下,该引脚是接上拉电阻还是下拉电阻?
Datasheet规格书中指的是管脚内部电阻是上拉的,板子上是指和外部器件的接法。具体请看下面工程师的回复。
I think you are referring to two different things. The DS talks about status of PULL structures associated with the IO after device POWER UP. Where as the Board schematic is talking about the external recommended interface. This signal is also going to the HOST.