This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA970: PGA970 EVM GUI 问题

Part Number: PGA970
Other Parts Discussed in Thread: USB2ANY

Dear All:

我在使用PGA970 EVM GUI 软件的时候遇到一个奇怪的问题,查阅了各种用户手册没有找到答案。
PGA970 EVM GUI 软件可以顺利安装,使用了两台电脑分别为win10 和Win7系统,情况是一样的。

 界面中除了<FRAM & DEVRAM> <Data & Waveform RAM>选项似乎可以正常工作外,

其他选项显示如  <Interface Settings [Broken]>   <ADC Settings [Broken] >   并有红色底色。

是安装的时候哪里设置错误还是其他原因?

是否要先写入PGA970的firmware?

我查阅其他资料似乎可以不用,PGA970 EVM GUI user's guide里也没提要先下载固件。

USB2Any firmware已经升级
跳线J11 J12 J18 J19 close

J15 connect 1-2 ( 也试过2-3,一样)
 12V 7.5V 5V 3.3V AVDD 3.0V and DVDD1.86V 电压都检查过似乎是正常的。

迫切需要得到您的指点。

BRs,

Jason