Other Parts Discussed in Thread: FDC1004
Hello dear TI experts, my client needs to check the liquid level in the drip pot of the liquid pump of the hemodialysis machine. The drip pot is a cylindrical tube with a length of 70mm and a diameter of 23mm, is it suitable for TDC1000 high accuracy level detection in this case? If so, what are the strengths and special points? What kind of effect can it achieve? If you compare it with FDC1004, is there an advantage, and what are the advantages?