This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6113: VSS GND EP的硬件连接

Part Number: TMUX6113

你好:

      我们在使用TMUX6113(WQFN封装)时,硬件上将VSS管脚接负电源-11.4V、VDD管脚接正电源+15.5V、GND和EP管脚接在连接到板卡参考地REF_GND(但数据手册中说EP在内部是电气连接到VSS上的)。在后续测试中部分板卡输出-11.4V的电源DC/DC出现异常(该DC/DC厂家分析说是过流保护),如果是过流保护是否是因为我们硬件设计上将VSS(-11.4V)的EP管脚接到REF_GND上导致的过流。-11.4V电源后级接了很多器件包括运放、MUX和模拟开关。

同时我们有以下几个问题:

1、出现异常的板卡中我们将输出-11.4V电压降低到-8.5V或-5V后,多数异常板卡能恢复正常,另外不能恢复正常的板卡发现有-11.4V电压对REF_GND短路的现象(有TMUX6113短路,还有其他器件短路);

2、我们30张板卡中大概有6张板卡出现异常;

2、我们相知道EP管脚在芯片内部与VSS、GND是如何连接的?

3、按照我们现在这种设计是否还有改进的措施。

谢谢!

硬件接线如下图所示(EP接的REF_GND,没接VSS)