CD4053在我们的应用中,有时用,有时不用,不用时可以浮空或接地,但不清除浮空,接地那种方式功耗小。
我们的工作电源为15VDC,请帮确认不用时相关功耗数据,如有浮空和接地的比较最好。
TKS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
datasheet 中如下截图给出了器件的静态电流值:
关于不使用管脚的连接,请查看下面视频:
您说的应该是I/O口的浮空或接地,这个不用时是建议浮空的,在高速信号应用场合,不使用的I/O是建议通过50Ω电阻接地的;
很抱歉,没有浮空与接地的功耗比较参数,也没有I/O口状态转换时的功耗参数。
根据CD4053B的工作原理,我个人认为不管浮空还是接地对 CD4053B的功耗是没有影响的,影响的应该是驱动设备的功耗。如果I/O通过50Ω接地了,那么驱动这个I/O的设备如果有输出的话,驱动接地的I/O功耗将大一些。