This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2640 luanchpad下载程序搜索不到设备

Other Parts Discussed in Thread: CC2540, BLE-STACK, CC2640R2F, CC2650

SDK版本simplelink_cc2640r2_sdk_1_30_00_25

下载SimpleBLEPeripheral 的HEX文件到Luanchpad 后,用iphone 6S 的APP 不知道为何搜索不到设备.

 下载工具为 Flash Programmer 2 能看到烧写成功,读Flash也可以。

 下载步骤:

  界面Main——Multiple 第一个文件为simple_peripheral_cc2640r2lp_stack.hex,第二文件为simple_peripheral_cc2640r2lp_app.hex。

  Action界面选择: 1 Erase --pages in image  ; 2 Program -- Entire source file 选择两项 

  之后烧录变成绿色:Success 

  请问 烧录成功后 为什么不能搜索到SimpleBLEPeripheral设备?是我下载的程序的方式出错吗?

  • 使用的APP是什么 ? 有无打开蓝牙? 推荐使用 lightblue,或者TI自己的apps.

    lightBlue

    https://itunes.apple.com/us/app/lightblue-explorer-bluetooth/id557428110?mt=8

    Description

    LightBlue Explorer can connect you to all of your devices that use Bluetooth 4.0 Low Energy (also known as Bluetooth Smart, or Bluetooth Light). 

    LightBlue Explorer has two modes, central and peripheral. In central mode, you can scan for and connect to all BLE devices around you. Once connected, you have a detailed view of all the device's profiles, from which you can read and write to characteristics and subscribe to notifications.

    To use peripheral mode, tap the blue circle next to one of the profiles listed under "Virtual Peripherals." When the blue checkmark appears, your iOS device will begin advertising as that particular BLE peripheral. LightBlue Explorer allows you to customize the services and characteristics of any virtual peripheral profile. Tap the "+" in the top right corner of the home screen to add new virtual peripherals. You can also clone any peripheral you connect to in central mode and save that profile to your list of virtual peripherals. 

    Full support of read, write, and notify is included. You can view the signal strength (RSSI) to get an idea of how close you are to the peripheral.

    The log feature allows you to keep track of all significant BLE events that occur while using the app (e.g., device discovery, connection, reading, writing).

    Use LightBlue Explorer to test your new BLE Heart Rate Monitor, temperature sensor, TI CC2540 Keyfob, Nordic uBlue, Panasonic PAN1720, etc. LightBlue Explorer is also ideal for developers wanting to test the firmware of their own BLE peripherals.

    Key Features:
    - Scan for any peripherals
    - Grab basic device info (UUID, RSSI )
    - Browse Characteristics and Services 
    - Register for Notifications
    - Read Characteristics
    - Write to Characteristics in Hex, Oct, Bin, Decimal or Ascii
    - Clone peripheral profiles
    - Choose from an array of common preconfigured peripheral profiles
    - Advertise as a peripheral using custom profiles
    - Thoroughly log BLE events

    This app will not work on iPhone4, iPhone3GS, iPhone3G or iPod Touches before the 5th generation, or any other iOS device without built-in Bluetooth Low Energy support.

    What's New in Version 2.4.0

    * Added new feature that allows the user to sort and filter discovered devices by signal strength.
    * Fixed alignment of alert that occurs when Bluetooth is turned off.

    Screenshots

    iPhone Screenshot 1
    iPhone Screenshot 2
    iPhone Screenshot 3
    iPhone Screenshot 4

    Customer Reviews

  • 最新的SDK是1_35_00_33了, 可以更新下再试试.另外,一定要确认你是R2的板子

    http://www.ti.com/tool/BLE-STACK?keyMatch=BLE-STACK&tisearch=Search-EN-Everything

    我的烧录供你测试下:

    BLE-STACK for CC26xx and CC13xx SimpleLink™ wireless MCUs

    Texas Instruments royalty-free BLE-Stack software development kit (SDK) for TI’s SimpleLink™ Bluetooth® low energy family of ARM® Cortex®-M3 based wireless microcontrollers (MCUs) including the SimpleLink Bluetooth low energy CC2640R2F wireless MCUSimpleLink Bluetooth low energy CC2640 wireless MCUSimpleLink multi-standard CC2650 wireless MCU and SimpleLink dual band CC1350 wireless MCU provides full-featured Bluetooth 4.2 and Bluetooth 5 certified stacks that includes all necessary software, sample applications and documentation to quickly get started with the development of single-mode Bluetooth low energy (BLE) applications.

    For an overview of TI’s Bluetooth low energy solutions, including information on how to select which SimpleLink wireless MCU is best for your Bluetooth low energy application, please visit http://www.ti.com/ble.

    To download the latest BLE-Stack SDK version, select the version above corresponding to your device or development kit.

    Features

    • Bluetooth 5 certified support for 2 Mbps High Speed Mode, Privacy 1.2.1 and Channel Selection Algorithm #2. Demonstration capability for evaluating LE Coded PHYs in Long Range mode. (CC2640R2F BLE5-Stack only)
    • Full support for all Bluetooth core specification 4.2 features: LE Secure Connections, LE Data Length Extension and LE Privacy 1.2.
    • Sample applications for all BLE device roles: Central, Peripheral, Broadcaster/Beacon and Observer.
    • Ability to operate without a 32-kHz crystal in peripheral and beacon configurations.
    • Device Firmware Upgrades using TI’s Over-the-air Download (OAD) service and tools.
    • Advanced topology including concurrent master/slave multi-role operation and support for up to 8 simultaneous connections.
    • Voice-over-BLE support on the CC2650 remote control kit.
    • Standalone System-on-Chip (SoC) and network processor software configurations
    • Ultra-low power advertisement and connected states for applications such as peripherals and beacons, including the popular Apple iBeacon® and Google Eddystone™ formats.
    • Built on top of TI-RTOS framework and includes peripheral drivers and advanced power management libraries.
    • Broad selection of development and Internet of Things (IoT) prototyping kits, including CC2640R2 LaunchPad™ development kitCC2650 LaunchPad development kitCC1350 LaunchPad development kitCC2650 SensorTag kit, CC2650 voice remote control kit and CC2650 Module BoosterPack.
    • Wide range of sample applications with certified profiles to reduce time to market
    • Bluetooth qualified design listing to reduce certification test time.
    • Flexible protocol stack configuration options to maximize application memory.
    • Supported in IAR Embedded Workbench for ARM® and Code Composer Studio™ integrated development environment (IDE) tool chains.

    Bluetooth 4.2 and Bluetooth 5 support for CC2640R2F

    The SimpleLink CC2640R2 Software Development Kit (SDK) includes the Texas Instruments royalty-free BLE software stacks for developing single-mode BLE applications on the SimpleLink CC2640R2F Bluetooth low energy wireless MCU. This SDK includes two components; one for developing Bluetooth 5 (BLE5-Stack) and one for Bluetooth 4.2 (BLE-Stack) applications on the CC2640R2 LaunchPad (LAUNCHXL-CC2640R2) development kit. Both software stacks support embedded and network processor applications and are backwards compatible with previous Bluetooth 4.1 and 4.0 specifications. Refer to the SDK release notes for a detailed description of the features available in this SDK.

  •  非常感谢!  是我的SDK 毕竟旧的缘故,现在用最新的版本可以用了