您好,我们现在尝试学习、使用WL1831mod模块在嵌入式Linux系统中实现蓝牙功能;但是由于我们是第一次接触这种技术,看了一些技术文档后,还是无从下手,不知道应该怎么实现这个蓝牙功能。
请问,可不可以介绍一下使用这个WL1831mod在Linux系统下实现蓝牙功能的具体操作流程、步骤;谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Butterfly 你好,我之前可能没有描述清楚,我们的目标是打算在OMAP-L138处理器开发板上的arm核运行Linux系统,然后在这个开发板上使用WL1831模块的蓝牙功能。 但是我们刚开始接触这类产品,不清楚具体的操作流程。
1、请问我们是不是应该:在运行Linux系统的电脑中安装Processor SDK,然后在这个linux系统电脑上开发;最后在添加了WL1831模块驱动的OMAP-L138开发板上连接WL1831模块使用蓝牙功能?
2、上面的那个开源WL18xx的Linux驱动下载不到,每次都是最后的时候就下载失败了。
谢谢回复。